How to run inference using the STAI MPU C++ API

Revision as of 08:45, 13 September 2024 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines


1. Article purpose[edit source]

This article describes how to run an inference on the STM32MPx using the STAI MPU C++ API. It is an example based on an image classification application. The unified architecture of the API allows deploying the same application on all the STM32MPx platforms.

Info white.png Information
This article provides a simple inferencing example using the STAI MPU C++ API. If you wish to explore all the functions provided by the API, please refer to the STAI MPU C++ Reference.

2. STAI MPU C++ API[edit source]

STAI MPU is a cross STM32MPx platforms machine learning and computer vision inferencing API with a flexible interface to run several deep learning models formats such as TFLite, ONNX and NBG. If you wish to learn more about the API structure please refer to STAI MPU: AI unified API for STM32MPUs. In the next section we explore, with a basic image-classification example, how to inference your models on the board using the STAI MPU C++ API whether you are running a TFLite, an ONNX or an NBG model on either STM32MP1x or STM32MP2x.

Warning DB.png Important
The STM32MP1 based platforms come with no AI hardware acceleration chip, so inferencing an NBG model on these platforms will reslt in an error.

3. Running an inference using the STAI MPU C++ API[edit source]

3.1. Install runtime prerequisites on the target[edit source]

After having configured the AI OpenSTLinux package, you can install the X-LINUX-AI components and the packages needed to run the example. First, we start by installing main packages needed for image processing which are Python Numpy, Python OpenCV.

Board $> apt-get install python3-numpy python3-opencv

Then, we will need to install the API plugins required during runtime depending on the model format used for the inference:

  • If you are using a TFLite™ model, please run the following command:
 x-linux-ai -i  stai-mpu-tflite
  • If you are using an ONNX™ model, please run the following command:
 x-linux-ai -i  stai-mpu-ort
  • If you are running your model on an STM32MP2 board and running and NBG model, please run the following command:
 x-linux-ai -i  stai-mpu-ovx
Info white.png Information
The package stai-mpu-ovx is not available on STM32MP1x boards. The TFLite™ and ONNX™ runtimes supported by the API are running exclusively on CPU.
Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

3.2. Install and launch of the X-LINUX-AI SDK[edit source]

First of all, the installation of the X-LINUX-SDK on your host machine is required to be able to cross-compile AI applications for STM32 boards.

Info white.png Information
The SDK environment setup script must be run once on each new working terminal on which you cross-compile.

Once the OpenSTLinux SDK is installed, go to the installation directory and source the environment:

 cd <working directory absolute path>/Developer-Package/SDK
  • On STM32MP2 series' boards More info green.png:
 source unknown package
  • On STM32MP1 series' boards More info green.png:
 source unknown package
Warning white.png Warning
The path to the SDK must be adapted depending of your working configuration (board used).

3.3. Write a simple NN inference C++ program[edit source]

#include "stai_mpu_network.h"
#include <opencv2/imgcodecs.hpp>
#include <opencv2/imgproc.hpp>
#include <sys/time.h>
#include <fstream>

int main (int argc, char* argv[]){
    if (argc != 3)
        return 0;
    /////////////////////////////////////////////////
    ///     Loading the model and metadata        ///
    /////////////////////////////////////////////////
    std::string model_path = argv[1]; // .onnx or .tflite or .nb file
    stai_mpu_network stai_model = stai_mpu_network(model_path);
    int num_inputs = stai_model.get_num_inputs();
    int num_outputs = stai_model.get_num_outputs();
    std::vector<stai_mpu_tensor> input_infos = stai_model.get_input_infos();
    std::vector<stai_mpu_tensor> output_infos = stai_model.get_output_infos();
    std::vector<int> input_shape(input_infos[0].get_rank());
    std::vector<int> output_shape(output_infos[0].get_rank());
    for (int i = 0; i < num_inputs; i++) {
        stai_mpu_tensor input_info = input_infos[i];
        std::cout << "** Input node: " << i;
        std::cout << " -Input name: " << input_info.get_name();
        std::cout << " -Input dims: " << input_info.get_rank();
        std::cout << " -Input type: " << input_info.get_dtype();
        input_shape = input_info.get_shape();
        std::cout << std::endl;
    }
    for (int i = 0; i < num_outputs; i++) {
        stai_mpu_tensor output_info = output_infos[i];
        std::cout << "** Output node: " << i;
        std::cout << " -Output name: " << output_info.get_name();
        std::cout << " -Output dims: " << output_info.get_rank();
        std::cout << " -Output type: " << output_info.get_dtype();
        output_shape = output_info.get_shape();
        std::cout << std::endl;
    }
    int input_width = input_shape[1];
    int input_height = input_shape[2];
    int input_channels = input_shape[3];
    auto size_in_bytes = input_height * input_width * input_channels;
    ////////////////////////////////////////////////////
    ///           Pre-processing the Image           ///
    ////////////////////////////////////////////////////
    std::string image_path = argv[2]; // .onnx or .tflite file
    cv::Mat img_bgr = cv::imread(image_path);
    cv::Mat img_nn;
    cv::Size size_nn(input_width, input_height);
    cv::resize(img_bgr, img_nn, size_nn);
    cv::cvtColor(img_nn, img_nn, cv::COLOR_BGR2RGB);
    uint8_t* input_data = img_nn.data;
    bool floating_model = false;
    float input_mean = 127.5f;
    float input_std = 127.5f;
    ///////////////////////////////////////////////////
    ///         Setting input and infer             ///
    ///////////////////////////////////////////////////
    uint8_t* input_tensor_int = new uint8_t[size_in_bytes];
    float* input_tensor_f = new float[size_in_bytes];
    if (input_infos[0].get_dtype() == stai_mpu_dtype::STAI_MPU_DTYPE_FLOAT32)
        floating_model = true;
    if (floating_model) {
        for (int i = 0; i < size_in_bytes; i++)
            input_tensor_f[i] = (input_data[i] - input_mean) / input_std;
        stai_model.set_input(0, input_tensor_f);
    } else {
        for (int i = 0; i < size_in_bytes; i++)
            input_tensor_int[i] = input_data[i];
        stai_model.set_input(0, input_tensor_int);
    }
    stai_model.run();
    ///////////////////////////////////////////////////
    ///      Reading and post-processing output     ///
    ///////////////////////////////////////////////////
    void* outputs_tensor = stai_model.get_output(0);
    int output_dims = output_infos[0].get_rank();
    stai_mpu_dtype output_dtype = output_infos[0].get_dtype();
    output_shape = output_infos[0].get_shape();
    int output_size = output_shape[output_dims-1];
    std::vector<int> results_idx(5);
    std::vector<float> results_accu(5);
    if (output_dtype == stai_mpu_dtype::STAI_MPU_DTYPE_FLOAT32 || output_dtype == stai_mpu_dtype::STAI_MPU_DTYPE_FLOAT16) {
        float* output_data = static_cast<float*>(outputs_tensor);
    for (int i = 0; i < 5; i++) {
        results_idx[i] = std::distance(&output_data[0],
        std::max_element(&output_data[0], &output_data[output_size]));
        results_accu[i] = output_data[results_idx[i]];
        output_data[results_idx[i]] = 0;
    }
    } else if (output_dtype == stai_mpu_dtype::STAI_MPU_DTYPE_UINT8){
        uint8_t* output_data = static_cast<uint8_t*>(outputs_tensor);
        for (int i = 0; i < 5; i++) {
            results_idx[i] = std::distance(&output_data[0],
                 std::max_element(&output_data[0], &output_data[output_size]));
            results_accu[i] = output_data[results_idx[i]] / 255.0;
            output_data[results_idx[i]] = 0;
        }
    }
    free(outputs_tensor) //Required for NBG to avoid memory leak
    for (int i = 0; i < 5; i++) {
        std::cout << i << ": " << results_idx[i] << "-" << results_accu[i] <<
        std::endl;
    }
}
Warning DB.png Important
When using an NBG model, please pay attention to freeing the pointer of the output_tensor read from get_output function to avoid memory leaks issues.

3.4. Create the Makefile[edit source]

Create the following Makefile in the sources/stai_mpu/examples directory:

OPENCV_PKGCONFIG?="opencv4"
ARCHITECTURE?=""
TARGET_BIN = stai_mpu_image_classification
CXXFLAGS += -Wall $(shell pkg-config --cflags $(OPENCV_PKGCONFIG))
CXXFLAGS += -std=c++17 -O3
CXXFLAGS += -I../../

LDFLAGS += -lpthread -lopencv_core -lopencv_imgproc -lopencv_imgcodecs
LDFLAGS += -lstai_mpu -ldl

SRCS = stai_mpu_image_classification.cc
OBJS = $(SRCS:.cc=.o)

all: $(TARGET_BIN)

$(TARGET_BIN): $(OBJS)
	$(CXX)  -o $@ $^ $(LDFLAGS)

$(OBJS): $(SRCS)
	$(CXX) $(CXXFLAGS) -c $^

clean:
	rm -rf $(OBJS) $(TARGET_BIN)
Info white.png Information
The runtime plugin libraries such as libstai_mpu_ovx.so, libstai_mpu_tflite.so or libstai_mpu_ort.so are loaded dynamically during runtime, so there is no need to use them in the linking of you application during build time. Only the -lstai_mpu is required to link with the STAI MPU C++ API.


3.5. Download and prepare test data[edit source]

3.6. Cross-compilation and launch[edit source]

Run the cross-compilation:

 cd ..
 make

Once the compilation is finished, a binary file named stai_mpu_image_classification has been created.
Copy the binary file and the test data directory onto the board:

 scp -r edgetpu_cpp_example/ root@<board_ip>:/path/
 scp two_models_one_tpu    root@<board_ip>:/path/
Info white.png Information
The corresponding runtime plugin to your model should installed before running the binary.

Connect to the board and launch the example:

 ./stai_mpu_image_classification

After 2000 inferences the result is:

Running model: edgetpu_cpp_example/inat_bird_edgetpu.tflite and model: edgetpu_cpp_example/inat_plant_edgetpu.tflite for 2000 inferences
[Bird image analysis] max value index: 659 value: 0.652344
[Plant image analysis] max value index: 1680 value: 0.964844
Using one Edge TPU, # inferences: 2000 costs: 106.278 seconds.

Where the max value index represents the index of the class detected and the value represents the confidence. On these particular pictures, the bird detected is a poecile atricapillus (black-capped chickadee) and the plant is a helianthus annuus (sunflower). The index and the name of each class are available in the inat_bird_labels.txt and inat_plant_labels.txt stored in the edgetpu_cpp_example directory.