This article aims to give the following information:
- How to download and install the latest STM32CubeMP2 Package for the STM32 microprocessor series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP25-Ecosystem-v5.0.2.BETA release[edit source]
- The STM32CubeMP2 Package is delivered through an archive file named unknown revision.
- Download and install the STM32CubeMP2 Package
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.
STM32MP2 Developer Package STM32CubeMP2 Package - v5.0.2.BETA release | |
---|---|
Download |
|
Installation |
cd <working directory path>/Developer-Package
unzip unknown revision
|
Release note |
Details about the content of the STM32CubeMP2Package are available in the STM32CubeMP2/Release_Notes.html file.
|
- The STM32CubeMP2 Package installation directory is in the <Developer Package installation directory> directory, and is named unknown revision:
unknown revision STM32CubeMP2 Package: details in STM32CubeMP2 Package content article ├── Drivers │ ├── BSP BSP drivers for the supported STM32MP2 boards │ │ └── [...] │ ├── CMSIS │ │ └── [...] │ └── STM32MP2xx_HAL_Driver HAL drivers for the supported STM32MP2 devices │ └── [...] ├── _htmresc │ └── [...] ├── License.md ├── Middlewares │ └── [...] ├── package.xml ├── Projects │ ├── STM32CubeProjectsList.html List of examples and applications for STM32CubeMP2 Package │ └── STM32MP257F-EV1 Set of examples and applications → STM32MP25 Evaluation boards │ └── [...] ├── Readme.md ├── Release_Notes.html Release note for STM32CubeMP2 Package └── Utilities └── [...]
2. Archives
[edit source]
This wiki is for the v5 ecosystem releases. For information about the previous ecosystem releases, go through the Wiki archives.