Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 42: | Line 42: | ||
* The '''STM32CubeMP1 Package installation directory''' is in the {{HighlightParam|''<Developer Package installation directory>''}} directory, and is named ''STM32Cube_FW_MP1_V1.6.0'': | * The '''STM32CubeMP1 Package installation directory''' is in the {{HighlightParam|''<Developer Package installation directory>''}} directory, and is named ''STM32Cube_FW_MP1_V1.6.0'': | ||
{{Green|{{EcosystemRelease/Package | revision= | {{Green|{{EcosystemRelease/Package | revision=5.0.0 | package=STM32CubeMP1 | request=path}}}}			{{Highlight|'''STM32CubeMP1 Package''': details in [[STM32CubeMP1 Package#STM32CubeMP1 Package Content|STM32CubeMP1 Package content]] article}} | ||
├── {{Green|Drivers}} | ├── {{Green|Drivers}} | ||
│ ├── {{Green|BSP}}				{{Highlight|BSP drivers for the supported STM32MP1 boards}} | │ ├── {{Green|BSP}}				{{Highlight|BSP drivers for the supported STM32MP1 boards}} |
Revision as of 14:27, 29 August 2023
This article aims to give the following information:
- How to download and install the latest STM32CubeMP1 Package for the STM32 microprocessor series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP15-Ecosystem-v5.0.0 release[edit | edit source]
- The STM32CubeMP1 Package is delivered through an archive file named en.STM32Cube_FW_MP1_V1.6.0.zip.
- Download and install the STM32CubeMP1 Package
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
.
STM32MP1 Developer Package STM32CubeMP1 Package - v5.0.0 release | |
---|---|
Download |
|
Installation |
<working directory path>/Developer-Packagecd
unzip en.STM32Cube_FW_MP1_V1.6.0.zip
|
Release note |
Details about the content of the STM32CubeMP1 Package are available in the STM32Cube_FW_MP1_V1.6.0/Release_Notes.html file.
|
- The STM32CubeMP1 Package installation directory is in the <Developer Package installation directory> directory, and is named STM32Cube_FW_MP1_V1.6.0:
STM32Cube_FW_MP1_V1.6.0 STM32CubeMP1 Package: details in STM32CubeMP1 Package content article ├── Drivers │ ├── BSP BSP drivers for the supported STM32MP1 boards │ │ └── [...] │ ├── CMSIS │ │ └── [...] │ └── STM32MP1xx_HAL_Driver HAL drivers for the supported STM32MP1 devices │ └── [...] ├── _htmresc │ └── [...] ├── License.md ├── Middlewares │ └── [...] ├── package.xml ├── Projects │ ├── STM32CubeProjectsList.html List of examples and applications for STM32CubeMP1 Package │ ├── STM32MP157C-DK2 Set of examples and applications → STM32MP15 Discovery kits │ │ └── [...] │ └── STM32MP157C-EV1 Set of examples and applications → STM32MP15 Evaluation boards │ └── [...] ├── Readme.md ├── Release_Notes.html Release note for STM32CubeMP1 Package └── Utilities └── [...]
2. Archives
[edit | edit source]
This wiki is for the v5 ecosystem releases. For information about the previous ecosystem releases, go through the Wiki archives.