Registered User mNo edit summary Tag: 2017 source edit |
Registered User Tag: 2017 source edit |
||
(6 intermediate revisions by 3 users not shown) | |||
Line 5: | Line 5: | ||
<noinclude> | <noinclude> | ||
This article | |||
{{Warning|To start | This article explains how to assemble the '''STM32MP257x-EV1''' Evaluation boards. It is valid for the {{Board | type=257F-EV1 | name=short}} Evaluation board: the part numbers are specified in the [[STM32MP25 microprocessor#Part number codification|STM32MP25 microprocessor part numbers]] article. | ||
{{Warning|To start the board, it is recommended to go through the corresponding [[:Category:Starter Package|Starter Package]] article.}} | |||
</noinclude> | </noinclude> | ||
The STM32MP257x-EV1 Evaluation | The STM32MP257x-EV1 Evaluation board packages ({{Board | type=257F-EV1 | name=short}}), completed by the B-CAMS-IMX package, include the items listed below. | ||
[[File:STM32MP257x-EV1 split.jpg | 800px| left | link= | '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | [[File:STM32MP257x-EV1 split.jpg | 800px| left| link= | '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | ||
{| | {| | ||
|+ | |+ | ||
Line 18: | Line 19: | ||
| 1 || [[MB1936]] main board | | 1 || [[MB1936]] main board | ||
|- | |- | ||
| 2 || 7” LVDS WSVGA display with touch panel ([[ | | 2 || 7” LVDS WSVGA display with touch panel ([[Display_panels_hardware_components#EDT_ETML0700Z9NDHA_-28LVDS-29|EDT ETML0700Z9NDHA panel]]) (optional) | ||
|- | |- | ||
| 3 || LVDS display cable | | 3 || LVDS display cable (optional) | ||
|- | |- | ||
| 4 || [[MB1854]] board AI camera (not part of STM32MP257x-EV1 Evaluation | | 4 || [[MB1854]] board AI camera (not part of the STM32MP257x-EV1 Evaluation board package; provided with the B-CAMS-IMX package) (optional) | ||
|- | |- | ||
| 5 || | | 5 || Camera board FFC (not part of the STM32MP257x-EV1 Evaluation board package; provided with the B-CAMS-IMX package) (optional) | ||
|} | |} | ||
<br clear=all> | <br clear=all> | ||
[[File: STM32MP257x-EV1_assembly.png| thumb | 800px | center | link= | STM32MP257x-EV1 Evaluation board assembly <br> '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | LVDS displays and CSI cameras are available for purchase to complete this basic setup.<br> | ||
=== | The complete set looks like this: | ||
[[File: STM32MP257x- | |||
[[File: STM32MP257x-EV1_assembly.png| thumb | 800px | center | link= | STM32MP257x-EV1 Evaluation board assembly <br> '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | |||
=== Connecting the LVDS display to the board === | |||
[[File: STM32MP257x-EV1_DisplayBoardAssembly1.jpg| thumb | 800px | center | link= | Display board assembly (picture is not contractual)]] | |||
* Check the cable orientation shown above using the black mark and the white twisted pairs. | |||
* Find the LVDS ports on the STM32MP257x-DK Discovery kit (CN2) and the display (CN1). The LVDS display box contains one cable. | |||
* Insert the cable into each port as shown below: | |||
[[File: STM32MP257x-EV1_DisplayBoardAssembly2.jpg| thumb | 800px | center | link= | Display board assembly (picture is not contractual)]] | |||
=== Connecting the MB1854 camera board to the board === | |||
[[File: STM32MP257x- | [[File: STM32MP257x-EV1_CameraBoardAssembly1.jpg| thumb | 500px | center | link= |Camera board assembly (picture is not contractual)]] | ||
* Find the camera ports on the STM32MP257x-EV1 Evaluation board (CN4) and MB1854 (CN1). One FFC is provided in the camera box. | |||
* Find the | * For each port: | ||
* | ** Pull the black plastic (#1 in the image below) lightly to insert the contact side of the FFC towards the board (#2 in the image below). | ||
** Push the black plastic carefully to hold the FFC (#3 in the image below). | |||
[[File: STM32MP257x- | [[File: STM32MP257x-EV1_CameraBoardAssembly2.jpg| thumb | 800px | center | link= | Camera board assembly (picture is not contractual)]] | ||
===STM32MP257x-EV1 Evaluation board assembled === | ===STM32MP257x-EV1 Evaluation board assembled=== | ||
<br clear=all> | <br clear="all"> | ||
[[File:STM32MP257x-EV1_assembled.jpg| thumb | 700px | center | link= | STM32MP257x-EV1 Evaluation board assembled <br> '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | [[File:STM32MP257x-EV1_assembled.jpg| thumb | 700px | center | link= | STM32MP257x-EV1 Evaluation board assembled <br> '''STM32MP257F-EV1''' shown here (picture is not contractual)]] | ||
<noinclude> | <noinclude> | ||
{{NoIndex}} | {{NoIndex}} | ||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
{{PublicationRequestId | 7572 | {{PublicationRequestId | 33602 | 2025-01-13 | previous: 7572, 2018-06-19, AlainF}} | ||
</noinclude> | </noinclude> |
Latest revision as of 16:56, 28 March 2025
This article explains how to assemble the STM32MP257x-EV1 Evaluation boards. It is valid for the STM32MP257F-EV1 Evaluation board: the part numbers are specified in the STM32MP25 microprocessor part numbers article.
The STM32MP257x-EV1 Evaluation board packages (STM32MP257F-EV1 ), completed by the B-CAMS-IMX package, include the items listed below.

Position | Description |
---|---|
1 | MB1936 main board |
2 | 7” LVDS WSVGA display with touch panel (EDT ETML0700Z9NDHA panel) (optional) |
3 | LVDS display cable (optional) |
4 | MB1854 board AI camera (not part of the STM32MP257x-EV1 Evaluation board package; provided with the B-CAMS-IMX package) (optional) |
5 | Camera board FFC (not part of the STM32MP257x-EV1 Evaluation board package; provided with the B-CAMS-IMX package) (optional) |
LVDS displays and CSI cameras are available for purchase to complete this basic setup.
The complete set looks like this:
1. Connecting the LVDS display to the board[edit | edit source]
- Check the cable orientation shown above using the black mark and the white twisted pairs.
- Find the LVDS ports on the STM32MP257x-DK Discovery kit (CN2) and the display (CN1). The LVDS display box contains one cable.
- Insert the cable into each port as shown below:
2. Connecting the MB1854 camera board to the board[edit | edit source]
- Find the camera ports on the STM32MP257x-EV1 Evaluation board (CN4) and MB1854 (CN1). One FFC is provided in the camera box.
- For each port:
- Pull the black plastic (#1 in the image below) lightly to insert the contact side of the FFC towards the board (#2 in the image below).
- Push the black plastic carefully to hold the FFC (#3 in the image below).
3. STM32MP257x-EV1 Evaluation board assembled[edit | edit source]