deleted>Frq07399 mNo edit summary |
Registered User No edit summary |
||
(5 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
{{ApplicableFor | |||
{{ | |MPUs list=STM32MP13x, STM32MP15x, STM32MP25x | ||
|MPUs checklist=STM32MP13x, STM32MP15x, STM32MP25x | |||
}} | |||
<noinclude></noinclude> | |||
</noinclude> | |||
'''OpenSTLinux filesystem''' follows the Standard Linux<sup>®</sup> filesystem, represented on the below diagram. | '''OpenSTLinux filesystem''' follows the Standard Linux<sup>®</sup> filesystem, represented on the below diagram. | ||
Line 15: | Line 13: | ||
:- [[Pseudo filesystem]] which manages volatile data linked to the current running session | :- [[Pseudo filesystem]] which manages volatile data linked to the current running session | ||
The Virtual File System<ref>{{CodeSource | Linux kernel | Documentation/filesystems/vfs. | The Virtual File System<ref>{{CodeSource | Linux kernel | Documentation/filesystems/vfs.rst}}</ref> is a Linux core feature which proposes an abstraction layer for the Linux user space. | ||
{{ImageMap|Image: OpenSTLinux filesystem overview.png{{!}} thumb{{!}} 800px {{!}} center {{!}} OpenSTLinux filesystem overview | {{ImageMap|Image: OpenSTLinux filesystem overview.png{{!}} thumb{{!}} 800px {{!}} center {{!}} OpenSTLinux filesystem overview | ||
rect 192 15 950 144 [[File Hierarchy Standard (FHS)]] | rect 192 15 950 144 [[File Hierarchy Standard (FHS)]] | ||
rect 575 214 950 334 [[Pseudo filesystem]] | rect 575 214 950 334 [[Pseudo filesystem]] | ||
Line 27: | Line 25: | ||
== References == | == References == | ||
<references /> | <references /> | ||
<noinclude> | |||
{{NoIndex}} | |||
{{PublicationRequestId | 10266 | 2019-01-10 | AlainF}} | |||
[[Category:Sub-articles]] | |||
</noinclude> |
Latest revision as of 08:56, 5 June 2024
OpenSTLinux filesystem follows the Standard Linux® filesystem, represented on the below diagram.
It is based on the File Hierarchy Standard (FHS) at user space level.
Template:Highlight, by using two paths:
- - Filesystem layers which are associated to a device (with both block and raw interfaces), and which manage persistent data
- - Pseudo filesystem which manages volatile data linked to the current running session
The Virtual File System[1] is a Linux core feature which proposes an abstraction layer for the Linux user space.
1. References[edit | edit source]