1. Usage[edit source]
The CodeSource template is used to indicate the URL of any file from the software components (e.g., Linux® kernel, STM32Cube MPU Packages, BSP layers...) used in this wiki.
<domain> | repo=<repo> | <path> | <link text> | <version>}}Usage: {{CodeSource |
Where (lists below should be inline with https://github.com/STMicroelectronics/STM32MPU_EmbSW_Overall_Offer):
- <domain> is the mandatory string that identifies the domain (a.ka., software component) of the file. The possible values are given in the below table:
<domain> | Comment |
---|---|
Linux kernel | the file belongs to the Linux kernel domain. |
U-Boot | the file belongs to the U-Boot domain. |
TF-A | the file belongs to the TF-A domain. |
OP-TEE_OS | the file belongs to the OP-TEE OS domain. |
optee-stm32mp-addons | the file belongs to the optee-stm32mp-addons layer. |
External_DT | the file belongs to the external device tree domain. |
STM32CubeMP1 | the file belongs to the STM32CubeMP1 domain. |
STM32CubeMP13 | the file belongs to the STM32CubeMP13 domain. |
STM32CubeMP2 | the file belongs to the STM32CubeMP2 domain. |
STM32CubeMP1htlm | the file belongs to the STM32CubeMP1 domain and we want to make readable an html file directly into github, without downloading the file. |
STM32CubeMP13html | the file belongs to the STM32CubeMP13 domain and we want to make readable an html file directly into github, without downloading the file. |
STM32CubeMP2html | the file belongs to the STM32CubeMP2 domain and we want to make readable an html file directly into github, without downloading the file. |
TF-M | the file belongs to the TF-M domain. |
TF-M_tests | the file belongs to the TF-M Tests domain. |
STM32DDRFW-UTIL | the file belongs to the STM32DDRFW-UTIL domain. |
STM32PRGFW-UTIL | the file belongs to the STM32PRGFW-UTIL domain. |
STM32PRGFW-UTILhtml | the file belongs to the STM32PRGFW-UTILdomain and we want to make readable an html file directly into github, without downloading the file. |
meta-st-stm32mp | the file belongs to the meta-st-stm32mp BSP layer domain. |
meta-st-stm32mp-addons | the file belongs to the meta-st-stm32mp-addons BSP layer domain. |
meta-st-openstlinux | the file belongs to the meta-st-openstlinux framework layer domain. |
wiki-stm32mp-addons | the file belongs to the wiki-stm32mp-addons domain, wiki-stm32mp-addons has been created to provide to customer some example of scripts, ... |
Android | the file belongs to the Android domain. |
Buildroot | the file belongs to the Buildroot domain. |
X-LINUX-AI | the file belongs to the X-LINUX-AI expansion package domain. |
X-LINUX-ISP | the file belongs to the X-LINUX-ISP expansion package domain. |
st-openstlinux-application | the file belongs to the st-openstlinux-application domain. |
- <path> is the optional relative path of the file from the root URL of the domain. If this parameter is omitted, then the root URL of the domain is returned (e.g., https://github.com/STMicroelectronics/linux.git), and all other parameters are ignored. If the file is a directory (e.g. "arch/arm/boot/dts" directory for the Linux kernel), this parameter must end with the slash
/
character (e.g. "arch/arm/boot/dts/"). To point to the root URL of the domain, this parameter must be the slash/
character. The root URLs are:
- <repo> is the mandatory repository in the Google Android git. This named parameter is ignored for all other domains than Android.
- <link text> is an optional link text (text that is displayed instead of the URL).
- <version> is an optional version number (branch or tag) if the default one doesn't fit. Per default, the URL points to the versions indicated in the below table:
<domain> | <version> | Alternatives |
---|---|---|
Linux kernel | default: v6.1-stm32mp branch |
|
U-Boot | default: v2022.10-stm32mp branch |
|
TF-A | default: v2.8-stm32mp branch |
|
OP-TEE_OS | default: 3.19.0-stm32mp branch |
|
optee-stm32mp-addons | default: 3.16.0-stm32mp-r1 tag | |
External_DT | default: v5.0-stm32mp branch | |
STM32CubeMP1 | default: master branch | |
STM32CubeMP13 | default: main branch | |
STM32CubeMP2 | default: main branch | |
TF-M | default : v1.7.0-stm32mp25-r9.1 tag | |
TF-M_tests | default: v1.7.0-stm32mp25-r6 tag |
|
STM32DDRFW-UTIL | default: main branch | |
STM32PRGFW-UTIL | default: main branch | |
meta-st-stm32mp | default: mickledore branch | |
meta-st-stm32mp-addons | default: mickledore branch | |
meta-st-openstlinux | default: mickledore branch | |
wiki-stm32mp-addons | default: main branch | |
Android | default: android-13.0.0_r82 | |
Buildroot | default: st/2024.02.3 branch | |
X-LINUX-AI | default: v5.1.0 tag | |
X-LINUX-ISP | default: v5.0.0 tag | |
st-openstlinux-application | default: main branch |
2. Basic examples[edit source]
You type | You get |
---|---|
Linux kernel
Linux kernel | Makefile}}<br /> 2- {{CodeSource | Linux kernel | arch/arm/boot/dts/}}<br /> 3- {{CodeSource | Linux kernel | /}}<br /> 4- {{CodeSource | Linux kernel}}<br />1- {{CodeSource | |
1- Makefile |
U-Boot
U-Boot | Makefile}}<br /> 2- {{CodeSource | U-Boot | arch/arm/dts/}}<br /> 3- {{CodeSource | U-Boot | /}}<br /> 4- {{CodeSource | U-Boot}}<br />1- {{CodeSource | |
1- Makefile |
TF-A
TF-A | Makefile}}<br /> 2- {{CodeSource | TF-A | fdts/}}<br /> 3- {{CodeSource | TF-A | /}}<br /> 4- {{CodeSource | TF-A}}<br />1- {{CodeSource | |
1- Makefile |
OP-TEE_OS
OP-TEE_OS | Makefile}}<br /> 2- {{CodeSource | OP-TEE_OS | core/arch/arm/kernel/}}<br /> 3- {{CodeSource | OP-TEE_OS | /}}<br /> 4- {{CodeSource | OP-TEE_OS}}<br />1- {{CodeSource | |
1- Makefile |
optee-stm32mp-addons
1- {{CodeSource | optee-stm32mp-addons | README.md}}<br />
2- {{CodeSource | optee-stm32mp-addons | stm32mp-calibration/}}<br />
3- {{CodeSource | optee-stm32mp-addons | /}}<br />
4- {{CodeSource | optee-stm32mp-addons}}<br />
|
1- README.md |
External_DT
DT | linux/Makefile}}<br /> 2- {{CodeSource | External_DT | linux/}}<br /> 3- {{CodeSource | External_DT | /}}<br /> 4- {{CodeSource | External_DT}}<br />1- {{CodeSource | External_ |
1- linux/Makefile |
STM32CubeMP1
HAL_Driver/Src/}}<br /> 3- {{CodeSource | STM32CubeMP1 | /}}<br /> 4- {{CodeSource | STM32CubeMP1html | Release_Notes.html}}<br /> 5- {{CodeSource | STM32CubeMP1}}<br />1- {{CodeSource | STM32CubeMP1 | Readme.md}}<br /> 2- {{CodeSource | STM32CubeMP1 | Drivers/STM32MP1xx_ |
1- Readme.md |
STM32CubeMP13
BSP/STM32MP13xx_DISCO/}}<br /> 3- {{CodeSource | STM32CubeMP13 | /}}<br /> 4- {{CodeSource | STM32CubeMP13 |Projects/STM32CubeProjectsList.html}}<br /> 5- {{CodeSource | STM32CubeMP13html |Projects/STM32CubeProjectsList.html}}<br /> 6- {{CodeSource | STM32CubeMP13}}<br />1- {{CodeSource | STM32CubeMP13 | Readme.md}}<br /> 2- {{CodeSource | STM32CubeMP13 |Drivers/ |
1- Readme.md |
STM32CubeMP2
HAL_Driver/Src/}}<br /> 3- {{CodeSource | STM32CubeMP2 | /}}<br /> 4- {{CodeSource | STM32CubeMP2}}<br /> 5- {{CodeSource |STM32CubeMP2html |Projects/STM32CubeProjectsList.html}}<br />1- {{CodeSource | STM32CubeMP2 | README.md}}<br /> 2- {{CodeSource | STM32CubeMP2 | Drivers/STM32MP2xx_ |
1- README.md |
TF-M
1- {{CodeSource | TF-M | readme.rst}}<br />
2- {{CodeSource | TF-M | bl1/config/}}<br />
3- {{CodeSource | TF-M | /}}<br />
4- {{CodeSource | TF-M}}<br />
|
1- readme.rst |
TF-M_tests
1- {{CodeSource | TF-M_tests | readme.rst}}<br />
2- {{CodeSource | TF-M_tests | test/bl2/}}<br />
3- {{CodeSource | TF-M_tests | /}}<br />
4- {{CodeSource | TF-M_tests}}<br />
|
1- readme.rst |
STM32DDRFW-UTIL
HAL_Driver/Src/}}<br /> 3- {{CodeSource | STM32DDRFW-UTIL | /}}<br /> 4- {{CodeSource | STM32DDRFW-UTIL}}<br />1- {{CodeSource | STM32DDRFW-UTIL | README.md}}<br /> 2- {{CodeSource | STM32DDRFW-UTIL | Drivers/STM32MP2xx_ |
1- README.md |
STM32PRGFW-UTIL
HAL_Driver/Src/}}<br /> 3- {{CodeSource | STM32PRGFW-UTIL | /}}<br /> 4- {{CodeSource | STM32PRGFW-UTIL }}<br />1- {{CodeSource | STM32PRGFW-UTIL | README.md}}<br /> 2- {{CodeSource | STM32PRGFW-UTIL | Drivers/STM32MP2xx_ |
1- README.md |
meta-st-stm32mp
1- {{CodeSource | meta-st-stm32mp | README.md}}<br />
2- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/}}<br />
3- {{CodeSource | meta-st-stm32mp | /}}<br />
4- {{CodeSource | meta-st-stm32mp}}<br />
|
1- README.md |
meta-st-openstlinux
1- {{CodeSource | meta-st-openstlinux | README.md}}<br />
2- {{CodeSource | meta-st-openstlinux | recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad/}}<br />
3- {{CodeSource | meta-st-openstlinux | /}}<br />
4- {{CodeSource | meta-st-openstlinux}}<br />
|
1- README.md |
meta-st-stm32mp-addons
1- {{CodeSource | meta-st-stm32mp-addons | README.md}}<br />
2- {{CodeSource | meta-st-stm32mp-addons | recipes-kernel/linux/}}<br />
3- {{CodeSource | meta-st-stm32mp-addons | /}}<br />
4- {{CodeSource | meta-st-stm32mp-addons}}<br />
|
1- README.md |
wiki-stm32mp-addons
1- {{CodeSource | wiki-stm32mp-addons | README.md}}<br />
2- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/}}<br />
3- {{CodeSource | wiki-stm32mp-addons | /}}<br />
4- {{CodeSource | wiki-stm32mp-addons}}<br />
|
1- README.md |
Android
1- {{CodeSource | Android | repo=platform/build | README.md}}<br />
2- {{CodeSource | Android | repo=platform/packages/apps/Settings | src/com/android/settings/}}<br />
3- {{CodeSource | Android | repo=platform/build | /}}<br />
4- {{CodeSource | Android}| repo=platform/build}<br />
|
1- platform/build/README.md |
Buildroot
1- {{CodeSource | Buildroot | README.md}}<br />
2- {{CodeSource | Buildroot | docs/}}<br />
3- {{CodeSource | Buildroot | /}}<br />
4- {{CodeSource | Buildroot }}<br />
|
1- README.md |
X-LINUX-AI
AI | README.md}}<br /> 2- {{CodeSource | X-LINUX-AI | conf/}}<br /> 3- {{CodeSource | X-LINUX-AI | /}}<br /> 4- {{CodeSource | X-LINUX-AI}}<br />1- {{CodeSource | X-LINUX- |
1- README.md |
X-LINUX-ISP
ISP| README.md}}<br /> 2- {{CodeSource | X-LINUX-ISP| conf/}}<br /> 3- {{CodeSource | X-LINUX-ISP| /}}<br /> 4- {{CodeSource | X-LINUX-ISP}}<br />1- {{CodeSource | X-LINUX- |
1- README.md |
st-openstlinux-application
1- {{CodeSource | st-openstlinux-application | README.md}}<br />
2- {{CodeSource | st-openstlinux-application | dcmipp-isp-ctrl/}}<br />
3- {{CodeSource | st-openstlinux-application | /}}<br />
4- {{CodeSource | st-openstlinux-application}}<br />
5- {{CodeSource | st-openstlinux-application | weston-cube/}}<br />
|
1- README.md |
3. More examples[edit source]
You type | You get |
---|---|
Linux kernel: regular file
Linux kernel | Makefile}}<br /> 2- {{CodeSource | Linux kernel | Makefile | Linux kernel root makefile - Makefile}}<br /> 3- {{CodeSource | Linux kernel | Makefile | | 4.19}}<br /> 4- {{CodeSource | Linux kernel | Makefile | Linux kernel root makefile - Makefile | 4.19}}<br /> 5- {{CodeSource | Linux kernel | repo=ignored | Makefile | Linux kernel root makefile - Makefile | 4.19}}<br />1- {{CodeSource | |
1- Makefile |
Linux kernel: directory
Linux kernel | arch/arm/boot/dts/}}<br /> 2- {{CodeSource | Linux kernel | arch/arm/boot/dts/ | arch/arm/boot/dts/stm32mp15*}}<br /> 3- {{CodeSource | Linux kernel | arch/arm/boot/dts/ | | 4.19}}<br /> 4- {{CodeSource | Linux kernel | arch/arm/boot/dts/ | arch/arm/boot/dts/stm32mp15* | 4.19}}<br /> 5- {{CodeSource | Linux kernel | arch/arm/boot/dts/ | repo=ignored | arch/arm/boot/dts/stm32mp15* | 4.19}}<br />1- {{CodeSource | |
1- arch/arm/boot/dts/ |
U-Boot: regular file
U-Boot | Makefile}}<br /> 2- {{CodeSource | U-Boot | Makefile | U-Boot root makefile - Makefile}}<br /> 3- {{CodeSource | U-Boot | Makefile | | 2018.03}}<br /> 4- {{CodeSource | U-Boot | Makefile | U-Boot root makefile - Makefile | 2018.03}}<br /> 5- {{CodeSource | U-Boot | Makefile | U-Boot root makefile - Makefile | repo=ignored | 2018.03}}<br />1- {{CodeSource | |
1- Makefile |
U-Boot: directory
U-Boot | arch/arm/dts/}}<br /> 2- {{CodeSource | U-Boot | arch/arm/dts/ | arch/arm/dts/stm32mp15*}}<br /> 3- {{CodeSource | U-Boot | arch/arm/dts/ | | 2018.03}}<br /> 4- {{CodeSource | U-Boot | arch/arm/dts/ | arch/arm/dts/stm32mp15* | 2018.03}}<br /> 5- {{CodeSource | repo=ignored | U-Boot | arch/arm/dts/ | arch/arm/dts/stm32mp15* | 2018.03}}<br />1- {{CodeSource | |
1- arch/arm/dts/ |
TF-A: regular file
TF-A | Makefile}}<br /> 2- {{CodeSource | TF-A | Makefile | TF-A root makefile - Makefile}}<br /> 3- {{CodeSource | TF-A | Makefile | | 1.4}}<br /> 4- {{CodeSource | TF-A | Makefile | TF-A root makefile - Makefile | 1.4}}<br /> 5- {{CodeSource | TF-A | repo=ignored | Makefile}}<br />1- {{CodeSource | |
1- Makefile |
TF-A: directory
TF-A | fdts/}}<br /> 2- {{CodeSource | TF-A | fdts/ | fdts/stm32mp15*}}<br /> 3- {{CodeSource | TF-A | fdts/ | | 1.4}}<br /> 4- {{CodeSource | TF-A | fdts/ | fdts/stm32mp15* | 1.4}}<br /> 5- {{CodeSource | TF-A | repo=ignored | fdts/ | fdts/stm32mp15*}}<br />1- {{CodeSource | |
1- fdts/ |
OP-TEE_OS: regular file
OP-TEE_OS | Makefile}}<br /> 2- {{CodeSource | OP-TEE_OS | Makefile | OP-TEE OS root makefile - Makefile}}<br /> 3- {{CodeSource | OP-TEE_OS | Makefile | | 3.0.0}}<br /> 4- {{CodeSource | OP-TEE_OS | Makefile | OP-TEE OS root makefile - Makefile | 3.0.0}}<br /> 5- {{CodeSource | OP-TEE_OS | Makefile | 3.0.0 | repo=ignored}}<br />1- {{CodeSource | |
1- Makefile |
OP-TEE_OS: directory
OP-TEE_OS | core/arch/arm/kernel/}}<br /> 2- {{CodeSource | OP-TEE_OS | core/arch/arm/kernel/ | core/arch/arm/kernel/*}}<br /> 3- {{CodeSource | OP-TEE_OS | core/arch/arm/kernel/ | | 3.0.0}}<br /> 4- {{CodeSource | OP-TEE_OS | core/arch/arm/kernel/ | core/arch/arm/kernel/* | 3.0.0}}<br /> 5- {{CodeSource | OP-TEE_OS | repo=ignored | core/arch/arm/kernel/ | 3.0.0}}<br />1- {{CodeSource | |
1- core/arch/arm/kernel/ |
optee-stm32mp-addons: regular file
OP-TEE add-ons makefile - Makefile}}<br /> 3- {{CodeSource | optee-stm32mp-addons | Makefile | | master}}<br /> 4- {{CodeSource | optee-stm32mp-addons | Makefile | OP-TEE add-ons makefile - Makefile | master}}<br /> 5- {{CodeSource | optee-stm32mp-addons | Makefile | | master | repo=ignored}}<br />1- {{CodeSource | optee-stm32mp-addons | Makefile}}<br /> 2- {{CodeSource | optee-stm32mp-addons | Makefile | |
1- Makefile |
optee-stm32mp-addons: directory
1- {{CodeSource | optee-stm32mp-addons | stm32mp-calibration/host/}}<br />
2- {{CodeSource | optee-stm32mp-addons | stm32mp-calibration/host/ | stm32mp-calibration/host/*}}<br />
3- {{CodeSource | optee-stm32mp-addons | stm32mp-calibration/host/ | | master}}<br />
4- {{CodeSource | optee-stm32mp-addons | stm32mp-calibration/host/ | stm32mp-calibration/host/* | master}}<br />
5- {{CodeSource | optee-stm32mp-addons | repo=ignored | stm32mp-calibration/host/ | master}}<br />
|
1- stm32mp-calibration/host/ |
External_DT: regular file
DT | linux/Makefile}}<br /> 2- {{CodeSource | External_DT | linux/Makefile | External DT Linux makefile - Makefile}}<br /> 3- {{CodeSource | External_DT | linux/Makefile | | 5.0-stm32mp-r1-rc9}}<br /> 4- {{CodeSource | External_DT | linux/Makefile | External DT Linux - Makefile | 5.0-stm32mp-r1-rc9}}<br /> 5- {{CodeSource | External_DT | repo=ignored | linux/Makefile}}<br />1- {{CodeSource | External_ |
1- linux/Makefile |
External_DT: directory
DT | linux/}}<br /> 2- {{CodeSource | External_DT | linux/ | linux/stm32mp25*}}<br /> 3- {{CodeSource | External_DT | linux/ | | 5.0-stm32mp-r1-rc9}}<br /> 4- {{CodeSource | External_DT| linux/ | linux/stm32mp25* | 5.0-stm32mp-r1-rc9}}<br /> 5- {{CodeSource | External_DT | repo=ignored | linux/ | linux/stm32mp25*}}<br />1- {{CodeSource | External_ |
1- linux/ |
STM32CubeMP1: regular file
1- {{CodeSource | STM32CubeMP1 | Readme.md}}<br />
2- {{CodeSource | STM32CubeMP1 | Readme.md | STM32CubeMP1 readme}}<br />
3- {{CodeSource | STM32CubeMP1 | Readme.md | | master}}<br />
4- {{CodeSource | STM32CubeMP1 | Readme.md | STM32CubeMP1 readme | master}}<br />
5- {{CodeSource | STM32CubeMP1 | Readme.md | STM32CubeMP1 readme | repo=ignored | master}}<br />
|
1- Readme.md |
STM32CubeMP1: directory
HAL_Driver/Src/}}<br /> 2- {{CodeSource | STM32CubeMP1 | Drivers/STM32MP1xx_HAL_Driver/Src/ | Drivers/STM32MP1xx_HAL_Driver/Src/*}}<br /> 3- {{CodeSource | STM32CubeMP1 | Drivers/STM32MP1xx_HAL_Driver/Src/ | | master}}<br /> 4- {{CodeSource | STM32CubeMP1 | Drivers/STM32MP1xx_HAL_Driver/Src/ | Drivers/STM32MP1xx_HAL_Driver/Src/* | master}}<br /> 5- {{CodeSource | STM32CubeMP1 | repo=ignored | Drivers/STM32MP1xx_HAL_Driver/Src/}}<br />1- {{CodeSource | STM32CubeMP1 | Drivers/STM32MP1xx_ |
1- Drivers/STM32MP1xx_HAL_Driver/Src/ |
STM32CubeMP2: regular file
1- {{CodeSource | STM32CubeMP2 | README.md}}<br />
2- {{CodeSource | STM32CubeMP2 | README.md | STM32CubeMP2 readme}}<br />
3- {{CodeSource | STM32CubeMP2 | README.md | | 0.2.0}}<br />
4- {{CodeSource | STM32CubeMP2 | README.md | STM32CubeMP2 readme | 0.2.0}}<br />
5- {{CodeSource | STM32CubeMP2 | README.md | STM32CubeMP2 readme | repo=ignored | 0.2.0}}<br />
|
1- README.md |
STM32CubeMP2: directory
HAL_Driver/Src/}}<br /> 2- {{CodeSource | STM32CubeMP2 | Drivers/STM32MP2xx_HAL_Driver/Src/ | Drivers/STM32MP2xx_HAL_Driver/Src/*}}<br /> 3- {{CodeSource | STM32CubeMP2 | Drivers/STM32MP2xx_HAL_Driver/Src/ | | 0.2.0}}<br /> 4- {{CodeSource | STM32CubeMP2 | Drivers/STM32MP2xx_HAL_Driver/Src/ | Drivers/STM32MP2xx_HAL_Driver/Src/* | 0.2.0}}<br /> 5- {{CodeSource | STM32CubeMP2 | repo=ignored | Drivers/STM32MP2xx_HAL_Driver/Src/}}<br />1- {{CodeSource | STM32CubeMP2 | Drivers/STM32MP2xx_ |
1- Drivers/STM32MP2xx_HAL_Driver/Src/ |
TF-M: regular file
1- {{CodeSource | TF-M | readme.rst}}<br />
2- {{CodeSource | TF-M | readme.rst | TF-M readme}}<br />
3- {{CodeSource | TF-M | readme.rst | | 1.7.0-stm32mp25-r6}}<br />
4- {{CodeSource | TF-M | readme.rst | TF-M readme | 1.7.0-stm32mp25-r6}}<br />
5- {{CodeSource | TF-M | readme.rst | TF-M readme | repo=ignored | 1.7.0-stm32mp25-r6}}<br />
|
1- readme.rst |
TF-M: directory
1- {{CodeSource | TF-M | bl1/config/}}<br />
2- {{CodeSource | TF-M | bl1/config/ | bl1/config/*}}<br />
3- {{CodeSource | TF-M | bl1/config/ | | 1.7.0-stm32mp25-r6}}<br />
4- {{CodeSource | TF-M | bl1/config/ | bl1/config/* | 1.7.0-stm32mp25-r6}}<br />
5- {{CodeSource | TF-M | repo=ignored | bl1/config/}}<br />
|
1- bl1/config/ |
TF-M_tests: regular file
1- {{CodeSource | TF-M_tests | readme.rst}}<br />
2- {{CodeSource | TF-M_tests | readme.rst | TF-M readme}}<br />
3- {{CodeSource | TF-M_tests | readme.rst | | 1.7.0-stm32mp25-r6}}<br />
4- {{CodeSource | TF-M_tests | readme.rst | TF-M readme | 1.7.0-stm32mp25-r6}}<br />
5- {{CodeSource | TF-M_tests | readme.rst | TF-M readme | repo=ignored | 1.7.0-stm32mp25-r6}}<br />
|
1- readme.rst |
TF-M_tests: directory
1- {{CodeSource | TF-M_tests | test/bl2/}}<br />
2- {{CodeSource | TF-M_tests | test/bl2/ | test/bl2/*}}<br />
3- {{CodeSource | TF-M_tests | test/bl2/ | | 1.7.0-stm32mp25-r6}}<br />
4- {{CodeSource | TF-M_tests | test/bl2/ | test/bl2/* | 1.7.0-stm32mp25-r6}}<br />
5- {{CodeSource | TF-M_tests | repo=ignored | test/bl2/}}<br />
|
1- test/bl2/ |
STM32DDRFW-UTIL: regular file
1- {{CodeSource | STM32DDRFW-UTIL | README.md}}<br />
2- {{CodeSource | STM32DDRFW-UTIL | README.md | STM32DDRFW-UTIL readme}}<br />
3- {{CodeSource | STM32DDRFW-UTIL | README.md | | 1.0.0}}<br />
4- {{CodeSource | STM32DDRFW-UTIL | README.md | STM32DDRFW-UTIL readme | 1.0.0}}<br />
5- {{CodeSource | STM32DDRFW-UTIL | README.md | STM32DDRFW-UTIL readme | repo=ignored | 1.0.0}}<br />
|
1- README.md |
STM32DDRFW-UTIL: directory
BSP/}}<br /> 2- {{CodeSource | STM32DDRFW-UTIL | Drivers/BSP/ | Drivers/BSP/*}}<br /> 3- {{CodeSource | STM32DDRFW-UTIL | Drivers/BSP/ | | 1.0.0}}<br /> 4- {{CodeSource | STM32DDRFW-UTIL | Drivers/BSP/ | Drivers/BSP/* | 1.0.0}}<br /> 5- {{CodeSource | STM32DDRFW-UTIL | repo=ignored | Drivers/BSP/}}<br />1- {{CodeSource | STM32DDRFW-UTIL | Drivers/ |
1- Drivers/BSP/ |
STM32PRGFW-UTIL: regular file
1- {{CodeSource | STM32PRGFW-UTIL | README.md}}<br />
2- {{CodeSource | STM32PRGFW-UTIL | README.md | STM32PRGFW-UTIL readme}}<br />
3- {{CodeSource | STM32PRGFW-UTIL | README.md | | 1.0.3}}<br />
4- {{CodeSource | STM32PRGFW-UTIL | README.md | STM32PRGFW-UTIL readme | 1.0.3}}<br />
5- {{CodeSource | STM32PRGFW-UTIL | README.md | STM32PRGFW-UTIL readme | repo=ignored | 1.0.3}}<br />
|
1- README.md |
STM32PRGFW-UTIL: directory
BSP/}}<br /> 2- {{CodeSource | STM32PRGFW-UTIL | Drivers/BSP/ | Drivers/BSP/*}}<br /> 3- {{CodeSource | STM32PRGFW-UTIL | Drivers/BSP/ | | 1.0.3}}<br /> 4- {{CodeSource | STM32PRGFW-UTIL | Drivers/BSP/ | Drivers/BSP/* | 1.0.3}}<br /> 5- {{CodeSource | STM32PRGFW-UTIL | repo=ignored | Drivers/BSP/}}<br />1- {{CodeSource | STM32PRGFW-UTIL | Drivers/ |
1- Drivers/BSP/ |
meta-st-stm32mp: regular file
Linux build}}<br /> 3- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt | |openstlinux-4.19-thud-mp1-19-02-20}}<br /> 4- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt | Helper file for Linux build | thud}}<br /> 5- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt | Helper file for Linux build | repo=ignored | thud}}<br />1- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt}}<br /> 2- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt | Helper file for |
1- recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt |
meta-st-stm32mp: directory
1- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/}}<br />
2- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/ | recipes-kernel/linux/linux-stm32mp/}}<br />
3- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/ | | thud}}<br />
4- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/ | recipes-kernel/linux/linux-stm32mp/ | thud}}<br />
5- {{CodeSource | meta-st-stm32mp | recipes-kernel/linux/linux-stm32mp/ | recipes-kernel/linux/linux-stm32mp/ | repo=ignored | thud}}<br />
|
1- recipes-kernel/linux/linux-stm32mp/ |
meta-st-openstlinux: regular file
1- {{CodeSource | meta-st-openstlinux | README.md}}<br />
2- {{CodeSource | meta-st-openstlinux | README.md | meta-st-openstlinux readme}}<br />
3- {{CodeSource | meta-st-openstlinux | README.md | | thud}}<br />
4- {{CodeSource | meta-st-openstlinux | README.md | meta-st-openstlinux readme | thud}}<br />
5- {{CodeSource | meta-st-openstlinux | README.md | meta-st-openstlinux readme | repo=ignored | thud}}<br />
|
1- README.md |
meta-st-openstlinux: directory
1- {{CodeSource | meta-st-openstlinux | recipes-multimedia/gstreamer/}}<br />
2- {{CodeSource | meta-st-openstlinux | recipes-multimedia/gstreamer/ | GStreamer recipes}}<br />
3- {{CodeSource | meta-st-openstlinux | recipes-multimedia/gstreamer/ | |openstlinux-4.19-thud-mp1-19-02-20}}<br />
4- {{CodeSource | meta-st-openstlinux | recipes-multimedia/gstreamer/ | GStreamer recipes | thud}}<br />
5- {{CodeSource | meta-st-openstlinux | recipes-multimedia/gstreamer/ | GStreamer recipes | repo=ignored | thud}}<br />
|
1- recipes-multimedia/gstreamer/ |
meta-st-stm32mp-addons: regular file
1- {{CodeSource | meta-st-stm32mp-addons | docs/How_to_create_a_custom_machine_mx.txt}}<br />
2- {{CodeSource | meta-st-stm32mp-addons | docs/How_to_create_a_custom_machine_mx.txt | Helper file for creating a custom machine}}<br />
3- {{CodeSource | meta-st-stm32mp-addons | docs/How_to_create_a_custom_machine_mx.txt | |openstlinux-4.19-thud-mp1-19-02-20}}<br />
4- {{CodeSource | meta-st-stm32mp-addons | docs/How_to_create_a_custom_machine_mx.txt | Helper file for creating a custom machine | thud }}<br />
5- {{CodeSource | meta-st-stm32mp-addons | docs/How_to_create_a_custom_machine_mx.txt | Helper file for creating a custom machine | repo=ignored | thud }}<br />
|
1- docs/How_to_create_a_custom_machine_mx.txt |
meta-st-stm32mp-addons: directory
1- {{CodeSource | meta-st-stm32mp-addons | recipes-kernel/linux/ }}<br />
2- {{CodeSource | meta-st-stm32mp-addons | recipes-kernel/linux/ | recipes-kernel/linux/}}<br />
3- {{CodeSource | meta-st-stm32mp-addons | recipes-kernel/linux/ | | thud}}<br />
4- {{CodeSource | meta-st-stm32mp-addons | recipes-kernel/linux/ | recipes-kernel/linux/ | thud}}<br />
5- {{CodeSource | meta-st-stm32mp-addons | recipes-kernel/linux/ | recipes-kernel/linux/ | repo=ignored | thud}}<br />
|
1- recipes-kernel/linux/ |
wiki-stm32mp-addons: regular file
GDB setup}}<br /> 3- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/Setup.gdb | | 4.0.0}}<br /> 4- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/Setup.gdb | GDB setup | 4.0.0 }}<br /> 5- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/Setup.gdb | GDB setup | repo=ignored | 4.0.0 }}<br />1- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/Setup.gdb}}<br /> 2- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/Setup.gdb | |
1- gdb-scripts/Setup.gdb |
wiki-stm32mp-addons: directory
GDB scripts}}<br /> 3- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/ | | 4.0.0}}<br /> 4- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/ | GDB scripts | 4.0.0 }}<br /> 5- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/ | GDB scripts | repo=ignored | 4.0.0 }}<br />1- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/}}<br /> 2- {{CodeSource | wiki-stm32mp-addons | gdb-scripts/ | |
1- gdb-scripts/ |
Android: regular file
1- {{CodeSource | Android | repo=platform/build | core/main.mk}}<br />
2- {{CodeSource | Android | repo=platform/build | core/main.mk | Main configuration}}<br />
3- {{CodeSource | Android | repo=platform/build | core/main.mk | | android-8.1.0_r66}}<br />
4- {{CodeSource | Android | repo=platform/build | core/main.mk | Main configuration | android-8.1.0_r66}}<br />
5- {{CodeSource | Android | core/main.mk}}
|
1- platform/build/core/main.mk |
Android: directory
1- {{CodeSource | Android | repo=platform/build | target/product/}}<br />
2- {{CodeSource | Android | repo=platform/build | target/product/ | platform/build/target/product/*}}<br />
3- {{CodeSource | Android | repo=platform/build | target/product/ | | android-8.1.0_r66}}<br />
4- {{CodeSource | Android | repo=platform/build | target/product/ | platform/build/target/product/* | android-8.1.0_r66}}<br />
5- {{CodeSource | Android | target/product/}}<br />
|
1- platform/build/target/product/ |
Buildroot: regular file
1- {{CodeSource | Buildroot | README.md}}<br />
2- {{CodeSource | Buildroot | README.md | STM32MP1 Buildroot external tree}}<br />
3- {{CodeSource | Buildroot | README.md | | st/2021.02}}<br />
4- {{CodeSource | Buildroot | README.md | STM32MP1 Buildroot external tree | st/2021.02}}<br />
5- {{CodeSource | Buildroot | repo=ignored | README.md | STM32MP1 Buildroot external tree | st/2021.02}}<br />
|
1- README.md |
Buildroot: directory
1- {{CodeSource | Buildroot | docs/}}<br />
2- {{CodeSource | Buildroot | docs/ | STM32MP1 Buildroot documentation}}<br />
3- {{CodeSource | Buildroot | docs/ | | st/2021.02}}<br />
4- {{CodeSource | Buildroot | docs/ | STM32MP1 Buildroot documentation | st/2021.02}}<br />
5- {{CodeSource | Buildroot | docs/ | repo=ignored | STM32MP1 Buildroot documentation | st/2021.02}}<br />
|
1- docs/ |
X-LINUX-AI: regular file
AI | README.md}}<br /> 2- {{CodeSource | X-LINUX-AI | README.md | AI expansion package for STM32MPUs}}<br /> 3- {{CodeSource | X-LINUX-AI | README.md | | 2.2.0}}<br /> 4- {{CodeSource | X-LINUX-AI | README.md | AI expansion package for STM32MPUs | 2.2.0}}<br /> 5- {{CodeSource | X-LINUX-AI | repo=ignored | README.md | AI expansion package for STM32MPUs | 2.2.0}}<br />1- {{CodeSource | X-LINUX- |
1- README.md |
X-LINUX-AI: directory
AI | conf/}}<br /> 2- {{CodeSource | X-LINUX-AI | conf/ | X-LINUX-AI configuration file}}<br /> 3- {{CodeSource | X-LINUX-AI | conf/ | | 2.2.0}}<br /> 4- {{CodeSource | X-LINUX-AI | conf/ | X-LINUX-AI configuration file | 2.2.0}}<br /> 5- {{CodeSource | X-LINUX-AI | conf/ | repo=ignored | X-LINUX-AI configuration file | 2.2.0}}<br />1- {{CodeSource | X-LINUX- |
1- README.md |
st-openstlinux-application: regular file
AI expansion package for STM32MPUs}}<br /> 3- {{CodeSource | st-openstlinux-application | README.md | | 2.2.0}}<br /> 4- {{CodeSource | st-openstlinux-application | README.md | AI expansion package for STM32MPUs | 2.2.0}}<br /> 5- {{CodeSource | st-openstlinux-application | repo=ignored | README.md | AI expansion package for STM32MPUs | 2.2.0}}<br />1- {{CodeSource | st-openstlinux-application | README.md}}<br /> 2- {{CodeSource | st-openstlinux-application | README.md | |
1- README.md |
st-openstlinux-application: directory
AI configuration file}}<br /> 3- {{CodeSource | st-openstlinux-application | conf/ | | 2.2.0}}<br /> 4- {{CodeSource | st-openstlinux-application | conf/ | X-LINUX-AI configuration file | 2.2.0}}<br /> 5- {{CodeSource | st-openstlinux-application | conf/ | repo=ignored | X-LINUX-AI configuration file | 2.2.0}}<br />1- {{CodeSource | st-openstlinux-application | conf/}}<br /> 2- {{CodeSource | st-openstlinux-application | conf/ | X-LINUX- |
1- conf/ |
Unsupported domain
{{CodeSource | Unsupported domain | Makefile}}
|
Unsupported domain! |
4. Code[edit source]
Unsupported domain!