This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The Has to be updated for property indicates for which release the page must be updated d
This is a property of type Text.
The allowed values for this property are:
- STM32MP15-v3.0.0: the page has to be updated for STM32MP15 ecosystem release v3.0.0
- STM32MP15-v3.1.0: the page has to be updated for STM32MP15 ecosystem release v3.1.0
- STM32MP13-v0.3.0: the page has to be updated for STM32MP13 ecosystem release v0.3.0
{}
- "type": "PROPERTY_CONSTRAINT_SCHEMA",
-"constraints": {}
- "type_constraint": "_txt",
-"allowed_values": []
- "STM32MP15-v3.0.0",
- "STM32MP15-v3.1.0",
- "STM32MP13-v0.3.0"