X-LINUX-AI OpenSTLinux Expansion Package - v3.0.0

Revision as of 18:05, 30 June 2022 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines

AI X-LINUX-AI-logo.png

X-LINUX-AI is an STM32 MPU OpenSTLinux Expansion Package that targets artificial intelligence for STM32MP1 Series devices. It contains Linux AI frameworks, as well as application examples to get started with some basic use cases such as computer vision (CV). It is composed of an OpenEmbedded meta layer, named meta-st-stm32mpu-ai, to be added on top of the STM32MP1 Distribution Package. It brings a complete and coherent easy-to-build / install environment to take advantage of AI on STM32MP1 Series devices.

AI Expansion Package In STM32MPU Embedded Software.png

1. X-LINUX-AI v2.2.0[edit source]

Info white.png Information
This version is compatible with Yocto Project® build system Kirkstone/Dunfell and has been validated against the OpenSTLinux ecosystem release v4.0.0 More info.png , ecosystem release v3.1.0 and validated on STM32MP1X boards.

1.1. Contents[edit source]

Warning white.png Warning
The face recognition binary is available on demand. Please contact the local STMicroelectronics support for more information about this application or send a request to edge.ai@st.com
  • Application support for the 720p, 480p, and 272p display configurations
  • New.png Application user interface with updated look and feel
  • New.png Python™ and C++ application rework for better performance
  • New.png X-LINUX-AI SDK add-on extending the OpenSTLinux SDK with AI functionality to develop and build an AI application easily. The X-LINUX-AI SDK add-on provides support for all the above frameworks. It is available from the X-LINUX-AI product page

1.2. Validated hardware[edit source]

As any software expansion package, the X-LINUX-AI is supported on all STM32MP1 Series and it has been validated on the following boards:

  • STM32MP157F-DK2[5]
  • STM32MP157F-EV1[6]
  • STM32MP157D-EV1[7]

1.3. Software structure[edit source]

X-LINUX-AI v2.1.0 Expansion Package Software structure

2. Starter package: install from the OpenSTLinux AI package repository[edit source]

Info white.png Information
The STMicroelectronics packages repository service is provided for evaluation purposes only, its content may be updated at any time without notice and is therefore not approved for use in production.

All the generated X-LINUX-AI packages are available from the OpenSTLinux AI package repository service hosted at the non-browsable URL http://extra.packages.openstlinux.st.com/AI.

This repository contains AI packages that can be simply installed using apt-* utilities, which the same as those used on a Debian system:

  • the main group contains the selection of AI packages whose installation is automatically tested by STMicroelectronics
  • the updates group is reserved for future uses such as package revision update.

You can install them individually or by package group.

2.1. Prerequisites[edit source]

  • Flash the Starter Package on your SDCard
For OpenSTLinux ecosystem release v4.0.0 More info.png :
STM32MP157x-DKx Starter Package procedure
or
STM32MP157x-EV1 Starter Package procedure
  • Your board has an internet connection either through the network cable or through a WiFi connection.
Info white.png Information

If your internet access depends on a proxy server, you should define the http_proxy environment variable with the following command before any apt-* commands:

 export http_proxy='http://<proxy url>:<proxy port>/'

2.2. Configure the AI OpenSTLinux package repository[edit source]

Once the board is booted, execute the following command in the console in order to configure the AI OpenSTLinux package repository:

For ecosystem release   v4.0.0 More info.png :

 wget http://extra.packages.openstlinux.st.com/AI/4.0/pool/config/a/apt-openstlinux-ai/apt-openstlinux-ai_1.0_armhf.deb
 dpkg -i apt-openstlinux-ai_1.0_armhf.deb 
For ecosystem release   v3.1.0 :
 wget http://extra.packages.openstlinux.st.com/AI/3.1/pool/config/a/apt-openstlinux-ai/apt-openstlinux-ai_1.0_armhf.deb
 dpkg -i apt-openstlinux-ai_1.0_armhf.deb 

Then synchronize the AI OpenSTLinux package repository.

 apt-get update

2.3. Install AI packages[edit source]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.

2.3.1. Install all X-LINUX-AI packages[edit source]

Command Description
apt-get install packagegroup-x-linux-ai
Install all the X-LINUX-AI packages (TensorFlow™ Lite, Edge TPU™, application samples and tools)

2.3.2. Install AI framework related packages[edit source]

Command Description
apt-get install packagegroup-x-linux-ai-tflite
Install X-LINUX-AI packages related to TensorFlow™ Lite framework (including application samples)
apt-get install packagegroup-x-linux-ai-tflite-edgetpu
Install X-LINUX-AI packages related to the Coral Edge TPU™ framework (including application samples)

2.3.3. Install individual packages[edit source]

Command Description
apt-get install libedgetpu2
Install libedgetpu for Coral Edge TPU™
apt-get install libcoral2
Install libcoral API for Coral Edge TPU™
apt-get install libtensorflow-lite-tools
Install Tensorflow™ Lite utilities
apt-get install libtensorflow-lite2
Install Tensorflow™ Lite runtime
apt-get install python3-libtensorflow-lite
Install Python TensorFlow™ Lite inference engine
apt-get install python3-pycoral
Install Python PyCoral API for Coral Edge TPU™
apt-get install tflite-cv-apps-edgetpu-image-classification-c++
Install C++ image classification example using Coral Edge TPU™ TensorFlow™ Lite API
apt-get install tflite-cv-apps-edgetpu-image-classification-python
Install Python image classification example using Coral Edge TPU™ TensorFlow™ Lite API
apt-get install tflite-cv-apps-edgetpu-object-detection-c++
Install C++ object detection example using Coral Edge TPU™ TensorFlow™ Lite API
apt-get install tflite-cv-apps-edgetpu-object-detection-python
Install Python object detection example using Coral Edge TPU™ TensorFlow™ Lite API
apt-get install tflite-cv-apps-image-classification-c++
Install C++ image classification using TensorFlow™ Lite
apt-get install tflite-cv-apps-image-classification-python
Install Python image classification example using TensorFlow™ Lite
apt-get install tflite-cv-apps-object-detection-c++
Install C++ object detection example using TensorFlow™ Lite
apt-get install tflite-cv-apps-object-detection-python
Install Python object detection example using TensorFlow™ Lite
apt-get install tflite-edgetpu-benchmark
Install benchmark application for Coral Edge TPU™ models
apt-get install tflite-models-coco-ssd-mobilenetv1
Install TensorFlow™ Lite COCO SSD Mobilenetv1 model
apt-get install tflite-models-coco-ssd-mobilenetv1-edgetpu
Install TensorFlow™ Lite COCO SSD Mobilenetv1 model for Coral Edge TPU™
apt-get install tflite-models-mobilenetv1
Install TensorFlow™ Lite Mobilenetv1 model
apt-get install tflite-models-mobilenetv1-edgetpu
Install TensorFlow™ Lite Mobilenetv1 model for Coral Edge TPU™
Info white.png Information
If you need more information about how to use apt-* utilities check the Package repository for OpenSTLinux distribution article.

3. Developer package: build AI application from the X-LINUX-AI add-on SDK[edit source]

To go one step further in the use of AI on STM32MPU the Developer package is a good approach. This package is designed for developer which wants to make their own developments on top of the STM32MPU Embedded Software distribution or replace the Starter Package pre-built binaries.

The X-LINUX-AI extension package provide an add-on to the OpenSTLinux SDK already provided in the Developer package. This add-on allows to integrate to the SDK all the necessary libraries to develop and build an AI application easily without using the YOCTO build system.

All the information you need to install and use the X-LINUX-AI SDK add-on can be found in the following article : How to install and use the X-LINUX-AI SDK add-on

4. Distribution package: re-generate X-LINUX-AI OpenSTLinux distribution[edit source]

With the following procedure, you can re-generate the complete distribution enabling the X-LINUX-AI expansion package.
This procedure is mandatory if you want to update frameworks by yourself, or if you want to modify the application samples.

4.1. Download the STM32MP1 Distribution Package[edit source]

For ecosystem release v4.0.0 More info.png :
Install the STM32MP1 Distribution Package v4.0.0, but do not initialize the OpenEmbedded environment (do not source the envsetup.sh).

For ecosystem release v3.1.0 :

Install the STM32MP1 Distribution Package v3.1.0, but do not initialize the OpenEmbedded environment (do not source the envsetup.sh).

4.2. Install X-LINUX-AI environment[edit source]

  • Clone the meta-st-stm32mpu-ai git repositories
Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
For X-LINUX-AI v2.2.0:
 cd <Distribution Package installation directory>/layers/meta-st
 git clone https://github.com/STMicroelectronics/meta-st-stm32mpu-ai.git -b v2.2.0

  • Set up the build environment
 cd ../..
 DISTRO=openstlinux-weston MACHINE=stm32mp1 BSP_DEPENDENCY='layers/meta-st/meta-st-stm32mpu-ai' source layers/meta-st/scripts/envsetup.sh

4.3. Build the image[edit source]

 bitbake st-image-ai
Info white.png Information
Note that building the image could take long time depending on the host computer performance.

4.4. Flash the built image[edit source]

Follow this link to see how to flash the built image.

5. How to use the X-LINUX-AI Expansion Package[edit source]

5.1. Material needed[edit source]

To use the X-LINUX-AI OpenSTLinux Expansion Package, choose one of the following materials:

  • STM32MP157F-DK2[5] + an UVC USB WebCam
  • STM32MP157F-EV1[6] with the built in OV5640 parallel camera
  • STM32MP157D-EV1[7] with the built in OV5640 parallel camera

Optional:

  • Coral USB Edge TPU™[2] accelerator

5.2. Boot the OpenSTlinux Starter Package[edit source]

At the end of the boot sequence, the demo launcher application appears on the screen.

Demo launcher appearance when X-LINUX-AI is not installed

5.3. Install the X-LINUX-AI[edit source]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.

After having configured the AI OpenSTLinux package you can install the X-LINUX-AI components.

 apt-get install packagegroup-x-linux-ai

And restart the demo launcher:

- For OpenSTLinux distribution with a version lower than 4.0 use

 systemctl restart weston@root

- For other OpenSTLinux distribution use :

 systemctl restart weston-launch

5.4. Launch an AI application sample[edit source]

Once the demo launcher is restarted, notice that it is slightly different because new AI application samples have been installed.
The demo laucher has the following appearance, and you can navigate into the different screens by using the NEXT or BACK buttons.

Demo launcher appearance when X-LINUX-AI is installed

Screens 2, 3 and 4 contain AI application samples that are described within dedicated article available in the X-LINUX-AI application samples zoo page.

5.5. Enjoy running your own NN models[edit source]

The above examples provide application samples to demonstrate how to execute models easily on the STM32MP1.

You are free to update the C/C++ application or Python scripts for your own purposes, using your own NN models.

Source code locations are provided in application sample pages.

6. References[edit source]

7. Archives Archive box.png[edit source]

X-LINUX-AI release Release note
X-LINUX-AI v2.1.1 X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-1-1 page for the v3 ecosystem releases (in archived wiki)
X-LINUX-AI v2.1.0 X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-1-0 page for the v2 ecosystem releases (in archived wiki)
X-LINUX-AI v2.0.0 X-LINUX-AI_OpenSTLinux_Expansion_Package#X-LINUX-AI_v2-0-0 page for the v2 ecosystem releases (in archived wiki)