Last edited one year ago

STM32MP1 Distribution Package - OpenSTLinux distribution

This article aims to give the following information:

  • How to download and install the latest OpenSTLinux distribution for the STM32 microprocessors Series
  • Where to find the associated release note
  • Where to find the previous releases (archives)

1. STM32MP15-Ecosystem-v3.0.0 release

  • The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision (unknown revision).
  • The installation relies on the repo command. In case the Repo tool (a Google-built repository management tool that runs on top of git) is not yet installed and configured on the host PC, refer to the PC prerequisites article.
  • The OpenSTLinux distribution is massively using open source software (OSS) packages that are downloaded from a variety of open source repositories; so it is required that the IT infrastructure proxies do not forbid such accesses. If some proxy-related issues are suspected, refer to the How to avoid proxy issues article.
  • Install the STM32MP1 OpenSTLinux distribution
STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP15-Ecosystem-v3.0.0 release
Installation
PC $> cd <working directory path>/Distribution-Package
  • Create the OpenSTLinux distribution installation sub-directory:
PC $> mkdir unknown revision 
PC $> cd unknown revision
  • Initialize repo in the current directory (More details on 'repo init' here).
PC $> repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/unknown revision


Note: "ERROR 404" may appear during "repo init" command without any impact on the process

  • Synchronize the local project directories with the remote repositories specified in the manifest (more details on 'repo sync' here)
PC $> repo sync


Note: Distribution package needs around 140MB to be installed (and around 25GB once distribution package is compiled).

Release note

Details about the content of this software package are available in the associated STM32MP15 ecosystem release note.

Archive box.png If interested in previous releases, go through the archives of the ecosystem release note.

  • The OpenSTLinux distribution installation directory is in the <Distribution Package installation directory>, and is named unknown revision:
unknown revision  OpenSTLinux distribution
├── layers 
│    ├── meta-openembedded                Collection of layers for the OpenEmbedded-Core universe (OpenEmbedded standard)
│    ├── meta-qt5                         QT5 layer for OpenEmbedded (standard)
│    ├── meta-st
│    │   ├── meta-st-openstlinux          STMicroelectronics layer that contains the frameworks and images settings for the OpenSTLinux distribution
│    │   ├── meta-st-stm32mp              STMicroelectronics layer that contains the description of the BSP for the STM32 MPU devices
│    │   │   ├── recipes-bsp
│    │   │   │   ├── alsa                 Recipes for ALSA control configuration
│    │   │   │   ├── drivers              Recipes for Vivante GCNANO GPU kernel drivers
│    │   │   │   ├── trusted-firmware-a   Recipes for TF-A
│    │   │   │   └── u-boot               Recipes for U-Boot
│    │   │   ├── recipes-extended
│    │   │   │   ├── linux-examples       Recipes for Linux examples for STM32 MPU devices
│    │   │   │   ├── m4coredump           Recipes for script to manage coredump of cortexM4
│    │   │   │   └── m4projects           Recipes for firmware examples for Cortex M4
│    │   │   ├── recipes-graphics
│    │   │   │   ├── gcnano-userland      Recipes for Vivante libraries OpenGL ES, OpenVG and EGL (multi backend)
│    │   │   │   └── [...]
│    │   │   ├── recipes-kernel
│    │   │   │   ├── linux                Recipes for Linux kernel
│    │   │   │   └── linux-firmware       Recipes for Linux firmwares (example, Bluetooth firmware)
│    │   │   ├── recipes-security
│    │   │   │   └── optee                Recipes for OPTEE
│    │   │   ├── recipes-st
│    │   │   │   └── images               Recipes for the bootfs and userfs partitions binaries
│    │   │   └── [...]
│    │   ├── meta-st-stm32mp-addons       STMicroelectronics layer that helps managing the STM32CubeMX integration
│    │   └── scripts
│    │       ├── envsetup.sh              Environment setup script for Distribution Package
│    │       └── [...]
│    └── openembedded-core                Core metadata for current versions of OpenEmbedded (standard)



2. Archives Archive box.png

This wiki is for the v2 ecosystem releases. For information about the previous ecosystem releases, please go through the Wiki archives.