X-LINUX-AI - object detection using ONNX C++ API

Revision as of 10:51, 7 April 2023 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines

This article explains how to experiment with ONNX Runtime [1] applications for object detection based on the COCO SSD MobileNet v1 model using ONNX C++ API runtime.


1. Description[edit source]

The object detection[2] neural network model allows identification and localization of a known object within an image.

C/C++ ONNX Runtime object detection application

The application demonstrates a computer vision use case for object detection where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model interpreted by the ONNX Runtime [1] framework.
A Gstreamer pipeline is used to stream camera frames (using v4l2src), to display a preview (using waylandsink) and to execute a neural network inference (using appsink).
The result of the inference is displayed on the preview. The overlay is done using GtkWidget with cairo.
This combination is quite simple and efficient in terms of CPU overhead.


The performance depends on the number of CPUs available. The camera preview is limited to one CPU core while the ONNX runtime[1] interpreter is configured to use the maximum of the available resources.

The model used with this application is the COCO SSD MobileNet v1 downloaded from TensorFlow For Mobile & Edge[2] and converted to ONNX opset 16 format using tf2onnx


Info white.png Information
To convert the Tensorflow Lite model to ONNX you can check this article : How to convert a Tensorflow™ Lite model to ONNX

2. Installation[edit source]

2.1. Install from the OpenSTLinux AI package repository[edit source]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.

After having configured the AI OpenSTLinux package, the user can install the X-LINUX-AI components for this application:

 apt-get install onnx-cv-apps-object-detection-c++

Then, the user can restart the demo launcher:

- For OpenSTLinux distribution with a version lower than 4.0 use:

 systemctl restart weston@root

- For other OpenSTLinux distribution use:

 systemctl restart weston-launch

2.2. Source code location[edit source]

  • in the Openembedded OpenSTLinux Distribution with the X-LINUX-AI Expansion Package:
<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/onnx-cv-apps/files/object-detection/src
  • on GitHub:
https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/v3.0.0/recipes-samples/onnxrt-cv-apps/files/object-detection/src

2.3. Re-generate the package from OpenSTLinux Distribution (optional)[edit source]

Using the Openembedded OpenSTLinux distribution, you are able to rebuild the application.

Info white.png Information
If not already installed, the X-LINUX-AI OpenSTLinux Distribution need to be installed by following this link


  • Set up the build environment:
 cd <Distribution Package installation directory>
 source layers/meta-st/scripts/envsetup.sh
  • Rebuild the application:
 bitbake onnx-cv-apps-object-detection-c++ -c compile

The generated binary is available here:

<Distribution Package installation directory>/<build directory>/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/onnx-cv-apps-object-detection-c++/3.0.0-r0/onnx-cv-apps-object-detection-c++-3.0.0/object-detection/src/

3. How to use the application[edit source]

3.1. Launching via the demo launcher[edit source]

Demo launcher

3.2. Executing with the command line[edit source]

The objdetect_onnx_gst_gtk C/C++ application is located in the userfs partition:

/usr/local/demo-ai/computer-vision/onnx-object-detection/bin/objdetect_onnx_gst_gtk

It accepts the following input parameters:

Usage: ./objdetect_onnx_gst_gtk -m <model .onnx> -l <label .txt file>

-m --model_file <.onnx file path>:  .onnx model to be executed
-l --label_file <label file path>:    name of file containing labels
-i --image <directory path>:          image directory with image to be classified
-v --video_device <n>:                video device (default /dev/video0)
--crop:                               if set, the nn input image is cropped (with the expected nn aspect ratio) before being resized,
                                      else the nn input image is only resized to the nn input size (could cause picture deformation).
--frame_width  <val>:                 width of the camera frame (default is 640)
--frame_height <val>:                 height of the camera frame (default is 480)
--framerate <val>:                    framerate of the camera (default is 15fps)
--input_mean <val>:                   model input mean (default is 127.5)
--input_std  <val>:                   model input standard deviation (default is 127.5)
--verbose:                            enable verbose mode
--validation:                         enable the validation mode
-t --threshold <val>:                 threshold of accuracy above which the boxes are displayed (default 0.62)
--help:                               show this help

3.3. Testing with COCO ssd MobileNet v1[edit source]

The model used for test is the detect.onnx downloaded from TensorFlow For Mobile & Edge[2] and converted to ONNX format.

Info white.png Information
The different objects that the neural network is able to detect are listed in the labels.txt file located in the target:

/usr/local/demo-ai/computer-vision/models/coco_ssd_mobilenet/labels.txt

To ease launching of the application, two shell scripts are available:

  • launch object detection based on camera frame inputs
 /usr/local/demo-ai/computer-vision/onnx-object-detection/bin/launch_bin_objdetect_onnx_coco_ssd_mobilenet.sh
  • launch object detection based on the pictures located in /usr/local/demo-ai/computer-vision/models/coco_ssd_mobilenet/testdata directory:
 /usr/local/demo-ai/computer-vision/onnx-object-detection/bin/launch_bin_objdetect_onnx_coco_ssd_mobilenet_testdata.sh
Info white.png Information
Note that you need to populate the testdata directory with your own data sets.

The pictures are then randomly read from the testdata directory

4. References[edit source]