This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.![]() |
This page is a candidate for renaming (move). The requested new name is: STM32MP135 Discovery kits - required material . The supplied reason is: STM32MP13 as such does not exist while STM32MP135 is the name of a line. Such a title is OK as long as it is made clear to the reader that the article applies to STM32MP135x-DK boards with STM32MP135F-DK used as an example. . -- Registered User (-) 15:38, 29 September 2022 (CEST). Wiki maintainers: remember to update the pages that link this page before renaming (moving) it. |
This article presents the mandatory and optional material needed for an STM32MP135x-DK Discovery kit. It is valid for the STM32MP135F-DK Discovery kit
: the part numbers are specified in the STM32MP13 microprocessor part numbers article.
Mandatory
PC | Linux® or Windows® operating systems. See PC prerequisites for more details on the required configurations. |
STM32MP135x-DK Discovery kit | Flexible and complete development platform for the STM32MP135 microprocessor device including:
|
Power supply | Including:
|
microSD™ card | Populated with OpenSTLinux distribution (Linux® software), and providing extra storage capacity. A 2-Gbyte minimum microSD™ card is needed. |
USB Micro-B cable | To connect the STM32MP135x-DK Discovery kit to the PC through the USB Micro-B (ST-LINK/V2-1) connector |
USB Type-C® cable | To connect the STM32MP135x-DK Discovery kit to a USB OTG device through the USB Type-C®/sup> connector |
Optional
USB keyboard and mouse | Through its USB Type-A connectors, the STM32MP135x-DK Discovery kit can be equipped with a full-size keyboard and mouse |
Ethernet cable | To connect the STM32MP135x-DK Discovery kit to a network through the RJ45 connector |
Optional, more devices and extension boards might be plugged to the STM32MP135x-DK Discovery kit thanks to expansion connectors such as:
- the GPIO expansion connector
- ...