This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User m (Undo revision 85790 by Registered User (-)) Tag: Undo |
Registered User mNo edit summary |
||
Line 1: | Line 1: | ||
{|class="st_table" | |||
! colspan="4" style="text-align:center;" | STM32MP13 boards | |||
{|class=" | |||
! colspan=" | |||
|- | |- | ||
! Boards !! PCBs list !! style="width: 40%;" | Main features !! Ordering | |||
|- | |- | ||
| | | style="text-align:center;" | [[File:STM32MP135x-DK.png|x150px|link=Category:STM32MP13_Discovery_kits]]<br />[[:Category:STM32MP13_Discovery_kits|STM32MP135F-DK Discovery kit]] | ||
| | |||
* MB1635C (motherboard) | |||
* MB1723 (daughterboard CSI camera) | |||
| | |||
* STM32MP135FAF7<ref name="STM32MP13_codification">[[STM32MP13 microprocessor#Part number codification|STM32MP13 microprocessor part numbers]]</ref> Rev.Z | |||
** Arm<sup>®</sup>-based Cortex<sup>®</sup>-A7 1 GHz | |||
** Secure boot and cryptography | |||
** 512-Mbyte DDR3L, 16 bits, 533 MHz | |||
* ST PMIC STPMIC1DPQR | |||
* 4.3" TFT 480x272 pixels with LED backlight, and capacitive touch panel | |||
* 5-megapixel, 10-bit camera | |||
* Wi-Fi<sup>®</sup> 802.11b/g/n | |||
* Bluetooth<sup>®</sup> Low Energy 4.1 | |||
| | |||
{{UnderConstruction}} | |||
|} | |} | ||
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 14:57, 14 January 2022 (CET)<br />To be updated when available with "Daughterboard camera MB1897"}} | {{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 14:57, 14 January 2022 (CET)<br />To be updated when available with "Daughterboard camera MB1897"}} | ||
<noinclude> | |||
<references/> | |||
{{NoIndex}} | {{NoIndex}} | ||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
{{PublicationRequestId | | {{PublicationRequestId | Auto}} | ||
{{UpdateNeededForNewBoard|Point to the new board (if it belongs to the STM32MP13 | {{UpdateNeededForNewBoard|Point to the new board (if it belongs to the STM32MP13 Series)}} | ||
</noinclude> | </noinclude> |
Revision as of 15:42, 13 January 2023
STM32MP13 boards | |||||
---|---|---|---|---|---|
Boards | PCBs list | Main features | Ordering | ||
![]() STM32MP135F-DK Discovery kit |
|
|
|