This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User m (Undo revision 85790 by Registered User (-)) Tag: Undo |
Registered User mNo edit summary |
||
(12 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
{|class="st_table" | |||
! colspan="4" style="text-align:center;" | STM32MP13 boards | |||
{|class=" | |||
! colspan=" | |||
|- | |- | ||
! Boards !! PCBs list !! style="width: 40%;" | Main features !! Ordering | |||
|- | |- | ||
|| | | style="text-align:center;" | [[File:STM32MP135x-DK.png|x150px|link=Category:STM32MP13_Discovery_kits]]<br />[[:Category:STM32MP13_Discovery_kits|STM32MP135F-DK Discovery kit]] | ||
|| | | | ||
* MB1635 (motherboard) | |||
* MB1897 (camera module board) | |||
| | |||
* STM32MP135FAF7<ref name="STM32MP13_codification">[[STM32MP13 microprocessor#Part number codification|STM32MP13 microprocessor part numbers]]</ref> Rev.Y | |||
** Arm<sup>®</sup>-based Cortex<sup>®</sup>-A7 1 GHz | |||
** Secure boot and cryptography | |||
** 4-Gbit DDR3L, 16 bits, 533 MHz | |||
* ST PMIC STPMIC1 | |||
* 4.3" TFT 480x272 pixels with LED backlight, and capacitive touch panel | |||
* 2-megapixel dual lane CSI-2 camera module with 15-pin FFC connector | |||
* Wi-Fi<sup>®</sup> 802.11b/g/n | |||
* Bluetooth<sup>®</sup> Low Energy 4.1 | |||
| | |||
[https://www.st.com/en/evaluation-tools/stm32mp135f-dk.html#sample-buy Discovery kit with STM32MP135F MPU] | |||
|} | |} | ||
<noinclude> | |||
<references/> | |||
{{NoIndex}} | {{NoIndex}} | ||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
{{PublicationRequestId | | {{PublicationRequestId | to be created}} | ||
{{UpdateNeededForNewBoard|Point to the new board (if it belongs to the STM32MP13 | {{UpdateNeededForNewBoard|Point to the new board (if it belongs to the STM32MP13 Series)}} | ||
</noinclude> | </noinclude> |
Latest revision as of 16:33, 9 March 2023
STM32MP13 boards | |||
---|---|---|---|
Boards | PCBs list | Main features | Ordering |
![]() STM32MP135F-DK Discovery kit |
|
|