This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 3: | Line 3: | ||
|MPUs checklist=STM32MP13x, STM32MP15x | |MPUs checklist=STM32MP13x, STM32MP15x | ||
}}</noinclude> | }}</noinclude> | ||
This article explains how to assemble the STM32MP135x-DK Discovery kit. It is valid for the | This article explains how to assemble the STM32MP135x-DK Discovery kit. It is valid for the {{Board | type=135F-DK}}: the part numbers are specified in the [[STM32MP13 microprocessor#Part number codification|STM32MP13 microprocessor part numbers]] article. | ||
{{Warning|To start the board successfully, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}} | {{Warning|To start the board successfully, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}} |
Revision as of 18:27, 28 November 2022
This article explains how to assemble the STM32MP135x-DK Discovery kit. It is valid for the STM32MP135F-DK Discovery kit : the part numbers are specified in the STM32MP13 microprocessor part numbers article.
The STM32MP135F-DK Discovery kit delivery is composed of the items listed below.
Position | Description |
---|---|
1 | MB1635 mother board |
2 | MB1723 camera module |
3 | Camera module flat cable |
4 | microSD™ card |
Note that the STM32MP135F-DK Discovery kit delivery does not contain a USB cable or a USB charger.