Registered User mNo edit summary |
Registered User mNo edit summary |
||
(18 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
==Overview== | ==Overview== | ||
This stage explains how to install the SDK.<br> | This stage explains how to install the SDK.<br> | ||
Line 18: | Line 17: | ||
{{SoftwareLicenseAgreement | distribution=OpenSTLinux}} | {{SoftwareLicenseAgreement | distribution=OpenSTLinux}} | ||
* Download the [{{EcosystemRelease/Package | revision=4.1.0 | package=SDK package | request=url}}/{{EcosystemRelease/Package | revision=4.1.0 | package=SDK package | request=name}} Developer Package Yocto SDK] into the following directory: '''$HOME/STM32MPU_workspace/tmp''' | |||
* | |||
* Uncompress the tarball file to get the SDK installation script | * Uncompress the tarball file to get the SDK installation script | ||
{{PC$}} cd $HOME/STM32MPU_workspace/tmp | {{PC$}} cd $HOME/STM32MPU_workspace/tmp | ||
{{PC$}} tar xvf {{EcosystemRelease/Package | revision= | {{PC$}} tar xvf {{EcosystemRelease/Package | revision=4.1.0| package=SDK package | request=name}} | ||
==Run the SDK installation script== | ==Run the SDK installation script== | ||
* Create your STM32MP1 Developer Package SDK directory on your host computer | |||
{{PC$}} mkdir -p $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK | |||
* Change the permissions of the SDK installation script so that it is executable | * Change the permissions of the SDK installation script so that it is executable | ||
{{PC$}} chmod +x {{EcosystemRelease/Package | revision= | {{PC$}} chmod +x {{EcosystemRelease/Package | revision=4.1.0 | package=SDK installation script | request=path}}/{{EcosystemRelease/Package | revision=4.1.0 | package=SDK installation script | request=name}} | ||
* Execute the SDK installation script | * Execute the SDK installation script | ||
{{PC$}} ./{{EcosystemRelease/Package | revision= | {{PC$}} ./{{EcosystemRelease/Package | revision=4.1.0 | package=SDK installation script | request=path}}/{{EcosystemRelease/Package | revision=4.1.0 | package=SDK installation script | request=name}} -d <working directory absolute path>/Developer-Package/SDK | ||
* The following log is output when the installation is successful: | * The following log is output when the installation is successful: | ||
<pre> | <pre> | ||
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version | ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 4.0.4-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23 | ||
============================================================================================================================ | =================================================================================================================================== | ||
Enter target directory for SDK (default: /opt/st/stm32mp1/4.0.4-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23):/home/osboxes/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK | |||
You are about to install the SDK to "/home/osboxes/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK". Proceed [Y/n]? | |||
You are about to install the SDK to "/home/osboxes/STM32MPU_workspace/ | |||
Extracting SDK.........................................................................................................................................................................................................................done | Extracting SDK.........................................................................................................................................................................................................................done | ||
Setting it up...done | Setting it up...done | ||
SDK has been successfully set up and is ready to be used. | SDK has been successfully set up and is ready to be used. | ||
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | ||
$ . /home/osboxes/STM32MPU_workspace/ | $ . /home/osboxes/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | ||
</pre> | </pre> | ||
==Start the SDK up== | ==Start the SDK up== | ||
{{info|The SDK environment setup script must be run once on each new working terminal on which you cross-compile}} | {{info|The SDK environment setup script must be run once on each new working terminal on which you cross-compile}} | ||
{{PC$}} cd $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package | |||
{{PC$}} cd $HOME/STM32MPU_workspace/ | {{PC$}} source SDK/{{EcosystemRelease/Package | revision=4.1.0 | package=SDK setup script | request=name}} | ||
{{PC$}} source SDK/{{EcosystemRelease/Package | revision= | |||
--------------------- | |||
Line 129: | Line 64: | ||
* Check the C compiler version | * Check the C compiler version | ||
{{PC$}} $CC --version | {{PC$}} $CC --version | ||
arm-ostl-linux-gnueabi-gcc (GCC) | arm-ostl-linux-gnueabi-gcc (GCC) 11.3.0 | ||
Copyright (C) | Copyright (C) 2021 Free Software Foundation, Inc. | ||
This is free software; see the source for copying conditions. There is NO | This is free software; see the source for copying conditions. There is NO | ||
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. | warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. | ||
* Check that the SDK version is the expected one (e.g.) | * Check that the SDK version is the expected one (e.g.) | ||
{{PC$}} echo $OECORE_SDK_VERSION | {{PC$}} echo $OECORE_SDK_VERSION | ||
4.0.4-{{EcosystemRelease/Package | revision=4.1.0 | package=OpenSTLinux distribution | request=name}} | |||
If any of these commands fails or does not return the expected result, try to reinstall the SDK. | If any of these commands fails or does not return the expected result, try to reinstall the SDK. |
Latest revision as of 11:32, 22 November 2022
1. Overview
This stage explains how to install the SDK.
The SDK for OpenSTLinux distribution provides a standalone cross-development toolchain and libraries tailored to the contents of the specific image flashed onto the board.
2. Host computer configuration
2.1. Install extra packages
Additional Ubuntu packages must be installed to perform basic development tasks, basic cross-compilation (via Developer Package) or more complex cross-compilation such as OpenEmbedded does (via Distribution Package):
- Packages required by OpenEmbedded/Yocto (details here):
PC $> sudo apt-get update
PC $> sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev pylint3 pylint xterm
PC $> sudo apt-get install make xsltproc docbook-utils fop dblatex xmlto
PC $> sudo apt-get install libmpc-dev libgmp-dev
- Packages needed for some "Developer Package" use cases:
PC $> sudo apt-get install libncurses5 libncurses5-dev libncursesw5-dev libssl-dev linux-headers-generic u-boot-tools device-tree-compiler bison flex g++ libyaml-dev libmpc-dev libgmp-dev
- Package for repo (used to download the "Distribution Package" source code):
repo. For Ubuntu 20.04, first sets python3 as default: PC $> sudo apt install python-is-python3Please follow the installation instructions described in
- Useful tools:
PC $> sudo apt-get install coreutils bsdmainutils sed curl bc lrzsz corkscrew cvs subversion mercurial nfs-common nfs-kernel-server libarchive-zip-perl dos2unix texi2html diffstat libxml2-utils
2.2. Additional configurations
Additional configurations have to be installed to support up to 16 partitions per MMC. By default, on Linux® systems, a maximum of 8 partitions are allowed on MMC. All Packages (Starter Package, ...) need more than 10 partitions for the storage device. In order to extend the number of partitions per device to 16, the following options must be added to modprobe:
PC $> echo 'options mmc_block perdev_minors=16' > /tmp/mmc_block.conf
PC $> sudo mv /tmp/mmc_block.conf /etc/modprobe.d/mmc_block.conf
3. Download the SDK
- Download the [unknown revision/unknown revision Developer Package Yocto SDK] into the following directory: $HOME/STM32MPU_workspace/tmp
- Uncompress the tarball file to get the SDK installation script
unknown revisionPC $> cd $HOME/STM32MPU_workspace/tmp PC $> tar xvf
4. Run the SDK installation script
- Create your STM32MP1 Developer Package SDK directory on your host computer
PC $> mkdir -p $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK
- Change the permissions of the SDK installation script so that it is executable
unknown revision/unknown revisionPC $> chmod +x
- Execute the SDK installation script
unknown revision/unknown revision -d <working directory absolute path>/Developer-Package/SDKPC $> ./
- The following log is output when the installation is successful:
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 4.0.4-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23
===================================================================================================================================
Enter target directory for SDK (default: /opt/st/stm32mp1/4.0.4-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23):/home/osboxes/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK
You are about to install the SDK to "/home/osboxes/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK". Proceed [Y/n]?
Extracting SDK.........................................................................................................................................................................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
$ . /home/osboxes/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
5. Start the SDK up
unknown revisionPC $> cd $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package PC $> source SDK/
The following checks ensure that the environment is correctly set up:
- Check the target architecture
PC $> echo $ARCH
arm
- Check the toolchain binary prefix for the target tools
PC $> echo $CROSS_COMPILE
arm-ostl-linux-gnueabi-
- Check the C compiler version
PC $> $CC --version
arm-ostl-linux-gnueabi-gcc (GCC) 11.3.0
Copyright (C) 2021 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
- Check that the SDK version is the expected one (e.g.)
unknown revisionPC $> echo $OECORE_SDK_VERSION 4.0.4-
If any of these commands fails or does not return the expected result, try to reinstall the SDK.