This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(9 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
This article | {{ApplicableFor | ||
|MPUs list=STM32MP13x | |||
|MPUs checklist=STM32MP13x,STM32MP15x | |||
}} | |||
</noinclude> | |||
<noinclude> | |||
This article presents the mandatory and optional material needed for an {{Board | type=135x-DK | name=short}} Discovery kit. It is valid for the {{Board | type=135F-DK }}: the part numbers are specified in the [[STM32MP13 microprocessor#Part number codification|STM32MP13 microprocessor part numbers]] article. | |||
{{Warning|For assistance with starting up the boards, it is recommended to go through the related Starter Package articles: [[:Category:Starter Package]]}} | {{Warning|For assistance with starting up the boards, it is recommended to go through the related Starter Package articles: [[:Category:Starter Package]]}} | ||
</noinclude> | </noinclude> | ||
Line 7: | Line 14: | ||
{| class="st-table" | {| class="st-table" | ||
|- | |- | ||
| '''PC''' || Linux or Windows operating systems. See [[PC prerequisites]] for more details on the required configurations. | | '''PC''' || Linux<sup>®</sup> or Windows<sup>®</sup> operating systems. See [[PC prerequisites]] for more details on the required configurations. | ||
|- | |- | ||
| [[STM32MP135x- | | [[STM32MP135x-DK - hardware description#Board overview | '''STM32MP135x-DK Discovery kit''']] || Flexible and complete development platform for the STM32MP135 microprocessor device including: | ||
* | * an MB1635 mother board | ||
|- | |- | ||
| '''Power supply''' || Including: | | '''Power supply''' || Including: | ||
* a USB Type-C<sup> | * a USB Type-C<sup>®</sup> cable (included in the packaging) | ||
* a USB Type-C<sup> | * a USB Type-C<sup>®</sup> charger (5 V, 3 A) (not included in the packaging) | ||
|- | |- | ||
| ''' | | '''microSD<sup>™</sup> card''' || Populated with OpenSTLinux distribution (Linux<sup>®</sup> software), and providing extra storage capacity. A 2-Gbyte minimum microSD<sup>™</sup> card is needed. | ||
|- | |- | ||
| '''USB | | '''USB Micro-B cable''' || To connect the STM32MP135x-DK Discovery kit to the PC through the USB Micro-B (ST-LINK/V2-1) connector. | ||
|- | |- | ||
| '''USB Type-C<sup> | | '''USB Type-C<sup>®</sup> cable''' || To connect the STM32MP135x-DK Discovery kit to a USB OTG device through the USB Type-C<sup>®</sup> connector. | ||
|} | |} | ||
<br> | <br> | ||
Line 26: | Line 33: | ||
{| class="st-table" | {| class="st-table" | ||
|- | |- | ||
| '''USB keyboard and mouse''' || | | '''USB keyboard and mouse''' || Through its USB Type-A connectors, the STM32MP135x-DK Discovery kit can be equipped with a full-size keyboard and mouse. | ||
|- | |- | ||
| '''Ethernet cable''' || | | '''Ethernet cable''' || To connect the STM32MP135x-DK Discovery kit to a network through the RJ45 connector. | ||
|} | |} | ||
{{highlight|'''Optional'''}} | {{highlight|'''Optional'''}}: It is possible to plug more devices and extension boards to the STM32MP135x-DK Discovery kit by means of its expansion connectors such as the GPIO expansion connector. | ||
<noinclude> | <noinclude> | ||
{{NoIndex}} | {{NoIndex}} | ||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
{{PublicationRequestId | 24673 | 2022-09-26 |}} | |||
</noinclude> | </noinclude> |
Latest revision as of 15:30, 18 November 2022
This article presents the mandatory and optional material needed for an STM32MP135x-DK Discovery kit. It is valid for the STM32MP135F-DK Discovery kit
: the part numbers are specified in the STM32MP13 microprocessor part numbers article.
Mandatory
PC | Linux® or Windows® operating systems. See PC prerequisites for more details on the required configurations. |
STM32MP135x-DK Discovery kit | Flexible and complete development platform for the STM32MP135 microprocessor device including:
|
Power supply | Including:
|
microSD™ card | Populated with OpenSTLinux distribution (Linux® software), and providing extra storage capacity. A 2-Gbyte minimum microSD™ card is needed. |
USB Micro-B cable | To connect the STM32MP135x-DK Discovery kit to the PC through the USB Micro-B (ST-LINK/V2-1) connector. |
USB Type-C® cable | To connect the STM32MP135x-DK Discovery kit to a USB OTG device through the USB Type-C® connector. |
Optional
USB keyboard and mouse | Through its USB Type-A connectors, the STM32MP135x-DK Discovery kit can be equipped with a full-size keyboard and mouse. |
Ethernet cable | To connect the STM32MP135x-DK Discovery kit to a network through the RJ45 connector. |
Optional: It is possible to plug more devices and extension boards to the STM32MP135x-DK Discovery kit by means of its expansion connectors such as the GPIO expansion connector.