This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User |
||
Line 4: | Line 4: | ||
==Install STM32CubeMP1 package== | ==Install STM32CubeMP1 package== | ||
{{SoftwareLicenseAgreement | distribution=STM32CubeMP1 }} | {{SoftwareLicenseAgreement | distribution=STM32CubeMP1 }} | ||
* Download [{{EcosystemRelease/Package | revision=4. | * Download [{{EcosystemRelease/Package | revision=4.1.0 | package=STM32CubeMP1 | request=url}}/{{EcosystemRelease/Package | revision=4.1.0 | package=STM32CubeMP1 | request=name}} {{EcosystemRelease/Package | revision=4.1.0 | package=STM32CubeMP1 | request=name}}] to the following directory:<br> '''$HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package''' | ||
* Uncompress the archive file to get the STM32CubeMP1 Package | * Uncompress the archive file to get the STM32CubeMP1 Package | ||
{{PC$}} unzip {{EcosystemRelease/Package | revision=4. | {{PC$}} unzip {{EcosystemRelease/Package | revision=4.1.0 | package=STM32CubeMP1 | request=name}} | ||
==STM32CubeMP1 package structure== | ==STM32CubeMP1 package structure== |
Latest revision as of 18:41, 17 November 2022
1. Overview[edit source]
This stage explains how to install the STM32CubeMP1 package.
2. Install STM32CubeMP1 package[edit source]
- Download [unknown revision/unknown revision unknown revision] to the following directory:
$HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package - Uncompress the archive file to get the STM32CubeMP1 Package
unknown revisionunzip
3. STM32CubeMP1 package structure[edit source]
The STM32CubeMP1 Package is located in your $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Developer-Package directory. It is named unknown revision:
unknown revision ├── Drivers │ ├── BSP BSP drivers for the supported STM32MP1 boards │ │ └── [...] │ ├── CMSIS │ │ └── [...] │ └── STM32MP1xx_HAL_Driver HAL drivers for the supported STM32MP1 devices │ └── [...] ├── _htmresc │ └── [...] ├── License.md ├── Middlewares │ └── [...] ├── package.xml ├── Projects │ ├── STM32CubeProjectsList.html List of examples and applications for STM32CubeMP1 package │ ├── STM32MP157C-DK2 Set of examples and applications → STM32MP15 Discovery kits │ │ └── [...] │ └── STM32MP157C-EV1 Set of examples and applications → STM32MP15 Evaluation boards │ └── [...] ├── Readme.md ├── Release_Notes.html Release note for STM32CubeMP1 package └── Utilities └── [...]