This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 15: | Line 15: | ||
| '''PC''' || Linux or Windows operating systems. See [[PC prerequisites]] for more details on the required configurations. | | '''PC''' || Linux or Windows operating systems. See [[PC prerequisites]] for more details on the required configurations. | ||
|- | |- | ||
| [[STM32MP135x- | | [[STM32MP135x-DK - hardware description#Board overview | '''STM32MP135x-DK Discovery kit''']] || Flexible and complete development platform for the STM32MP13 microprocessor device including: | ||
* a | * a MB1635 motherboard | ||
|- | |- | ||
| '''Power supply''' || Including: | | '''Power supply''' || Including: | ||
Line 24: | Line 24: | ||
| '''MicroSD card''' || Populated with OpenSTLinux distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed. | | '''MicroSD card''' || Populated with OpenSTLinux distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed. | ||
|- | |- | ||
| '''USB micro-B cable''' || In order to connect the STM32MP135x- | | '''USB micro-B cable''' || In order to connect the STM32MP135x-DK Discovery kit to the PC through the USB micro-B (ST-LINK/V2-1) connector | ||
|- | |- | ||
| '''USB Type-C<sup>™</sup> cable''' || In order to connect the STM32MP135x- | | '''USB Type-C<sup>™</sup> cable''' || In order to connect the STM32MP135x-DK Discovery kit to an USB OTG device through the USB Type-C<sup>™</sup> connector | ||
|} | |} | ||
<br> | <br> | ||
Line 32: | Line 32: | ||
{| class="st-table" | {| class="st-table" | ||
|- | |- | ||
| '''USB keyboard and mouse''' || Thanks to the USB type A connectors, the STM32MP135x- | | '''USB keyboard and mouse''' || Thanks to the USB type A connectors, the STM32MP135x-DK Discovery kit can be equipped with a full-size keyboard and mouse | ||
|- | |- | ||
| '''Ethernet cable''' || In order to connect the STM32MP135x- | | '''Ethernet cable''' || In order to connect the STM32MP135x-DK Discovery kit to a network through the RJ45 connector | ||
|} | |} | ||
{{highlight|'''Optional'''}}, more devices and extension boards might be plugged to the STM32MP135x- | {{highlight|'''Optional'''}}, more devices and extension boards might be plugged to the STM32MP135x-DK Discovery kit thanks to expansion connectors such as: | ||
* the GPIO expansion connector | * the GPIO expansion connector | ||
* ... | * ... |
Revision as of 16:14, 3 January 2022
This article aims to present the mandatory and optional material needed for a STM32MP135x-DK Discovery kits. It is valid for the STM32MP135F-DK Discovery kit
: the part numbers are specified in the STM32MP13 microprocessor part numbers article.
Mandatory
PC | Linux or Windows operating systems. See PC prerequisites for more details on the required configurations. |
STM32MP135x-DK Discovery kit | Flexible and complete development platform for the STM32MP13 microprocessor device including:
|
Power supply | Including:
|
MicroSD card | Populated with OpenSTLinux distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed. |
USB micro-B cable | In order to connect the STM32MP135x-DK Discovery kit to the PC through the USB micro-B (ST-LINK/V2-1) connector |
USB Type-C™ cable | In order to connect the STM32MP135x-DK Discovery kit to an USB OTG device through the USB Type-C™ connector |
Optional
USB keyboard and mouse | Thanks to the USB type A connectors, the STM32MP135x-DK Discovery kit can be equipped with a full-size keyboard and mouse |
Ethernet cable | In order to connect the STM32MP135x-DK Discovery kit to a network through the RJ45 connector |
Optional, more devices and extension boards might be plugged to the STM32MP135x-DK Discovery kit thanks to expansion connectors such as:
- the GPIO expansion connector
- ...