This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.deleted>Frq08988 mNo edit summary |
Registered User mNo edit summary |
||
(7 intermediate revisions by the same user not shown) | |||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
{{ | This article aims to present how to assemble the '''STM32MP157x-EV1''' Evaluation boards. It is valid for the {{Board | type=157A-EV1 | name=short}}, {{Board | type=157D-EV1 | name=short}}, {{Board | type=157C-EV1 | name=short}} and {{Board | type=157F-EV1 | name=short}} Evaluation boards: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article. | ||
{{ | |||
{{ | |||
[[ | |||
{{Warning|To start efficiently the board, it's recommended to go through its Starter Package article: [[:Category:Starter Package]]}} | {{Warning|To start efficiently the board, it's recommended to go through its Starter Package article: [[:Category:Starter Package]]}} | ||
</noinclude> | </noinclude> | ||
The | The STM32MP157x-EV1 Evaluation boards packages ({{Board | type=157A-EV1 | name=short}}, {{Board | type=157D-EV1 | name=short}}, {{Board | type=157C-EV1 | name=short}} and {{Board | type=157F-EV1 | name=short}}) include all the items listed below. | ||
[[File: | [[File: STM32MP157x-EV1_split.png | thumb | upright=4 | left | link= | Out of the STM32MP157x-EV1 box <br> '''STM32MP157A-EV1''' shown here (picture is not contractual)]] | ||
{| | {| | ||
|+ | |+ | ||
Line 31: | Line 25: | ||
<br clear=all> | <br clear=all> | ||
The following figures explain how to assemble these different items to get the | The following figures explain how to assemble these different items to get the STM32MP157x-EV1 Evaluation boards. | ||
[[File: STM32MP157x-EV1_assembly.png | thumb | upright=4 | center | link= | STM32MP157x-EV1 Evaluation board assembly <br> '''STM32MP157A-EV1''' shown here (picture is not contractual)]] | |||
[[File: | [[File: STM32MP157x-EV1_assembled.png | thumb | upright=4 | center | link= | STM32MP157x-EV1 Evaluation board assembled <br> '''STM32MP157A-EV1''' shown here (picture is not contractual)]] | ||
[[ | <noinclude> | ||
{{NoIndex}} | |||
[[Category:Sub-articles]] | |||
{{PublicationRequestId | 7572 | 2018-06-19 | AlainF}} | |||
</noinclude> |
Latest revision as of 17:31, 18 May 2020
This article aims to present how to assemble the STM32MP157x-EV1 Evaluation boards. It is valid for the STM32MP157A-EV1 , STM32MP157D-EV1
, STM32MP157C-EV1
and STM32MP157F-EV1
Evaluation boards: the part numbers are specified in the STM32MP15 microprocessor part numbers article.
Template:Warning
The STM32MP157x-EV1 Evaluation boards packages (STM32MP157A-EV1 , STM32MP157D-EV1
, STM32MP157C-EV1
and STM32MP157F-EV1
) include all the items listed below.
Position | Description |
---|---|
1 | MB1262 motherboard |
2 | MB1263 daughterboard |
3 | MB1230 DSI 720p display |
4 | MB1379 daughterboard camera |
5 | microSD card |
6 | Power supply block (5V, 3A) |
The following figures explain how to assemble these different items to get the STM32MP157x-EV1 Evaluation boards.