This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.deleted>Frq07399 mNo edit summary |
Registered User No edit summary |
||
Line 1: | Line 1: | ||
'''OpenSTLinux filesystem''' follows the Standard Linux<sup>®</sup> filesystem, represented on the below diagram. | '''OpenSTLinux filesystem''' follows the Standard Linux<sup>®</sup> filesystem, represented on the below diagram. | ||
Line 27: | Line 19: | ||
== References == | == References == | ||
<references /> | <references /> | ||
<noinclude> | |||
{{ ArticleApprovedVersion | Jean-PhilippeR | Jean-ChristopheT | No previous approved version | AlainF - 10Jan'19 - 10266 | 10Jan'19 }} | |||
[[Category:Sub-articles]] | |||
</noinclude> |
Revision as of 15:27, 12 September 2019
OpenSTLinux filesystem follows the Standard Linux® filesystem, represented on the below diagram.
It is based on the File Hierarchy Standard (FHS) at user space level.
Template:Highlight, by using two paths:
- - Filesystem layers which are associated to a device (with both block and raw interfaces), and which manage persistent data
- - Pseudo filesystem which manages volatile data linked to the current running session
The Virtual File System[1] is a Linux core feature which proposes an abstraction layer for the Linux user space.