This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User No edit summary |
Registered User mNo edit summary |
||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
{{ArticleApprovedVersion | Jean-ChristopheT | BernardP (Passed, 27June'18) | No previous approved version | BrunoB - 14Sep'18 - 8422 | 15Sep'18}} | {{ArticleApprovedVersion | Jean-ChristopheT | BernardP (Passed, 27June'18) | No previous approved version | BrunoB - 14Sep'18 - 8422 | 15Sep'18}} | ||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
This article aims to present the mandatory and optional material needed for an | This article aims to present the mandatory and optional material needed for an STM32MP157x-DKx Discovery kit. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article. | ||
{{Warning|For assistance with starting up the boards, it is recommended to go through the related Starter Package articles: [[:Category:Starter Package]]}} | {{Warning|For assistance with starting up the boards, it is recommended to go through the related Starter Package articles: [[:Category:Starter Package]]}} | ||
</noinclude> | </noinclude> | ||
Line 15: | Line 12: | ||
| '''PC''' || Linux or Windows operating systems. See [[PC prerequisites]] for more details on the required configurations. | | '''PC''' || Linux or Windows operating systems. See [[PC prerequisites]] for more details on the required configurations. | ||
|- | |- | ||
| [[STM32MP157X-DKX - hardware description#Board overview |''' | | [[STM32MP157X-DKX - hardware description#Board overview | '''STM32MP157x-DKx Discovery kit''' <br> ('''STM32MP157A-DK1''' or '''STM32MP157c-DK2''')]] || Flexible and complete development platform for the STM32MP15 microprocessor device including: | ||
* a [[MB1272]] motherboard | * a [[MB1272]] motherboard | ||
* a [[MB1407]] daughterboard (480x800 pixels DSI display): only for the | * a [[MB1407]] daughterboard (480x800 pixels DSI display): only for the STM32MP157C-DK2 Discovery kit | ||
|- | |- | ||
| '''Power supply''' || | | '''Power supply''' || Including: | ||
* a USB Type-C<sup>™</sup> cable | * a USB Type-C<sup>™</sup> cable (delivered in the packages) | ||
* a USB Type-C<sup>™</sup> charger (5 V, 3 A) | * a USB Type-C<sup>™</sup> charger (5 V, 3 A) (not delivered in the packages) | ||
|- | |- | ||
| '''MicroSD card''' || Populated with OpenSTLinux distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed. | | '''MicroSD card''' || Populated with OpenSTLinux distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed. | ||
|- | |- | ||
| '''USB micro-B cable''' || In order to connect the | | '''USB micro-B cable''' || In order to connect the STM32MP157x-DKx Discovery kit to the PC through the USB micro-B (ST-LINK/V2-1) connector | ||
|- | |- | ||
| '''USB Type-C<sup>™</sup> cable''' || In order to connect the | | '''USB Type-C<sup>™</sup> cable''' || In order to connect the STM32MP157x-DKx Discovery kit to an USB OTG device through the USB Type-C<sup>™</sup> connector | ||
|} | |} | ||
<br> | <br> | ||
Line 33: | Line 30: | ||
{| class="wikitable" | {| class="wikitable" | ||
|- | |- | ||
| '''USB keyboard and mouse''' || Thanks to the USB type A connectors, the | | '''USB keyboard and mouse''' || Thanks to the USB type A connectors, the STM32MP157x-DKx Discovery kit can be equipped with a full-size keyboard and mouse | ||
|- | |- | ||
| '''Ethernet cable''' || In order to connect the | | '''Ethernet cable''' || In order to connect the STM32MP157x-DKx Discovery kit to a network through the RJ45 connector | ||
|- | |- | ||
| '''HDMI cable''' || In order to connect the | | '''HDMI cable''' || In order to connect the STM32MP157x-DKx Discovery kit to an HDMI monitor (or TV) through the HDMI connector | ||
|} | |} | ||
{{highlight|'''Optional'''}}, more devices and extension boards might be plugged to the | {{highlight|'''Optional'''}}, more devices and extension boards might be plugged to the STM32MP157x-DKx Discovery kit thanks to expansion connectors such as: | ||
* the GPIO expansion connector | * the GPIO expansion connector | ||
* the Arduino Uno connector | * the Arduino Uno connector | ||
* ... | * ... |
Revision as of 17:56, 6 March 2019
Template:ArticleApprovedVersion
This article aims to present the mandatory and optional material needed for an STM32MP157x-DKx Discovery kit. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the STM32MP15 microprocessor part numbers article.
Mandatory
PC | Linux or Windows operating systems. See PC prerequisites for more details on the required configurations. |
STM32MP157x-DKx Discovery kit (STM32MP157A-DK1 or STM32MP157c-DK2) |
Flexible and complete development platform for the STM32MP15 microprocessor device including: |
Power supply | Including:
|
MicroSD card | Populated with OpenSTLinux distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed. |
USB micro-B cable | In order to connect the STM32MP157x-DKx Discovery kit to the PC through the USB micro-B (ST-LINK/V2-1) connector |
USB Type-C™ cable | In order to connect the STM32MP157x-DKx Discovery kit to an USB OTG device through the USB Type-C™ connector |
Optional
USB keyboard and mouse | Thanks to the USB type A connectors, the STM32MP157x-DKx Discovery kit can be equipped with a full-size keyboard and mouse |
Ethernet cable | In order to connect the STM32MP157x-DKx Discovery kit to a network through the RJ45 connector |
HDMI cable | In order to connect the STM32MP157x-DKx Discovery kit to an HDMI monitor (or TV) through the HDMI connector |
Optional, more devices and extension boards might be plugged to the STM32MP157x-DKx Discovery kit thanks to expansion connectors such as:
- the GPIO expansion connector
- the Arduino Uno connector
- ...