This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User No edit summary |
||
Line 21: | Line 21: | ||
| '''Power supply''' || Including: | | '''Power supply''' || Including: | ||
* a USB Type-C<sup>™</sup> cable | * a USB Type-C<sup>™</sup> cable | ||
* a USB Type-C<sup>™</sup> charger (5 V, 3 A) | * a USB Type-C<sup>™</sup> charger (5 V, 3 A) '''Not included''' | ||
|- | |- | ||
| '''MicroSD card''' || Populated with OpenSTLinux distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed. | | '''MicroSD card''' || Populated with OpenSTLinux distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed. |
Revision as of 12:57, 20 February 2019
Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion
This article aims to present the mandatory and optional material needed for an STM32MP15 Discovery kit. Template:Warning
PC | Linux or Windows operating systems. See PC prerequisites for more details on the required configurations. |
STM32MP157X-DKX Discovery kit (board name: STM32MP157X-DKX) |
Flexible and complete development platform for the STM32MP15 microprocessor device including:
|
Power supply | Including:
|
MicroSD card | Populated with OpenSTLinux distribution (Linux software), and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed. |
USB micro-B cable | In order to connect the STM32MP15 Discovery kit to the PC through the USB micro-B (ST-LINK/V2-1) connector |
USB Type-C™ cable | In order to connect the STM32MP15 Discovery kit to an USB OTG device through the USB Type-C™ connector |
USB keyboard and mouse | Thanks to the USB type A connectors, the STM32MP15 Discovery kit can be equipped with a full-size keyboard and mouse |
Ethernet cable | In order to connect the STM32MP15 Discovery kit to a network through the RJ45 connector |
HDMI cable | In order to connect the STM32MP15 Discovery kit to an HDMI monitor (or TV) through the HDMI connector |
Template:Highlight, more devices and extension boards might be plugged to the STM32MP15 Discovery kit thanks to expansion connectors such as:
- the GPIO expansion connector
- the Arduino Uno connector
- ...