Unpack the STM32MP157x-EV1 board

1. Overview

This first step explains how to unpack the STM32MP157x-EV1 Evaluation board and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.

STM32MP1 connection block diagram

2. Out-of-the-box board

STM32MP157x-EV1 back view
STM32MP157x-EV1 front view
STM32MP157x-EV1 with all delivered items

3. Required equipment

The following table lists the equipment required to start playing with your STM32MP157x-EV1 board.
Some of them are delivered within the STM32MP157x-EV1 Evaluation board. The others need to be purchased separately.

4. Connection

  • Connect your laptop to the board ST-LINK/V2-1 port through the micro USB Type-B to USB Type-A cable.
  • Connect the power supply.
  • Connect your laptop to the board USB Type-C™ OTG port through the micro USB Type-B to USB Type-A.
  • Optionally connect your Ethernet network to the board Ethernet port through the Ethernet cable.
STM32MP157x-EV1 Evaluation board connection
  • Remove JP1 jumper and place JP4 and JP5 jumpers as shown below to enable debugging through ST-LINK/V2-1.
STM32MP157x-EV1 Jumper configuration