1. Overview[edit source]
This step explains how to connect your host Linux® terminal to your host computer through the ST-LINK/V2-1.
It then describes how to execute basic commands with the Linux command line interface in order to order to get familiar with the Linux console.
2. Serial terminal[edit source]
The serial terminal allows communicating with the board through an UART serial interface.
- Install minicom
sudo apt-get install minicom
- Get the ttyACM device instance that needs to be used to access the ST-LINK/V2-1
ls /dev/ttyACM*
/dev/ttyACM0
- Connect the minicom to the /dev/ttyACM0 device
minicom -D /dev/ttyACM0
Welcome to minicom 2.7
OPTIONS: I18n
Compiled on Nov 15 2018, 20:18:47.
Port /dev/ttyACM0, 15:56:03
Press CTRL-A Z for help on special keys
- Press the reset button to reset the board. The boot log should be displayed on the minicom window:
For ecosystem release v3.1.0 :
PMIC version = 0x20 INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000 INFO: FCONF: Reading firmware configuration information for: stm32mp_io INFO: Using SDMMC INFO: Instance 1 INFO: Boot used partition fsbl1 NOTICE: BL2: v2.4-r2.0(debug):v2.4-dirty NOTICE: BL2: Built : 16:43:51, Nov 17 2020 INFO: BL2: Doing platform setup INFO: RAM: DDR3-DDR3L 32bits 533000kHz INFO: Memory size = 0x40000000 (1024 MB) INFO: BL2: Loading image id 31 INFO: Loading image id=31 at address 0x2ffff000 INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff226 INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000 INFO: FCONF: Reading firmware configuration information for: dyn_cfg INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall INFO: BL2: Loading image id 4 INFO: Loading image id=4 at address 0x2ffc5000 INFO: Image id=4 loaded: 0x2ffc5000 - 0x2ffd97ec WARNING: Not a known TEE, use default loading options. INFO: BL2: Skip loading image id 21 INFO: BL2: Skip loading image id 22 INFO: BL2: Loading image id 23 INFO: Loading image id=23 at address 0xc0500000 INFO: Image id=23 loaded: 0xc0500000 - 0xc051ebf6 INFO: BL2: Loading image id 26 INFO: Loading image id=26 at address 0x2ffc0000 INFO: Image id=26 loaded: 0x2ffc0000 - 0x2ffc47e1 INFO: BL2: Loading image id 5 INFO: Loading image id=5 at address 0xc0100000 INFO: Image id=5 loaded: 0xc0100000 - 0xc01d3ee8 NOTICE: BL2: Booting BL32 INFO: Entry point address = 0x2ffc5000 INFO: SPSR = 0x1d3 NOTICE: SP_MIN: v2.4-r2.0(debug):v2.4-dirty NOTICE: SP_MIN: Built : 16:43:51, Nov 17 2020 INFO: ARM GICv2 driver initialized INFO: Set calibration timer to 60 sec INFO: stm32mp1 IWDG1 is secure INFO: SP_MIN: Initializing runtime services INFO: SP_MIN: Preparing exit to normal world U-Boot 2020.10-stm32mp-r2 (Oct 05 2020 - 15:15:32 +0000) CPU: STM32MP157FAA Rev.Z Model: STMicroelectronics STM32MP157F eval daughter on eval mother Board: stm32mp1 in trusted mode (st,stm32mp157f-ev1) Board: MB1263 Var4.0 Rev.C-03 DRAM: 1 GiB Clocks: - MPU : 800 MHz - MCU : 208.878 MHz - AXI : 266.500 MHz - PER : 24 MHz - DDR : 533 MHz WDT: Started with servicing (32s timeout) NAND: 1024 MiB MMC: STM32 SD/MMC: 0, STM32 SD/MMC: 1 Loading Environment from MMC... OK In: serial Out: serial Err: serial Net: eth0: ethernet@5800a000 Hit any key to stop autoboot: 0 Boot over mmc0! switch to partitions #0, OK mmc0 is current device Scanning mmc 0:4... Found /mmc0_extlinux/stm32mp157f-ev1_extlinux.conf Retrieving file: /mmc0_extlinux/stm32mp157f-ev1_extlinux.conf 769 bytes read in 35 ms (20.5 KiB/s) Retrieving file: /splash_portrait.bmp 89462 bytes read in 38 ms (2.2 MiB/s) Select the boot mode 1: OpenSTLinux 2: stm32mp157f-ev1-a7-examples 3: stm32mp157f-ev1-m4-examples Enter choice: 1: OpenSTLinux Retrieving file: /st-image-resize-initrd 3635706 bytes read in 188 ms (18.4 MiB/s) Retrieving file: /uImage 7464336 bytes read in 350 ms (20.3 MiB/s) append: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 Retrieving file: /stm32mp157f-ev1.dtb 123279 bytes read in 40 ms (2.9 MiB/s) ## Booting kernel from Legacy Image at c2000000 ... Image Name: Linux-5.10.61 Created: 2021-08-26 12:51:21 UTC Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 7464272 Bytes = 7.1 MiB Load Address: c2000040 Entry Point: c2000040 Verifying Checksum ... OK ## Flattened Device Tree blob at c4000000 Booting using the fdt blob at 0xc4000000 XIP Kernel Image Loading Ramdisk to cfc88000, end cffff9fa ... OK Loading Device Tree to cfc66000, end cfc8718e ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 5.10.61 (oe-user@oe-host) (arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021 [ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d [ 0.000000] CPU: div instructions available: patching division code [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: STMicroelectronics STM32MP157F eval daughter on eval mother [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] Reserved memory: created DMA memory pool at 0x10000000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node mcuram2@10000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x10040000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node vdev0vring0@10040000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x10041000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node vdev0vring1@10041000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x10042000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node vdev0buffer@10042000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x10048000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node mcu_rsc_table@10048000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x30000000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node mcuram@30000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x38000000, size 0 MiB [ 0.000000] OF: reserved mem: initialized node retram@38000000, compatible id shared-dma-pool [ 0.000000] cma: Reserved 128 MiB at 0xe8000000 [ 0.000000] Zone ranges: [ 0.000000] Normal [mem 0x00000000c0000000-0x00000000efffffff] [ 0.000000] HighMem [mem 0x00000000f0000000-0x00000000ffffefff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x00000000c0000000-0x00000000f5cfffff] [ 0.000000] node 0: [mem 0x00000000f5d00000-0x00000000f5feffff] [ 0.000000] node 0: [mem 0x00000000f5ff0000-0x00000000f5ffffff] [ 0.000000] node 0: [mem 0x00000000f6000000-0x00000000fdffffff] [ 0.000000] node 0: [mem 0x00000000fe000000-0x00000000ffffefff] [ 0.000000] Initmem setup node 0 [mem 0x00000000c0000000-0x00000000ffffefff] [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 20 pages/cpu s51788 r8192 d21940 u81920 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 260415 [ 0.000000] Kernel command line: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear) [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 751136K/1048572K available (11264K kernel code, 1207K rwdata, 3308K rodata, 1024K init, 239K bss, 166364K reserved, 131072K cma-reserved, 128060K highmem) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] random: get_random_bytes called from start_kernel+0x388/0x560 with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (virt). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns [ 0.000008] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns [ 0.000024] Switching to timer-based delay loop, resolution 41ns [ 0.001484] Console: colour dummy device 80x30 [ 0.001540] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000) [ 0.001568] pid_max: default: 32768 minimum: 301 [ 0.001797] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 0.001822] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 0.002973] CPU: Testing write buffer coherency: ok [ 0.003377] /cpus/cpu@0 missing clock-frequency property [ 0.003415] /cpus/cpu@1 missing clock-frequency property [ 0.003432] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 [ 0.004482] Setting up static identity map for 0xc0100000 - 0xc0100060 [ 0.004665] rcu: Hierarchical SRCU implementation. [ 0.005880] smp: Bringing up secondary CPUs ... [ 0.006922] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 [ 0.007144] smp: Brought up 1 node, 2 CPUs [ 0.007171] SMP: Total of 2 processors activated (96.00 BogoMIPS). [ 0.007182] CPU: All CPU(s) started in SVC mode. [ 0.007970] devtmpfs: initialized [ 0.039261] VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5 [ 0.039661] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.039697] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.045634] pinctrl core: initialized pinctrl subsystem [ 0.047351] NET: Registered protocol family 16 [ 0.050191] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.051822] thermal_sys: Registered thermal governor 'step_wise' [ 0.052218] cpuidle: using governor menu [ 0.052572] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers. [ 0.052589] hw-breakpoint: maximum watchpoint size is 8 bytes. [ 0.052937] Serial: AMBA PL011 UART driver [ 0.103493] stm32-pm-domain pm_domain: domain core-ret-power-domain registered [ 0.103555] stm32-pm-domain pm_domain: subdomain core-power-domain registered [ 0.103571] stm32-pm-domain pm_domain: domains probed [ 0.127391] SCSI subsystem initialized [ 0.128227] usbcore: registered new interface driver usbfs [ 0.128303] usbcore: registered new interface driver hub [ 0.128370] usbcore: registered new device driver usb [ 0.128666] pps_core: LinuxPPS API ver. 1 registered [ 0.128683] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.128715] PTP clock support registered [ 0.129543] arm-scmi firmware:scmi0: SCMI Notifications - Core Enabled. [ 0.129625] arm-scmi firmware:scmi0: SCMI Protocol v2.0 'ST:' Firmware version 0x0 [ 0.132622] clocksource: Switched to clocksource arch_sys_counter [ 1.243928] simple-framebuffer f5d00000.framebuffer: framebuffer at 0xf5d00000, 0x1c2000 bytes, mapped to 0x(ptrval) [ 1.243962] simple-framebuffer f5d00000.framebuffer: format=r5g6b5, mode=720x1280x16, linelength=1440 [ 1.244385] simple-framebuffer f5d00000.framebuffer: fb0: simplefb registered! [ 1.256306] NET: Registered protocol family 2 [ 1.256591] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 1.258146] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear) [ 1.258293] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear) [ 1.258387] TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 1.258529] TCP: Hash tables configured (established 8192 bind 8192) [ 1.258709] UDP hash table entries: 512 (order: 2, 16384 bytes, linear) [ 1.258794] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear) [ 1.259392] NET: Registered protocol family 1 [ 1.260332] RPC: Registered named UNIX socket transport module. [ 1.260358] RPC: Registered udp transport module. [ 1.260369] RPC: Registered tcp transport module. [ 1.260380] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 1.260725] Trying to unpack rootfs image as initramfs... [ 1.559152] Freeing initrd memory: 3552K [ 1.559917] hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available [ 1.561760] Initialise system trusted keyrings [ 1.562143] workingset: timestamp_bits=14 max_order=18 bucket_order=4 [ 1.570989] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 1.572261] NFS: Registering the id_resolver key type [ 1.572317] Key type id_resolver registered [ 1.572329] Key type id_legacy registered [ 1.572489] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 1.572506] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 1.572810] ntfs: driver 2.1.32 [Flags: R/O]. [ 1.573116] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc. [ 1.573892] fuse: init (API version 7.32) [ 1.574816] NET: Registered protocol family 38 [ 1.574841] Key type asymmetric registered [ 1.574854] Asymmetric key parser 'x509' registered [ 1.574931] bounce: pool size: 64 pages [ 1.574994] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246) [ 1.575010] io scheduler mq-deadline registered [ 1.575021] io scheduler kyber registered [ 1.587013] STM32 USART driver initialized [ 1.607561] brd: module loaded [ 1.610706] random: fast init done [ 1.615374] random: crng init done [ 1.619801] loop: module loaded [ 1.625704] libphy: Fixed MDIO Bus: probed [ 1.627467] CAN device driver interface [ 1.629652] pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver [ 1.629742] usbcore: registered new interface driver pegasus [ 1.629814] usbcore: registered new interface driver asix [ 1.629868] usbcore: registered new interface driver ax88179_178a [ 1.629919] usbcore: registered new interface driver cdc_ether [ 1.629986] usbcore: registered new interface driver smsc75xx [ 1.630065] usbcore: registered new interface driver smsc95xx [ 1.630118] usbcore: registered new interface driver net1080 [ 1.630169] usbcore: registered new interface driver cdc_subset [ 1.630220] usbcore: registered new interface driver zaurus [ 1.630295] usbcore: registered new interface driver cdc_ncm [ 1.631495] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 1.631547] ehci-platform: EHCI generic platform driver [ 1.632038] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver [ 1.632082] ohci-platform: OHCI generic platform driver [ 1.633074] usbcore: registered new interface driver usb-storage [ 1.637192] i2c /dev entries driver [ 1.641776] stm32-cpufreq stm32-cpufreq: Failed to get chip info: -517 [ 1.643054] sdhci: Secure Digital Host Controller Interface driver [ 1.643073] sdhci: Copyright(c) Pierre Ossman [ 1.643084] Synopsys Designware Multimedia Card Interface Driver [ 1.643586] sdhci-pltfm: SDHCI platform and OF driver helper [ 1.644902] ledtrig-cpu: registered to indicate activity on CPUs [ 1.645128] SMCCC: SOC_ID: ID = jep106:0020:0500 Revision = 0x00002001 [ 1.645568] usbcore: registered new interface driver usbhid [ 1.645584] usbhid: USB HID core driver [ 1.647011] remoteproc remoteproc0: releasing m4 [ 1.649573] NET: Registered protocol family 17 [ 1.649618] can: controller area network core [ 1.649733] NET: Registered protocol family 29 [ 1.649746] can: raw protocol [ 1.649761] can: broadcast manager protocol [ 1.649780] can: netlink gateway - max_hops=1 [ 1.650485] Key type dns_resolver registered [ 1.650645] ThumbEE CPU extension supported. [ 1.650669] Registering SWP/SWPB emulation handler [ 1.651077] registered taskstats version 1 [ 1.651105] Loading compiled-in X.509 certificates [ 1.687381] stm32-mdma 58000000.dma-controller: STM32 MDMA driver registered [ 1.691854] stm32-dma 48000000.dma-controller: STM32 DMA driver registered [ 1.694317] stm32-dma 48001000.dma-controller: STM32 DMA driver registered [ 1.703934] stm_thermal 50028000.thermal: stm_thermal_probe: Driver initialized successfully [ 1.709802] remoteproc remoteproc0: releasing m4 [ 1.711204] /soc/interrupt-controller@5000d000: bank0 [ 1.711233] /soc/interrupt-controller@5000d000: bank1 [ 1.711249] /soc/interrupt-controller@5000d000: bank2 [ 1.715609] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOA bank added [ 1.717987] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOB bank added [ 1.720321] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOC bank added [ 1.722591] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOD bank added [ 1.725037] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOE bank added [ 1.727312] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOF bank added [ 1.729580] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOG bank added [ 1.731843] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOH bank added [ 1.734242] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOI bank added [ 1.736570] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOJ bank added [ 1.738836] stm32mp157-pinctrl soc:pin-controller@50002000: GPIOK bank added [ 1.739110] stm32mp157-pinctrl soc:pin-controller@50002000: Pinctrl STM32 initialized [ 1.742447] stm32mp157-pinctrl soc:pin-controller-z@54004000: GPIOZ bank added [ 1.742487] stm32mp157-pinctrl soc:pin-controller-z@54004000: Pinctrl STM32 initialized [ 1.746180] stm32-usart 40010000.serial: interrupt mode for rx (no dma) [ 1.746208] stm32-usart 40010000.serial: interrupt mode for tx (no dma) [ 1.746246] 40010000.serial: ttySTM0 at MMIO 0x40010000 (irq = 66, base_baud = 4000000) is a stm32-usart [ 2.995054] printk: console [ttySTM0] enabled [ 3.008307] spi-nor spi0.0: mx66l51235l (65536 Kbytes) [ 3.016912] spi-nor spi0.1: mx66l51235l (65536 Kbytes) [ 3.025143] m_can_platform 4400e000.can: m_can device registered (irq=62, version=32) [ 3.033449] stm32-dwmac 5800a000.ethernet: IRQ eth_lpi not found [ 3.038253] stm32-dwmac 5800a000.ethernet: no reset control found [ 3.044864] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42 [ 3.051050] stm32-dwmac 5800a000.ethernet: DWMAC4/5 [ 3.056070] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported [ 3.063380] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported [ 3.070650] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported [ 3.077538] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported [ 3.083950] stm32-dwmac 5800a000.ethernet: TSO supported [ 3.089108] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer [ 3.096920] stm32-dwmac 5800a000.ethernet: Enabled Flow TC (entries=2) [ 3.103405] stm32-dwmac 5800a000.ethernet: TSO feature enabled [ 3.109268] stm32-dwmac 5800a000.ethernet: Using 32 bits DMA width [ 3.117873] libphy: stmmac: probed [ 3.133938] stm32_rtc 5c004000.rtc: registered as rtc0 [ 3.137762] stm32_rtc 5c004000.rtc: setting system clock to 2000-01-01T00:41:13 UTC (946687273) [ 3.146790] stm32_rtc 5c004000.rtc: Date/Time must be initialized [ 3.152460] stm32_rtc 5c004000.rtc: registered rev:1.2 [ 3.184564] stm32f7-i2c 40013000.i2c: STM32F7 I2C-0 bus adapter [ 3.205665] stm32f7-i2c 40015000.i2c: STM32F7 I2C-1 bus adapter [ 3.231804] stpmic1 2-0033: PMIC Chip Version: 0x20 [ 3.240961] vddcore: supplied by vin [ 3.246164] vdd_ddr: supplied by vin [ 3.251271] vdd: supplied by vin [ 3.256177] v3v3: supplied by vin [ 3.261226] vdda: supplied by v3v3 [ 3.264688] v2v8: supplied by v3v3 [ 3.267430] vtt_ddr: supplied by vdd_ddr [ 3.273722] vdd_usb: supplied by vin [ 3.276519] vdd_sd: supplied by v3v3 [ 3.283016] v1v8: supplied by v3v3 [ 3.285486] vref_ddr: supplied by vin [ 3.291885] bst_out: supplied by vin [ 3.294865] vbus_otg: supplied by bst_out [ 3.298780] vbus_sw: supplied by bst_out [ 3.305280] input: pmic_onkey as /devices/platform/soc/5c002000.i2c/i2c-2/2-0033/5c002000.i2c:stpmic@33:onkey/input/input0 [ 3.315897] stm32f7-i2c 5c002000.i2c: STM32F7 I2C-2 bus adapter [ 3.324082] mmci-pl18x 58005000.sdmmc: Got CD GPIO [ 3.328645] mmci-pl18x 58005000.sdmmc: mmc0: PL180 manf 53 rev2 at 0x58005000 irq 57,0 (pio) [ 3.368789] mmci-pl18x 58007000.sdmmc: mmc1: PL180 manf 53 rev2 at 0x58007000 irq 58,0 (pio) [ 3.417507] stm32-ipcc 4c001000.mailbox: ipcc rev:1.0 enabled, 6 chans, proc 0 [ 3.430343] stm32-rproc 10000000.m4: wdg irq registered [ 3.436218] remoteproc remoteproc0: m4 is available [ 3.446239] mmc0: new ultra high speed DDR50 SDHC card at address 5048 [ 3.453953] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xd3 [ 3.459725] mmcblk0: mmc0:5048 SD32G 29.0 GiB [ 3.463551] nand: Micron MT29F8G08ABACAH4 [ 3.467302] nand: 1024 MiB, SLC, erase size: 256 KiB, page size: 4096, OOB size: 224 [ 3.479006] Bad block table found at page 262080, version 0x01 [ 3.484453] Bad block table found at page 262016, version 0x01 [ 3.495427] mmcblk0: p1 p2 p3 p4 p5 p6 p7 [ 3.501878] reg11: supplied by vdd [ 3.504429] reg18: supplied by vdd [ 3.508980] stm32-usbphyc 5a006000.usbphyc: registered rev:1.0 [ 3.520233] fb0: switching to stmdrmfb from simple [ 3.524674] [drm] Initialized stm 1.0.0 20170330 for 5a001000.display-controller on minor 0 [ 3.533593] dwc2 49000000.usb-otg: supply vusb_d not found, using dummy regulator [ 3.541000] dwc2 49000000.usb-otg: supply vusb_a not found, using dummy regulator [ 3.551443] mmc1: new DDR MMC card at address 0001 [ 3.556227] mmcblk1: mmc1:0001 004GA0 3.69 GiB [ 3.559999] mmcblk1boot0: mmc1:0001 004GA0 partition 1 2.00 MiB [ 3.566097] mmcblk1boot1: mmc1:0001 004GA0 partition 2 2.00 MiB [ 3.571915] mmcblk1rpmb: mmc1:0001 004GA0 partition 3 512 KiB, chardev (243:0) [ 3.583913] mmcblk1: p1 p2 p3 p4 p5 [ 3.702848] usb33: supplied by vdd_usb [ 3.705833] dwc2 49000000.usb-otg: EPs: 9, dedicated fifos, 952 entries in SPRAM [ 3.713835] dwc2 49000000.usb-otg: DWC OTG Controller [ 3.717687] dwc2 49000000.usb-otg: new USB bus registered, assigned bus number 1 [ 3.725181] dwc2 49000000.usb-otg: irq 93, io mem 0x49000000 [ 3.732659] hub 1-0:1.0: USB hub found [ 3.735112] hub 1-0:1.0: 1 port detected [ 3.741262] ehci-platform 5800d000.usbh-ehci: EHCI Host Controller [ 3.746173] ehci-platform 5800d000.usbh-ehci: new USB bus registered, assigned bus number 2 [ 3.755345] ehci-platform 5800d000.usbh-ehci: irq 68, io mem 0x5800d000 [ 3.782701] ehci-platform 5800d000.usbh-ehci: USB 2.0 started, EHCI 1.00 [ 3.790000] hub 2-0:1.0: USB hub found [ 3.792481] hub 2-0:1.0: 2 ports detected [ 3.801188] stmfx-core 0-0042: STMFX id: 0x7b, fw version: 3.03 [ 3.836293] stmfx-pinctrl stmfx-pinctrl: DMA mask not set [ 3.844575] stmfx-pinctrl stmfx-pinctrl: 24 GPIOs available [ 3.857602] Goodix-TS 0-005d: supply AVDD28 not found, using dummy regulator [ 3.863752] Goodix-TS 0-005d: supply VDDIO not found, using dummy regulator [ 3.872026] Goodix-TS 0-005d: ID 9147, version: 1040 [ 3.897270] input: Goodix Capacitive TouchScreen as /devices/platform/soc/40013000.i2c/i2c-0/0-005d/input/input1 [ 3.936936] input: joystick as /devices/platform/joystick/input/input2 [ 3.949238] Freeing unused kernel memory: 1024K [ 3.952999] Run /init as init process [ 4.082763] usb 2-1: new high-speed USB device number 2 using ehci-platform Starting version 244.5+ [ 4.284753] hub 2-1:1.0: USB hub found [ 4.287378] hub 2-1:1.0: 4 ports detected [ 5.638811] EXT4-fs (mmcblk0p6): recovery complete [ 5.643496] EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null) [ 6.093187] systemd[1]: System time before build time, advancing clock. [ 6.222824] NET: Registered protocol family 10 [ 6.254773] Segment Routing with IPv6 [ 6.309459] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS -ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 6.330659] systemd[1]: Detected architecture arm. Welcome to ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 (dunfell)! [ 6.425414] systemd[1]: Set hostname to <stm32mp1>. [ 6.438170] systemd[1]: Hardware watchdog 'STM32 Independent Watchdog', version 0 [ 6.445566] systemd[1]: Set hardware watchdog to 32s. [ 7.183897] systemd[1]: Unnecessary job for /dev/ttySTM0 was removed. [ 7.196427] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 7.236967] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 7.274804] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 7.313895] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password …ts to Console Directory Watch. [ 7.353689] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ 7.393604] systemd[1]: Reached target Paths. [ OK ] Reached target Paths. [ 7.423204] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 7.463085] systemd[1]: Reached target Slices. [ OK ] Reached target Slices. [ 7.493263] systemd[1]: Reached target Swap. [ OK ] Reached target Swap. [ 7.558363] systemd[1]: Listening on RPCbind Server Activation Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ 7.593234] systemd[1]: Reached target RPC Port Mapper. [ OK ] Reached target RPC Port Mapper. [ 7.634659] systemd[1]: Listening on Syslog Socket. [ OK ] Listening on Syslog Socket. [ 7.694753] systemd[1]: Listening on Process Core Dump Socket. [ OK ] Listening on Process Core Dump Socket. [ 7.734477] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 7.782501] systemd[1]: Condition check resulted in Journal Audit Socket being skipped. [ 7.790812] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 7.824613] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 7.865283] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 7.904539] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 7.944089] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 7.984694] systemd[1]: Condition check resulted in Huge Pages File System being skipped. [ 7.999312] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 8.040778] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System... [ 8.083212] systemd[1]: Mounting Temporary Directory (/tmp)... Mounting Temporary Directory (/tmp)... [ 8.135467] systemd[1]: Starting Create list of static device nodes for the current kernel... Starting Create list of st…odes for the current kernel... [ 8.183445] systemd[1]: Starting Mount partitions... Starting Mount partitions... [ 8.232571] systemd[1]: Started Hardware RNG Entropy Gatherer Daemon. [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ 8.280306] systemd[1]: Starting RPC Bind... Starting RPC Bind... [ 8.313905] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. [ 8.363569] systemd[1]: Starting Journal Service... Starting Journal Service... [ 8.399842] systemd[1]: Condition check resulted in Load Kernel Modules being skipped. [ 8.429033] systemd[1]: Mounting FUSE Control File System... Mounting FUSE Control File System... [ 8.479048] systemd[1]: Mounting Kernel Configuration File System... Mounting Kernel Configuration File System... [ 8.540590] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems... [ 8.616194] EXT4-fs (mmcblk0p4): recovery complete [ 8.619582] EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: (null) [ 8.631918] systemd[1]: Starting Apply Kernel Variables... Starting Apply Kernel Variables... [ 8.679755] systemd[1]: Starting udev Coldplug all Devices... [ 8.694807] EXT4-fs (mmcblk0p6): re-mounted. Opts: (null) Starting udev Coldplug all Devices... [ 8.787301] systemd[1]: Started RPC Bind. [ OK ] Started RPC Bind. [ 8.801287] systemd[1]: Mounted POSIX Message Queue File System. [ OK ] Mounted POSIX Message Queue File System. [ 8.874866] systemd[1]: Mounted Kernel Debug File System. [ OK ] Mounted Kernel Debug File System. [ 8.914142] systemd[1]: Mounted Temporary Directory (/tmp). [ OK ] Mounted Temporary Directory (/tmp). [ 8.952869] systemd[1]: Started Create list of static device nodes for the current kernel. [ OK ] Started Create list of sta… nodes for the current kernel. [ 8.994043] systemd[1]: Mounted FUSE Control File System. [ OK ] Mounted FUSE Control File System. [ 9.014174] systemd[1]: Mounted Kernel Configuration File System. [ OK ] Mounted Kernel Configuration File System. [ 9.049587] systemd[1]: Started Remount Root and Kernel File Systems. [ OK ] Started Remount Root and Kernel File Systems. [ 9.104272] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. [ OK ] Started Appl[ 9.154462] EXT4-fs (mmcblk0p5): recovery complete [ 9.161238] EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null) [ OK ] Started Starts Psplash Boot screen. Starting Flush Journal to Persistent Storage... Starting Create Static Device Nodes in /dev... [ 9.374924] Goodix-TS 0-005d: I2C transfer error: -6 [ 9.378764] Goodix-TS 0-005d: I2C write end_cmd error [ 9.387600] systemd-journald[294]: Received client request to flush runtime journal. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Started Load/Save Random Seed. [ OK ] Started udev Kernel Device Manager. [ 9.961494] EXT4-fs (mmcblk0p7): recovery complete [ 9.984264] EXT4-fs (mmcblk0p7): mounted filesystem with ordered data mode. Opts: (null) [ OK ] Started Mount partitions. [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Set. [ OK ] Reached target System Time Synchronized. [ 11.536837] st,stm32-spdifrx 4000d000.audio-controller: No cache defaults, reading back from HW [ OK ] Created slice system-systemd\x2dbacklight.slice. [ 11.597889] stm32-dfsdm 4400d000.dfsdm: SPI clock not accurate [ 11.602379] stm32-dfsdm 4400d000.dfsdm: 24573875 = 2048000 * 12 + 2045875 [ 11.615814] mc: Linux media interface: v0.10 Starting Load/Save Screen …f backlight:panel-backlight... [ 11.676674] wm8994 0-001b: supply DCVDD not found, using dummy regulator [ 11.749530] wm8994 0-001b: supply AVDD1 not found, using dummy regulator [ 11.773014] videodev: Linux video capture interface: v2.00 [ OK ] Started Load/Save Screen B… of backlight:panel-backlight. [ OK ] Reached target Hardware activated USB gadget. [ 11.978079] stm32-dcmi 4c006000.dcmi: Probe done [ OK ] Started udev Coldplug all Devices. [ OK ] Reached target System Initialization. [ OK ] Started Daily apt download activities. [ 12.052288] stm32-hash 54002000.hash: will run requests pump with realtime priority [ OK ] Started Daily Cleanup of Temporary Directories. [ 12.074291] stm32-cryp 54001000.cryp: will run requests pump with realtime priority [ OK ] Reached target Timers. [ 12.109242] ov5640 0-003c: supply AVDD not found, using dummy regulator [ 12.110123] wm8994 0-001b: WM8994 revision D CUST_ID 00 [ 12.114915] ov5640 0-003c: supply DVDD not found, using dummy regulator [ 12.127557] stm32-hash 54002000.hash: Init HASH done HW ver 23 DMA mode 1 [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ 12.165739] wm8994 0-001b: No interrupt specified, no interrupts [ 12.179790] stm32-cryp 54001000.cryp: Initialized [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Listening on dropbear.socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ 12.440835] stm32-crc32 58009000.crc: Initialized [ OK ] Started Kernel Logging Service. [ OK ] Started 12.536763] galcore: loading out-of-tree module taints kernel. ;39mSystem Logging Service. [ OK ] Started D-Bus System Message Bus. [ 12.734680] Galcore version 6.4.3.279124 Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... Starting Netdata, Real-time performance monitoring... Starting Login Service... [ OK ] Started TEE Supplicant. Starting Enable USB Ethernet gadget... [ OK ] Started IPv6 Packet Filtering Framework. [ OK ] Started IPv4 Packet Filtering Framework. [ 13.679168] using random self ethernet address [ 13.682242] using random host ethernet address [ 13.877854] usb0: HOST MAC 60:eb:4a:5c:64:0b [ 13.880853] usb0: MAC 62:d1:99:ce:d3:71 [ 13.914421] dwc2 49000000.usb-otg: bound driver configfs-gadget [ OK ] Started Netdata, Real-time performance monitoring. [ OK ] Started Enable USB Ethernet gadget. [ 15.034653] wm8994-codec wm8994-codec: Failed to request Mic1 detect IRQ: -22 [ 15.040444] wm8994-codec wm8994-codec: Failed to request Mic1 short IRQ: -22 [ 15.072882] wm8994-codec wm8994-codec: Failed to request Mic2 detect IRQ: -22 [ 15.078691] wm8994-codec wm8994-codec: Failed to request Mic2 short IRQ: -22 [ OK ] Started Login Service. [ OK ] Created slice system-weston.slice. [ OK ] Reached target Network (Pre). [ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch. Starting Save/Restore Sound Card State... Starting Network Service... [ OK ] Started Save/Restore Sound Card State. [ OK ] Reached target Sound Card. [ OK ] Started Network Service. Starting Network Name Resolution... [ 17.040598] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [RTL8211E Gigabit Ethernet] (irq=POLL) [ 17.076293] dwmac4: Master AXI performs any burst length [ 17.080192] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found [ 17.102780] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported [ 17.116185] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock [ 17.142849] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode [ OK ] Started Network Name Resolution. [ OK ] Reached target Network. [ OK ] Reached target Host and Network Name Lookups. Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started IIO Daemon. [ OK ] Started Respond to IPv6 Node Information Queries. Starting Sound Service... [ OK ] Started Network Router Discovery Daemon. Starting Permit User Sessions... Starting Target Communication Framework agent... [ OK ] Started Permit User Sessions. [ OK ] Started Target Communication Framework agent. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttySTM0. [ OK ] Reached target Login Prompts. Starting Weston Wayland Compositor (on tty7)... [ OK ] Started Weston Wayland Compositor (on tty7). [ OK ] Created slice User Slice of UID 0. Starting User Runtime Directory /run/user/0... [ OK ] Started User Runtime Directory /run/user/0. Starting User Manager for UID 0... [ OK ] Started Sound Service. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. [ OK ] Started User Manager for UID 0. [ OK ] Started Session c1 of user root. ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 stm32mp1 ttySTM0 stm32mp1 login: root (automatic login) Last login: Sun Sep 20 10:44:11 UTC 2020 on tty7 root@stm32mp1:~#NOTICE: Model: STMicroelectronics STM32MP157F eval daughter on eval mother NOTICE: Board: MB1263 Var4.0 Rev.C-03 INFO: Reset reason (0x14): INFO: Pad Reset from NRST INFO:
For ecosystem release v3.0.0 :
3. Basic commands[edit source]
3.1. Printing distribution specific information[edit source]
For ecosystem release v3.1.0 :
initramfs = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b meta-multimedia = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b meta-networking = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b meta-webserver = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b meta-filesystems = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b meta-perl = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b meta-st-stm32mp = default.xml:3d49b4b37ab3d5b80047e494b3fd459da00ff4ba meta-qt5 = default.xml:b4d24d70aca75791902df5cd59a4f4a54aa4a125 meta-st-openstlinux = default.xml:9268cd36c765295f1abb8180f08d5502af2d1fd9 meta = default.xml:c7d2281eb6cda9c1637c20b3540b142073bca235root@stm32mp1:~# cat /etc/build ----------------------- Build Configuration: | ----------------------- BB_VERSION = 1.46.0 BUILD_SYS = x86_64-linux NATIVELSBSTRING = universal TARGET_SYS = arm-ostl-linux-gnueabi MACHINE = stm32mp1 DISTRO = openstlinux-weston DISTRO_VERSION = 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 TUNE_FEATURES = arm vfp cortexa7 neon vfpv4 thumb callconvention-hard TARGET_FPU = hard MANIFESTVERSION = ostl-21-11-17-rc4 DISTRO_CODENAME = dunfell ACCEPT_EULA_stm32mp1 = 1 GCCVERSION = 9.% PREFERRED_PROVIDER_virtual/kernel = linux-stm32mp PREFERRED_VERSION_linux-stm32mp = ----------------------- Layer Revisions: | ----------------------- meta-python = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b meta-oe = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b meta-gnome = default.xml:2e7e98cd0cb82db214b13224c71134b9335a719b meta-
For ecosystem release v3.0.0 :
3.2. Printing system information[edit source]
For ecosystem release v3.1.0 :
Linux stm32mp1 5.10.61 #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021 armv7l armv7l armv7l GNU/Linuxroot@stm32mp1:~# uname -a
For ecosystem release v3.0.0 :
3.3. Printing Linux kernel and GCC versions[edit source]
For ecosystem release v3.1.0 :
Linux version 5.10.61 (oe-user@oe-host) (arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021root@stm32mp1:~# cat /proc/version
For ecosystem release v3.0.0 :
3.4. Printing the amount of disk space available on all mounted file systems[edit source]
For ecosystem release v3.1.0 :
root@stm32mp1:~# df -h
Filesystem Size Used Avail Use% Mounted on
devtmpfs 367M 0 367M 0% /dev
/dev/mmcblk0p6 683M 470M 164M 75% /
tmpfs 433M 64K 433M 1% /dev/shm
tmpfs 433M 8.9M 425M 3% /run
tmpfs 433M 0 433M 0% /sys/fs/cgroup
tmpfs 433M 20K 433M 1% /tmp
/dev/mmcblk0p4 56M 15M 38M 28% /boot
/dev/mmcblk0p5 14M 6.8M 6.2M 53% /vendor
tmpfs 433M 144K 433M 1% /var/volatile
/dev/mmcblk0p7 27G 38M 25G 1% /usr/local
tmpfs 87M 0 87M 0% /run/user/0
For ecosystem release v3.0.0 :
3.5. ssh connection (only if the Ethernet cable is connected)[edit source]
- Get the IP address of your board
UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000 link/ether xx:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff inet xx.xx.xx.xx/xx brd xx.xx.xx.xx scope global dynamic eth0 valid_lft 159045sec preferred_lft 159045sec inet6 xxxx::xx:xx:xx:xx/64 scope link valid_lft forever preferred_lft foreverip addr show eth0 3: eth0: <BROADCAST,MULTICAST,
- On the host computer, connect the terminal to the board using ssh
xx.xx.xx.xx root@stm32mp1:~#ssh root@