User space shared library project

Revision as of 11:34, 24 March 2021 by Registered User (Nathalie Sangouard moved page STM32CubeIDE user space shared library project to How to debug a user space application with STM32CubeIDE/User space shared library project without leaving a redirect: LRA: improve browsing and organization in cate...)
Renaming.png This page is a candidate for renaming (move).
The requested new name is: How to debug a user space application with STM32CubeIDE/User space shared library project in STM32CubeIDE.
The supplied reason is: visibility.
-- Registered User (-) 14:53, 22 March 2021 (CET).
Wiki maintainers: remember to update the pages that link this page before renaming (moving) it.

1. Create a user space shared library project[edit source]

In context of Cortex-A7 sub-project, MP157C-DK2_CA7 here, right click and select Create a userspace Project..

User space project wizard shortcut

We select here Shared Library project type, in C language. Note that our user space project will use by default the SDK version associated to Cortex-A7 sub-project.

User space shared library creation

2. Build[edit source]

  • Select your project, right-click and then Build Project.
Shared library build


3. Update myExe project sources & properties, in order to use mySharedLib[edit source]

Hereafter is an updated code in order main() to call mySharedLib function say_hello().
You also have to reference mySharedLib project inside myExe properties: C/C++ General > Paths and Symbols > References; as depicted hereafter.

Executable source & properties update


4. Preparing Debug Configuration[edit source]

Your target must be Linux booted and network connected. Please, start Target Status widget on the bottom right and check for the green light.

Target Status - green


Please also check How to set up proxy and P2P Ethernet connection with STM32CubeIDE if you are in that case.


5. Linux deployment Configuration[edit source]

In order to run or debug the executable myExe and its shared library mySharedLib it is required to download the shared library object (.so) to the STM32MP15x device. Select the shared library project, right-click Run as... > Run Configurations, then select STM32 Cortex-A Linux Deployment'.

Run configuration shortcut
Linux deployment configuration


6. Debug Configuration[edit source]

Select your project, right-click Debug as... > Debug Configurations, then select STM32 Cortex-A Remote Application'.

The default Connection proposed is "MPU SSH", corresponding to the target IP address discovered by Target Status. The default destination directory is /home/root.
In order the executable myExe to load the mySharedLib dynamic library, a setup of LD_LIBRARY_PATH with the path to mySharedLib is needed before starting debug.

Debug configuration setup

7. Debug: stepping into mySharedLib[edit source]

Click Debug :

  1. Executable is downloaded to the target,
  2. GDBServer is launched on the target,
  3. GDBClient is launched on the workstation and can exchange via network with GDBServer,


User space shared library debug
Info white.png Information
in case of error; please stop any GDBServer running on the target before launching a new debug session.