This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleProposedVersion
Let's start | Develop on Arm® Cortex®-A7 | |||||||
Unpack the board | Populate the target and boot the image | Execute basic commands | Use the demo launcher |
1. Overview[edit source]
This stage will explain you how to connect the Linux terminal of your board to your host computer through the ST-LINK/V2-1.
Then you will see how to execute basic commands with the Linux command line interface in order to be familiarized with the Linux console.
2. The serial terminal[edit source]
The serial terminal will allow you to communicate with the board trough a UART serial interface.
- Install minicom
sudo apt-get install minicom
- Get the ttyACM device instance that need to be used to access the ST-LINK/V2-1
ls /dev/ttyACM* /dev/ttyACM0
- Connect the minicom to the /dev/ttyACM0 device
minicom -D /dev/ttyACM0 Welcome to minicom 2.7 OPTIONS: I18n Compiled on Nov 15 2018, 20:18:47. Port /dev/ttyACM0, 15:56:03 Press CTRL-A Z for help on special keys
- Press the reset button to reset the board. You should see logs displayed in the minicom window
Put some starting logs here
3. Basic commands[edit source]
3.1. Printing distribution specific information[edit source]
lsb_release -a
LSB Version: core-4.1-noarch:core-4.1-arm
Distributor ID: openstlinux-weston
Description: ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.4+openstlinux-4.14-rocko-mp1-18-11-26
Release: 2.4+openstlinux-4.14-rocko-mp1-18-11-26
Codename: rocko
3.2. Printing system information[edit source]
uname -a Linux stm32mp1-boards-rev[b/c] 4.14.48 #1 SMP PREEMPT Tue Nov 27 14:41:52 UTC 2018 armv7l armv7l armv7l GNU/Linux
3.3. Printing Linux kernel and GCC versions[edit source]
cat /proc/version Linux version 4.14.48 (xxxx@yyyy) (gcc version 7.3.0 (GCC)) #1 SMP PREEMPT Tue Nov 27 14:41:52 UTC 2018
3.4. Printing the amount of disk space available on all mounted file systems[edit source]
df -h Filesystem Size Used Avail Use% Mounted on /dev/root 719M 347M 334M 52% / devtmpfs 372M 0 372M 0% /dev tmpfs 436M 0 436M 0% /dev/shm tmpfs 436M 14M 423M 4% /run tmpfs 436M 0 436M 0% /sys/fs/cgroup tmpfs 436M 4.0K 436M 1% /tmp /dev/mmcblk0p4 58M 7.7M 46M 15% /boot tmpfs 436M 160K 436M 1% /var/volatile /dev/mmcblk0p7 15G 14G 0 100% /usr/local /dev/mmcblk0p5 15M 8.7M 4.7M 65% /vendor tmpfs 88M 0 88M 0% /run/user/0
3.5. ssh connection (only if Ethernet cable is connected)[edit source]
- Get the IP address of your board
ip addr show eth0 3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000 link/ether 00:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff inet 10.xx.xx.xx/22 brd 10.xx.xx.xx scope global dynamic eth0 valid_lft 159045sec preferred_lft 159045sec inet6 fe80::xx:xx:xx:xx/64 scope link valid_lft forever preferred_lft forever
- On the host computer connect the terminal to the board using ssh
ssh root@10.xx.xx.xx
root@stm32mp1:~#