This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleProposedVersion
![]() | ||||||||
Let's start | Develop on Arm® Cortex®-A7 | |||||||
![]() |
Unpack the board | ![]() |
Populate the target and boot the image | ![]() |
Execute basic commands | ![]() |
Use the demo launcher | ![]() |
1. Overview[edit source]
This stage will explain you how to get, install and boot the STM32MP15 Discovery kits with the Starter Package.
2. Open a terminal[edit source]
Open a terminal on the host computer.
![](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/9/99/Ubuntu_terminal.png)
Ubuntu terminal
All the command precede with have to be executed in the host computer terminal.
3. Install the tools[edit source]
3.1. STM32CubeProgrammer[edit source]
- Create your STM32MPU tools directory on your host computer
mkdir $HOME/STM32MPU-Tools cd $HOME/STM32MPU-Tools mkdir STM32CubeProgrammer-2.0.0
- Download the version 2.0.0 of STM32CubeProgrammer archive file in a temporary derectory of your host computer
- Uncompress the archive file to get the STM32CubeProgrammer installers
unzip SetupSTM32CubeProgrammer.zip
- Execute the Linux installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-2.0.0" as the installation directory, when it's requested by the installer
./SetupSTM32CubeProgrammer-2.0.0.linux
![](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/2/2d/STM32CubeProgrammer_installation_splashscreen.png)
Splash screen
File:STM32CubeProgrammer installation welcome.png
Welcome page
File:STM32CubeProgrammer installation path.png
Installation path
- Add the STM32CubeProgrammer binary path to your PATH environment variable
export PATH=$HOME/STM32MPU-Tools/STM32CubeProgrammer-2.0.0/bin:$PATH
- Check that the STM32CubeProgrammer tool is properly installed and accessible
STM32_Programmer_CLI --h ------------------------------------------------------------------- STM32CubeProgrammer <tool version> -------------------------------------------------------------------
3.2. USB serial link[edit source]
- Install the libusb on your host computer
sudo apt-get install libusb-1.0-0
- To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows
cd $HOME/STM32MPU-Tools/STM32CubeProgrammer-2.0.0/Drivers/rules sudo cp *.* /etc/udev/rules.d/
4. Download the image[edit source]
- Create your STM32MP15 Starter Package directory on your host computer
mkdir $HOME/STM32MP15-Ecosystem-v1.0.0 cd $HOME/STM32MP15-Ecosystem-v1.0.0 mkdir Starter-Package cd Starter-Package
- Download the STM32MP15-Ecosystem-v1.0.0 Starter Package in the Starter-Package directory newly created
- Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
tar xvf FLASH-stm32mp1-boards-revc-openstlinux-4.14-rocko-mp1-18-11-26.tar.xz
5. Populate the SDCard[edit source]
- Set the boot switches (located at the back of the board) to the off position
![](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/b/ba/STM32MP157C-DK2_jumper_flash.jpg)
boot switches position to flash the board
- Power up the board
- Press the reset button to reset the board
- Go to the Starter Package directory that contains the binaries and the Flash layout files
cd $HOME/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-boards-revc-openstlinux-4.14-rocko-mp1-18-11-26/images/stm32mp1-boards-revc
- Get the device port location for the USB link
STM32_Programmer_CLI -l usb ------------------------------------------------------------------- STM32CubeProgrammer <tool version> ------------------------------------------------------------------- Total number of available STM32 device in DFU mode: 1 Device Index : USB1 USB Bus Number : 002 USB Address Number : 002 Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000 Serial number : 000000000000 Firmware version : 0x011a Device ID : 0x0500
- Flash the microSD card with the image for the trusted boot chain
STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv
- This operation takes several minutes (mainly depending of the rootfs size). A successful flashing outputs the following log:
------------------------------------------------------------------- STM32CubeProgrammer <tool version> ------------------------------------------------------------------- USB speed : High Speed (480MBit/s) Manufacturer ID : STMicroelectronics Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000 Serial number : 000000000000 Firmware version : 0x011a Device ID : 0x0500 AREA NAME SECT.NBR PARTITION.ID SIZE TYPE Partition0 0000 0x00000000 0256 KB RW SECBL 0000 0x00000001 0001 MB RW Partition2 0000 0x00000002 0001 MB RW Partition3 0000 0x00000003 0256 KB RW Partition4 0000 0x00000004 0016 MB RW virtual 0000 0x000000f1 0512 B R Device name : STM32MPxxx Device type : MPU Device CPU : Cortex-A7 Start Embedded Flashing service Memory Programming ... Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32 File : tf-a-stm32mp157c-dk2-trusted.stm32 Size : 228536 Bytes Partition ID : 0x01 Download in Progress: [==================================================] 100% File download complete Time elapsed during the download operation is: 00:00:00.561 RUNNING Program ... PartID: :0x01 Start operation done successfully at partition 0x01 Flashlayout Programming ... [==================================================] 100% Running Flashlayout Partition ... Flashlayout partition started successfully Memory Programming ... Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32 File : u-boot-stm32mp157c-dk2-trusted.stm32 Size : 722945 Bytes Partition ID : 0x03 Download in Progress: [==================================================] 100% File download complete Time elapsed during the download operation is: 00:00:00.665 RUNNING Program ... PartID: :0x03 reconnecting the device ... USB speed : High Speed (480MBit/s) Manufacturer ID : STMicroelectronics Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x0000 Serial number : 0000000000 Firmware version : 0x0110 Device ID : 0x0500 AREA NAME SECT.NBR PARTITION.ID SIZE TYPE fsbl1 0000 0x00000001 0256 KB RW fsbl2 0000 0x00000002 0256 KB RW ssbl 0000 0x00000003 0002 MB RW bootfs 0000 0x00000011 0064 MB RW rootfs 0000 0x00000012 0768 MB RW userfs 0000 0x00000013 6846 MB RW virtual 0000 0x000000f1 0512 B RW OTP 0000 0x000000f2 0512 B RW PMIC 0000 0x000000f4 0008 B RW Start operation done successfully at partition 0x03 Memory Programming ... Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32 File : tf-a-stm32mp157c-dk2-trusted.stm32 Size : 228536 Bytes Partition ID : 0x01 Download in Progress: [==================================================] 100% File download complete Time elapsed during the download operation is: 00:00:00.097 RUNNING Program ... PartID: :0x01 Start operation done successfully at partition 0x01 Memory Programming ... Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32 File : tf-a-stm32mp157c-dk2-trusted.stm32 Size : 228536 Bytes Partition ID : 0x02 Download in Progress: [==================================================] 100% File download complete Time elapsed during the download operation is: 00:00:00.107 RUNNING Program ... PartID: :0x02 Start operation done successfully at partition 0x02 Memory Programming ... Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32 File : u-boot-stm32mp157c-dk2-trusted.stm32 Size : 722945 Bytes Partition ID : 0x03 Download in Progress: [==================================================] 100% File download complete Time elapsed during the download operation is: 00:00:00.326 RUNNING Program ... PartID: :0x03 Start operation done successfully at partition 0x03 Memory Programming ... Opening and parsing file: st-image-bootfs-openstlinux-weston-stm32mp1.ext4 File : st-image-bootfs-openstlinux-weston-stm32mp1.ext4 Size : 64 MBytes Partition ID : 0x11 Download in Progress: [==================================================] 100% File download complete Time elapsed during the download operation is: 00:00:32.392 RUNNING Program ... PartID: :0x11 Start operation done successfully at partition 0x11 Memory Programming ... Opening and parsing file: st-image-weston-openstlinux-weston-stm32mp1.ext4 File : st-image-weston-openstlinux-weston-stm32mp1.ext4 Size : 507952 KBytes Partition ID : 0x12 Download in Progress: [==================================================] 100% File download complete Time elapsed during the download operation is: 00:04:06.544 RUNNING Program ... PartID: :0x12 Start operation done successfully at partition 0x12 Memory Programming ... Opening and parsing file: st-image-userfs-openstlinux-weston-stm32mp1.ext4 File : st-image-userfs-openstlinux-weston-stm32mp1.ext4 Size : 64 MBytes Partition ID : 0x13 Download in Progress: [==================================================] 100% File download complete Time elapsed during the download operation is: 00:00:32.095 RUNNING Program ... PartID: :0x13 Start operation done successfully at partition 0x13 Flashing service completed successfully
6. Boot the board[edit source]
- Set the boot switches (located at the back of the board) to the on position
![](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/1/1d/STM32MP157C-DK2_jumper_boot.jpg)
boot switches position to boot the board
- Power up the board
- Press the reset button to reset the board
- After few seconds, the board starts and automatically go through the following screens
![](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/0/01/STM32MP1_uboot_splashscreen.png)
UBoot splash screen
![](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/4/43/STM32MP1_psplash.png)
Linux splash screen
![](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/4/45/STM32MP1_weston_desktop.png)
Weston desktop
![](/stm32mpu-ecosystem-v3/nsfr_img_auth.php/e/e9/STM32MP1_gtk_demo_launcher.png)
GTK demo launcher
![]() |
![]() |
![]() |