This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleProposedVersion
Let's start | Develop on Arm® Cortex®-A7 | |||||||
Unpack the board | Populate the target and boot the image | Execute basic commands | Use the demo launcher |
1. Overview[edit source]
This stage will explain to you how to get, install and boot the STM32MP15 Discovery kits Starter Package.
2. Install the tools[edit source]
2.1. STM32CubeProgrammer[edit source]
- Create your STM32MPU tools directory on your host computer
PC $> mkdir STM32MPU-Tools PC $> cd STM32MPU-Tools PC $> mkdir STM32CubeProgrammer-2.0.0
- Download the version 2.0.0 of STM32CubeProgrammer archive file in a temporary derectory of your host computer
- Uncompress the archive file to get the STM32CubeProgrammer installers
PC $> unzip SetupSTM32CubeProgrammer.zip
- Execute the Linux installer, which guides you through the installation process. Select "STM32MPU-Tools/STM32CubeProgrammer-2.0.0" as the installation directory, when it's requested by the installer
PC $> ./SetupSTM32CubeProgrammer-2.0.0.linux
2.2. USB serial link[edit source]
- Install the libusb on your host computer
sudo apt-get install libusb-1.0-0
- To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows
PC $> cd STM32MPU-Tools/STM32CubeProgrammer-2.0.0/Drivers/rules PC $> sudo cp *.* /etc/udev/rules.d/
3. Download the image[edit source]
- Create your STM32MP15 Starter Package directory on your host computer
PC $> mkdir STM32MP15-Ecosystem-v1.0.0 PC $> cd STM32MP15-Ecosystem-v1.0.0 PC $> mkdir Starter-Package PC $> cd Starter-Package
- Download the STM32MP15-Ecosystem-v1.0.0 Starter Package in this directory
- Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files:
PC $> tar xvf FLASH-stm32mp1-boards-revc-openstlinux-4.14-rocko-mp1-18-11-26.tar.x
4. Populate the SDCard[edit source]
5. Boot the board[edit source]