This article proposes to address the creation of a simple hello-world application with STM32CubeIDE.
1. Create GtkHelloWorld user space project[edit source]
In the context of a Cortex®-A7 sub-project, called here MP157C-DK2_CA7, right-click and select Create a userspace Project..
Here, an Executable project type in C language is selected. Note that the user space project uses by default the SDK version associated to the Cortex®-A7 sub-project.
2. Update GtkHelloWorld project sources and properties[edit source]
Below, the main.c source code is updated with gtk_hello_world.c as defined in article Create a simple hello-world application.
The proposal to reference the Gtk library is to use the pkg-config command to update the compiler and linker flags, just like it is done in the Makefile of article Create a simple hello-world application. This properties update is done inside menu GtkHelloWorld properties: C/C++ Build > Settings > Tool Settings.
- main.c update and C flag: `pkg-config --cflags gtk+-3.0`
- Linker flags update: `pkg-config --libs gtk+-3.0`
- Now you can build GtKHelloWorld project: right-click on it and then Build Project.
3. Preparing Debug Configuration[edit source]
Your target must be Linux® booted and network connected. Please, start Target Status widget inthe bottom right corner and check for the green light. Remember that the Linux® console cannot be shared outside STM32CubeIDE: butterfly icon.
Also check How to set up proxy and P2P Ethernet connection with STM32CubeIDE if you are in that case.
4. Debug Configuration[edit source]
Select your project, right-click Debug as... > Debug Configurations, then select STM32 Cortex-A Remote Application'.
In the Main tab, the default connection proposed is "MPU SSH", corresponding to the target IP address discovered by the Target Status widget. The default destination directory is /home/root.
5. Debug launch[edit source]
Click Debug :
- GtkHelloWorld is downloaded to the target,
- GDBServer is launched on the target,
- GDBClient is launched on the workstation and can exchange via the network with GDBServer.