This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(3 intermediate revisions by 2 users not shown) | |||
Line 12: | Line 12: | ||
<br> | <br> | ||
This module explains the basic steps to | This module explains the basic steps to control your STM32MP157x-EV1 board. | ||
{{Info|To complete this module, it is assumed a Linux PC running | {{Info|To complete this module, it is assumed a Linux<sup>®</sup> PC running under Ubuntu<sup>®</sup> 20.04 is used. | ||
Refer to [[PC_prerequisites]] }} | Refer to [[PC_prerequisites]] }} | ||
<br> | <br> | ||
Line 24: | Line 24: | ||
<noinclude> | <noinclude> | ||
{{PublicationRequestId | | {{PublicationRequestId | 19645 | 2021-04-19}} | ||
{{DISPLAYTITLE:{{SUBPAGENAME}}}} | {{DISPLAYTITLE:{{SUBPAGENAME}}}} | ||
[[Category:STM32MP157x-EV1 - Let's start|00]] | [[Category:STM32MP157x-EV1 - Let's start|00]] | ||
</noinclude> | </noinclude> |
Latest revision as of 14:44, 17 November 2021

This module explains the basic steps to control your STM32MP157x-EV1 board.
![]() |
To complete this module, it is assumed a Linux® PC running under Ubuntu® 20.04 is used.
Refer to PC_prerequisites |