This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(One intermediate revision by one other user not shown) | |||
Line 14: | Line 14: | ||
This module explains the basic steps to control your STM32MP157x-DK2 board. | This module explains the basic steps to control your STM32MP157x-DK2 board. | ||
{{Info|To complete this module, it is assumed a Linux<sup>®</sup> PC running under Ubuntu<sup>®</sup> | {{Info|To complete this module, it is assumed a Linux<sup>®</sup> PC running under Ubuntu<sup>®</sup> 20.04 is used. | ||
Refer to [[PC_prerequisites]] }} | Refer to [[PC_prerequisites]] }} | ||
<br> | <br> | ||
Line 27: | Line 27: | ||
<noinclude> | <noinclude> | ||
{{DISPLAYTITLE:{{SUBPAGENAME}}}} | {{DISPLAYTITLE:{{SUBPAGENAME}}}} | ||
[[Category:STM32MP157x-DK2 - let's start | 00]] | [[Category:STM32MP157x-DK2 - let's start|00]] | ||
{{PublicationRequestId | 19645 | 2021-04-19}} | {{PublicationRequestId | 19645 | 2021-04-19}} | ||
</noinclude> | </noinclude> |
Latest revision as of 11:50, 17 November 2021

The STM32MP157x-DK2 Discovery kit is a flexible and complete solution for evaluating the capabilities of STM32MP15 microprocessor devices.
This module explains the basic steps to control your STM32MP157x-DK2 board.
![]() |
To complete this module, it is assumed a Linux® PC running under Ubuntu® 20.04 is used.
Refer to PC_prerequisites |