Exceptionally, this wiki is under maintenance.

You can continue to browse it to discover the STM32MP1 series and associated ecosystems (STM32 boards, embedded software, development tools, trace & debug tools...) but contributors can not improve their favorite articles, during phase.

Thank you for your understanding.

STPurple

1 Usage

The STPurple template is used to color text in pages, with the STMicroelectronics corporate primary color shade of purple (█).

Where:

Usage:  {{STPurple|<text to color>|tint=<tint>}}
  • <text to color> is the text to format in purple. If this template is called with no text, the hexadecimal code of the color is returned.
  • <tint> is the tint of the color expressed in percentage. If tint is not set then the original color is used (tint = 100%). The possible value are:
    • 75: 75% of the original color tint
    • 50: 50% of the original color tint
    • 25: 25% of the original color tint

2 Basic examples

You type You get
Coloring text in purple
This is a {{STPurple|STMicroelectronics corporate color: shade of purple: █}}

This is a STMicroelectronics corporate color: shade of purple: █

Coloring text in 75% tint of purple
This is a {{STPurple|STMicroelectronics corporate color: 75% tint of purple: █ | tint=75}}

This is a STMicroelectronics corporate color: 75% tint of purple: █

Coloring text in 50% tint of purple
This is a {{STPurple|STMicroelectronics corporate color: 50% tint of purple: █ | tint=50}}

This is a STMicroelectronics corporate color: 50% tint of purple: █

Coloring text in 25% tint of purple
This is a {{STPurple|STMicroelectronics corporate color: 25% tint of purple: █ | tint=25}}

This is a STMicroelectronics corporate color: 25% tint of purple: █

Getting the hexadecimal code of the color
{{STPurple}} is the hexadecimal code of STMicroelectronics purple.

#8C0078 is the hexadecimal code of STMicroelectronics purple.

Getting the hexadecimal code of the 75% tint of the color
{{STPurple | tint=75}} is the hexadecimal code of STMicroelectronics 75% tint of purple.

#A9409A is the hexadecimal code of STMicroelectronics 75% tint of purple.

Getting the hexadecimal code of the 50% tint of the color
{{STPurple | tint=50}} is the hexadecimal code of STMicroelectronics 50% tint of purple.

#C57FBB is the hexadecimal code of STMicroelectronics 50% tint of purple.

Getting the hexadecimal code of the 25% tint of the color
{{STPurple | tint=25}} is the hexadecimal code of STMicroelectronics 25% tint of purple.

#E2BFDD is the hexadecimal code of STMicroelectronics 25% tint of purple.

3 More examples

You type You get
purple and bold
This is a {{STPurple|'''STMicroelectronics'''}} corporate color: '''{{STPurple|shade of purple: █}}'''

This is a STMicroelectronics corporate color: shade of purple: █

purple and italic
This is a {{STPurple|''STMicroelectronics''}} corporate color: ''{{STPurple|shade of purple: █}}''

This is a STMicroelectronics corporate color: shade of purple: █

4 Maintenance

This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.

5 Code

#8C0078