Approved version. Approved on: 07:52, 24 May 2022
- Last edited one year ago ago
GDB$
1 Usage[edit]
The GDB$ template is used to prefix a command that must be executed on GDB, with a GDB-specific prompt.
Thanks to the gdb-prompt
class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.
Usage: {{GDB$}}
2 Basic examples[edit]
You type | You get |
---|---|
info break command executed on GDB
{{GDB$}} show listsize<br>
Number of source lines gdb will list by default is 10.
|
show listsize |
3 More examples[edit]
You type | You get |
---|---|
2 commands executed on GDB and preformatted text block (space at the beginning of each line)
{{GDB$}} show listsize Number of source lines gdb will list by default is 10. {{GDB$}} continue |
show listsize Number of source lines gdb will list by default is 10. continue |
Command executed on GDB and preformatted text block (space at the beginning of each line)
{{GDB$}} show listsize
Number of source lines gdb will list by default is 10.
|
show listsize Number of source lines gdb will list by default is 10. |
Long command executed on GDB and preformatted text block (space at the beginning of each line)
{{GDB$}} this is a so long command executed on GDB that a horizontal scrolling bar is needed |
this is a so long command executed on GDB that a horizontal scrolling bar is needed
|
Template used within another public message box template
{{Info |
Message before the command
{{GDB$}} show listsize
Number of source lines gdb will list by default is 10.
Message after the command
}}
|
|
Template used within another protected message box template
{{InternalInfo |
Message before the command
{{GDB$}} show listsize
Number of source lines gdb will list by default is 10.
Message after the command
}}
|
4 Maintenance[edit]
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5 Code[edit]