This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User (Merge articles) |
||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
==Usage== | ==Usage== | ||
The [[Template:PC$|PC$]] template is used '''to prefix a command that must be executed on an host PC, with an host-specific prompt'''. | The [[Template:PC$|PC$]] template is used '''to prefix a command that must be executed on an host PC, with an host-specific prompt'''.<br> | ||
Thanks to the <code>pc-prompt</code> class defined in [[MediaWiki:Common.css]], a double (or triple) click to select the command doesn't select the prompt. | |||
Usage: <nowiki>{{</nowiki>PC$}} | Usage: <nowiki>{{</nowiki>PC$}} | ||
Line 9: | Line 10: | ||
! You type !! You get | ! You type !! You get | ||
|- | |- | ||
| <code>ls</code> command executed on the host PC | | <code>ls test</code> command executed on the host PC | ||
<pre style="white-space: pre-wrap;"> | <pre style="white-space: pre-wrap;"> | ||
{{PC$}} ls | {{PC$}} ls test<br> | ||
test1.txt test2.txt | |||
</pre> | </pre> | ||
| | | | ||
{{PC$}} ls | {{PC$}} ls test<br> | ||
test1.txt test2.txt | |||
|} | |||
==More examples== | |||
{| class="st-table" | |||
! You type !! You get | |||
|- | |||
| 2 commands executed on the host PC and preformatted text block (space at the beginning of each line) | |||
<pre style="white-space: pre-wrap;"> | |||
{{PC$}} ls test | |||
test1.txt test2.txt | |||
{{PC$}} cat test/test1.txt | |||
This is a test | |||
</pre> | |||
| | |||
{{PC$}} ls test | |||
test1.txt test2.txt | |||
{{PC$}} cat test/test1.txt | |||
This is a test | |||
|- | |||
| Command executed on the host PC and preformatted text block (space at the beginning of each line) | |||
<pre style="white-space: pre-wrap;"> | |||
{{PC$}} ls test | |||
test1.txt test2.txt | |||
</pre> | |||
| | |||
{{PC$}} ls test | |||
test1.txt test2.txt | |||
|- | |||
| Long command executed on the host PC and preformatted text block (space at the beginning of each line) | |||
<pre style="white-space: pre-wrap;"> | |||
{{PC$}} this is a so long command executed on the host PC that a horizontal scrolling bar is needed | |||
</pre> | |||
| style="max-width:30em;" | | |||
{{PC$}} this is a so long command executed on the host PC that a horizontal scrolling bar is needed | |||
|} | |} | ||
Line 23: | Line 60: | ||
==Code== | ==Code== | ||
</noinclude> | </noinclude><span class="pc-prompt"></span> |
Revision as of 11:00, 18 May 2022
1. Usage
The PC$ template is used to prefix a command that must be executed on an host PC, with an host-specific prompt.
Thanks to the pc-prompt
class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.
Usage: {{PC$}}
2. Basic examples
You type | You get |
---|---|
ls test command executed on the host PC
{{PC$}} ls test<br>
test1.txt test2.txt
|
PC $> ls test |
3. More examples
You type | You get |
---|---|
2 commands executed on the host PC and preformatted text block (space at the beginning of each line)
{{PC$}} ls test
test1.txt test2.txt
{{PC$}} cat test/test1.txt
This is a test
|
PC $> ls test
test1.txt test2.txt
PC $> cat test/test1.txt
This is a test
|
Command executed on the host PC and preformatted text block (space at the beginning of each line)
{{PC$}} ls test
test1.txt test2.txt
|
PC $> ls test
test1.txt test2.txt
|
Long command executed on the host PC and preformatted text block (space at the beginning of each line)
{{PC$}} this is a so long command executed on the host PC that a horizontal scrolling bar is needed
|
PC $> this is a so long command executed on the host PC that a horizontal scrolling bar is needed
|
4. Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5. Code