This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User m (→References) |
Registered User (Merge articles) |
||
Line 3: | Line 3: | ||
The [[Template:ImageMap|ImageMap]] template is used '''to enhance images with dynamic contents''' (explanations and links) using '''image maps''' (aka "clickable images"). An image map is a list of coordinates in an image, that links areas of the image to multiple destinations. In the STM32 MPU wiki, the image maps rely on: | The [[Template:ImageMap|ImageMap]] template is used '''to enhance images with dynamic contents''' (explanations and links) using '''image maps''' (aka "clickable images"). An image map is a list of coordinates in an image, that links areas of the image to multiple destinations. In the STM32 MPU wiki, the image maps rely on: | ||
* the MediaWiki ImageMap extension<ref>[https://www.mediawiki.org/wiki/Extension:ImageMap MediaWiki Extension:ImageMap]</ref> | * the MediaWiki ImageMap extension<ref>[https://www.mediawiki.org/wiki/Extension:ImageMap MediaWiki Extension:ImageMap]</ref> | ||
* the | * the MediaWiki:Imagemap-Highlight.js script, embedded in the ST BlueSpice extension | ||
Usage: <nowiki>{{</nowiki>ImageMap | File:{{HighlightParam|<filename>}}.{{HighlightParam|<extension>}} <nowiki>{{</nowiki>!}} {{HighlightParam|<options>}} <nowiki>{{</nowiki>!}} {{HighlightParam|<caption>}} | Usage: <nowiki>{{</nowiki>ImageMap | File:{{HighlightParam|<filename>}}.{{HighlightParam|<extension>}} <nowiki>{{</nowiki>!}} {{HighlightParam|<options>}} <nowiki>{{</nowiki>!}} {{HighlightParam|<caption>}} | ||
Line 9: | Line 9: | ||
}} | }} | ||
Where: | Where: | ||
* {{HighlightParam|<filename>}}, {{HighlightParam|<extension>}}, {{HighlightParam|<options>}} and {{HighlightParam|<caption>}} are defined in the [[Contributors:Images|images help]] page | * {{HighlightParam|<filename>}}, {{HighlightParam|<extension>}}, {{HighlightParam|<options>}} and {{HighlightParam|<caption>}} are defined in the [[stcontributormanual:Contributors:Images|images help]] page | ||
* {{HighlightParam|<list of coordinates>}} are the coordinates of forms (rectangles, circles...) in the image | * {{HighlightParam|<list of coordinates>}} are the coordinates of forms (rectangles, circles...) in the image | ||
* {{HighlightParam|<list of explanations and links>}} are the explanations and links associated with these forms | * {{HighlightParam|<list of explanations and links>}} are the explanations and links associated with these forms |
Latest revision as of 09:26, 9 July 2021
1. Usage[edit source]
The ImageMap template is used to enhance images with dynamic contents (explanations and links) using image maps (aka "clickable images"). An image map is a list of coordinates in an image, that links areas of the image to multiple destinations. In the STM32 MPU wiki, the image maps rely on:
- the MediaWiki ImageMap extension[1]
- the MediaWiki:Imagemap-Highlight.js script, embedded in the ST BlueSpice extension
<filename>.<extension> {{!}} <options> {{!}} <caption> <list of coordinates> <list of explanations and links> }}Usage: {{ImageMap | File:
Where:
- <filename>, <extension>, <options> and <caption> are defined in the images help page
- <list of coordinates> are the coordinates of forms (rectangles, circles...) in the image
- <list of explanations and links> are the explanations and links associated with these forms
2. Basic examples[edit source]
You type |
{{ImageMap | File:Image_map_example.png {{!}} frame {{!}} center {{!}} Add your text legend here
rect 160 2 248 77 [https://www.st.com/content/st_com/en.html Rectangle example: external link to STMicroelectronics]
poly 292 228 312 187 387 188 407 229 386 271 313 269 292 228 [[Contributors:Fake article | Polygon example: internal link to "Fake article"]]
circle 47 225 44 [[#Fake anchor | Circle example: an explanation about this area]]
poly 87 155 129 105 120 96 160 93 162 130 152 125 108 180 83 159 83 160 [[Contributors:Fake article | Polygons example: internal link to "Fake article"]]
poly 137 225 162 199 163 212 253 212 252 243 163 242 163 253 137 225 [[Contributors:Fake article | Polygons example: internal link to "Fake article"]]
poly 261 110 300 162 294 167 290 168 330 176 334 140 334 137 325 144 283 88 259 106 [[Contributors:Fake article | Polygons example: internal link to "Fake article"]]
}}
|
---|---|
You get |
![]() |
|
3. Maintenance[edit source]
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
4. References[edit source]
5. Code[edit source]
Error: Must specify an image in the first line.