Registered User |
Registered User mNo edit summary |
||
(24 intermediate revisions by 5 users not shown) | |||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
This article aims to give the following information: | This article aims to give the following information: | ||
* How to download and install the '''latest''' SDK for the STM32 microprocessor Series | * How to download and install the '''latest''' SDK for the STM32 microprocessor Series | ||
Line 23: | Line 7: | ||
{{Warning|To use efficiently this SDK, please go through the Developer Package article relative to your STM32 microprocessor Series: [[:Category:Developer Package]]}} | {{Warning|To use efficiently this SDK, please go through the Developer Package article relative to your STM32 microprocessor Series: [[:Category:Developer Package]]}} | ||
==STM32MP15-Ecosystem- | ==STM32MP15-Ecosystem-v2.1.0 release== | ||
</noinclude> | </noinclude> | ||
* The STM32MP1 SDK is delivered through a tarball file named : ''' | * The STM32MP1 SDK is delivered through a tarball file named : '''{{EcosystemRelease/Package | revision=2.1.0 | package=SDK package | request=name}}''' | ||
<span id="Download"></span> | <span id="Download"></span> | ||
* Download and install the STM32MP1 SDK. | * Download and install the STM32MP1 SDK. | ||
{{SoftwareLicenseAgreement | distribution=OpenSTLinux}} | |||
{| class=" | {| class="st-table" | ||
|- | |- | ||
! !! STM32MP1 Developer Package SDK - STM32MP15-Ecosystem- | ! !!style="text-align:center;"|STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v2.1.0 release | ||
|- | |- | ||
| Download || | | Download || | ||
You need to be logged on ''my.st.com'' before accessing the following link: <br /> | You need to be logged on ''my.st.com'' before accessing the following link: <br /> | ||
[ | [{{EcosystemRelease/Package | revision=2.1.0 | package=SDK package | request=url}}/{{EcosystemRelease/Package | revision=2.1.0 | package=SDK package | request=name}} {{EcosystemRelease/Package | revision=2.1.0 | package=SDK package | request=name}}] | ||
|- | |- | ||
| Installation || | | Installation || | ||
* Uncompress the tarball file to get the SDK installation script | * Uncompress the tarball file to get the SDK installation script | ||
< | |||
$ | tar xvf {{EcosystemRelease/Package | revision=2.1.0 | package=SDK package | request=name}} | ||
* If needed, change the permissions on the SDK installation script so that it is executable | |||
<div style="max-width:60em;"> | |||
$ chmod +x {{EcosystemRelease/Package | revision=2.1.0 | package=SDK installation script | request=path}}/{{EcosystemRelease/Package | revision=2.1.0 | package=SDK installation script | request=name}} | |||
</div> | |||
* Run the SDK installation script | |||
** Use the ''-d <SDK installation directory absolute path>'' option to specify the absolute path to the directory in which you want to install the SDK (''<SDK installation directory>'') | |||
** If you follow the [[Example of directory structure for Packages|proposition to organize the working directory]], it means: | |||
<div style="max-width:60em;"> | |||
$ ./{{EcosystemRelease/Package | revision=2.1.0 | package=SDK installation script | request=path}}/{{EcosystemRelease/Package | revision=2.1.0 | package=SDK installation script | request=name}} -d <working directory absolute path>/Developer-Package/SDK | |||
</div> | |||
:* A successful installation outputs the following log: | |||
<pre style="max-width:60em;"> | |||
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 3.1-openstlinux-5-4-dunfell-mp1-20-11-12 | |||
=========================================================================================== | |||
You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed [Y/n]? | |||
Extracting SDK................................................................................................................................................................................................................done | |||
Setting it up...done | |||
SDK has been successfully set up and is ready to be used. | |||
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | |||
$ . <working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | |||
</pre> | </pre> | ||
|- | |||
| Release note || | |||
Details about the content of the SDK are available in the '''associated''' [[STM32MP15 ecosystem release note - v2.1.0|STM32MP15 ecosystem release note]]. | |||
[[File:Archive_box.png|25px|link=]] If you are interested in older releases, please have a look into the section [[STM32MP1_Developer_Package_-_SDK#Archives|Archives]]. | |||
|} | |||
* The SDK is in the ''<SDK installation directory>'': | |||
{{Green|<SDK installation directory>}} {{Highlight|'''SDK for OpenSTLinux distribution''': details in [[Standard SDK directory structure]] article}} | |||
├── environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi {{Highlight|'''Environment setup script''' for Developer Package}} | |||
├── site-config-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | |||
├── {{Green|sysroots}} | |||
│ ├── {{Green|cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi}} {{Highlight|Target sysroot (libraries, headers, and symbols)}} | |||
│ │ └── [...] | |||
│ └── {{Green|x86_64-ostl_sdk-linux}} {{Highlight|Native sysroot (libraries, headers, and symbols)}} | |||
│ └── [...] | |||
└── version-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | |||
<noinclude> | |||
==Archives [[File:Archive_box.png|25px|link=]]== | |||
{{EcosystemFlow/Archives}} | |||
<div class="mw-collapsible mw-collapsed"> | |||
===STM32MP15-Ecosystem-v2.0.0 release=== | |||
<div class="mw-collapsible-content"> | |||
* The STM32MP1 SDK is delivered through a tarball file named : '''{{EcosystemRelease/Package | revision=2.0.0 | package=SDK package | request=name}}''' | |||
<span id="Download"></span> | |||
* Download and install the STM32MP1 SDK. | |||
{{SoftwareLicenseAgreement | distribution=OpenSTLinux}} | |||
{| class="st-table" | |||
|- | |||
! !!style="text-align:center;"|STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v2.0.0 release | |||
|- | |||
| Download || | |||
You need to be logged on ''my.st.com'' before accessing the following link: <br /> | |||
[{{EcosystemRelease/Package | revision=2.0.0 | package=SDK package | request=url}}/{{EcosystemRelease/Package | revision=2.0.0 | package=SDK package | request=name}} {{EcosystemRelease/Package | revision=2.0.0 | package=SDK package | request=name}}] | |||
|- | |||
| Installation || | |||
* Uncompress the tarball file to get the SDK installation script | |||
tar xvf {{EcosystemRelease/Package | revision=2.0.0 | package=SDK package | request=name}} | |||
* If needed, change the permissions on the SDK installation script so that it is executable | * If needed, change the permissions on the SDK installation script so that it is executable | ||
< | <div style="max-width:60em;"> | ||
$ chmod +x | $ chmod +x {{EcosystemRelease/Package | revision=2.0.0 | package=SDK installation script | request=path}}/{{EcosystemRelease/Package | revision=2.0.0 | package=SDK installation script | request=name}} | ||
</ | </div> | ||
* Run the SDK installation script | * Run the SDK installation script | ||
** Use the ''-d <SDK installation directory absolute path>'' option to specify the absolute path to the directory in which you want to install the SDK (''<SDK installation directory>'') | ** Use the ''-d <SDK installation directory absolute path>'' option to specify the absolute path to the directory in which you want to install the SDK (''<SDK installation directory>'') | ||
** If you follow the [[Example of directory structure for Packages|proposition to organize the working directory]], it means: | ** If you follow the [[Example of directory structure for Packages|proposition to organize the working directory]], it means: | ||
< | <div style="max-width:60em;"> | ||
$ ./ | $ ./{{EcosystemRelease/Package | revision=2.0.0 | package=SDK installation script | request=path}}/{{EcosystemRelease/Package | revision=2.0.0 | package=SDK installation script | request=name}} -d <working directory absolute path>/Developer-Package/SDK | ||
</ | </div> | ||
:* A successful installation outputs the following log: | :* A successful installation outputs the following log: | ||
<pre> | <pre style="max-width:60em;"> | ||
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version | ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 3.1-snapshot | ||
=========================================================================================== | |||
You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed[Y/n]? | You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed [Y/n]? | ||
Extracting SDK.......................................................................................................done | Extracting SDK................................................................................................................................................................................................................done | ||
Setting it up...done | Setting it up...done | ||
SDK has been successfully set up and is ready to be used. | SDK has been successfully set up and is ready to be used. | ||
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | ||
$ . | $ . <working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | ||
</pre> | </pre> | ||
|- | |- | ||
| Release note || | | Release note || | ||
Details about the content of the SDK are available in the '''associated''' [[STM32MP15 ecosystem release note - | Details about the content of the SDK are available in the '''associated''' [[STM32MP15 ecosystem release note - v2.0.0|STM32MP15 ecosystem release note]]. | ||
[[File:Archive_box.png|25px|link=]] If you are interested in older releases, please have a look into the section [[STM32MP1_Developer_Package_-_SDK#Archives|Archives]]. | |||
|} | |} | ||
Line 72: | Line 124: | ||
{{Green|<SDK installation directory>}} {{Highlight|'''SDK for OpenSTLinux distribution''': details in [[Standard SDK directory structure]] article}} | {{Green|<SDK installation directory>}} {{Highlight|'''SDK for OpenSTLinux distribution''': details in [[Standard SDK directory structure]] article}} | ||
├── environment-setup-cortexa7t2hf-neon-vfpv4- | ├── environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi {{Highlight|'''Environment setup script''' for Developer Package}} | ||
├── site-config-cortexa7t2hf-neon-vfpv4- | ├── site-config-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | ||
├── {{Green|sysroots}} | ├── {{Green|sysroots}} | ||
│ ├── {{Green|cortexa7t2hf-neon-vfpv4- | │ ├── {{Green|cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi}} {{Highlight|Target sysroot (libraries, headers, and symbols)}} | ||
│ │ └── [...] | │ │ └── [...] | ||
│ └── {{Green|x86_64- | │ └── {{Green|x86_64-ostl_sdk-linux}} {{Highlight|Native sysroot (libraries, headers, and symbols)}} | ||
│ └── [...] | │ └── [...] | ||
└── version-cortexa7t2hf-neon-vfpv4- | └── version-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | ||
{{NoIndex}} | |||
[[Category:Sub-articles]] | |||
{{UpdateNeededForNewRelease| | |||
* Copy the current release (first chapter) in the "Archives" chapter | |||
* Make the following modifications in this copy: | |||
** Change the "Download" span id to "Download <name of the old release>" (example: "Download STM32MP15-Ecosystem-v1.0.0 release") | |||
* Make the following modifications in the first chapter | |||
** Change the name of the tarball file | |||
** Change the download URLs | |||
** Change the link to the release note | |||
** Change the path and the description of the installation directory | |||
}} | |||
</noinclude> |
Latest revision as of 11:24, 30 October 2020
This article aims to give the following information:
- How to download and install the latest SDK for the STM32 microprocessor Series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP15-Ecosystem-v2.1.0 release[edit source]
- The STM32MP1 SDK is delivered through a tarball file named : en.SDK-x86_64-stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12.tar.xz
- Download and install the STM32MP1 SDK.
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v2.1.0 release | |
---|---|
Download |
You need to be logged on my.st.com before accessing the following link: |
Installation |
SDK-x86_64-stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12.tar.xztar xvf en.
$ chmod +x stm32mp1-openstlinux-5.4-dunfell-mp1-20-11-12/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1-openstlinux-5.4-dunfell-mp1-20-11-12.sh
SDK$ ./stm32mp1-openstlinux-5.4-dunfell-mp1-20-11-12/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1-openstlinux-5.4-dunfell-mp1-20-11-12.sh -d <working directory absolute path>/Developer-Package/
SDK installer version 3.1-openstlinux-5-4-dunfell-mp1-20-11-12 =========================================================================================== You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed [Y/n]? Extracting SDK................................................................................................................................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . <working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabiST OpenSTLinux - Weston - (A Yocto Project Based Distro) |
Release note |
Details about the content of the SDK are available in the associated STM32MP15 ecosystem release note.
|
- The SDK is in the <SDK installation directory>:
<SDK installation directory> SDK for OpenSTLinux distribution: details in Standard SDK directory structure article ├── environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi Environment setup script for Developer Package ├── site-config-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi ├── sysroots │ ├── cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi Target sysroot (libraries, headers, and symbols) │ │ └── [...] │ └── x86_64-ostl_sdk-linux Native sysroot (libraries, headers, and symbols) │ └── [...] └── version-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
2. Archives
[edit source]
This wiki is for the v2 ecosystem releases. For information about the previous ecosystem releases, please go through the Wiki archives.