This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User No edit summary |
Registered User |
||
(22 intermediate revisions by 4 users not shown) | |||
Line 4: | Line 4: | ||
==Download the the Linux® kernel source code== | ==Download the the Linux® kernel source code== | ||
{{SoftwareLicenseAgreement | distribution=OpenSTLinux | chapter=Kernel partitions:}} | |||
* Download the [ | ======For {{EcosystemRelease | revision=2.1.0}}====== | ||
* Download the [{{EcosystemRelease/Package | revision=2.1.0 | package=Linux kernel package | request=url}}/{{EcosystemRelease/Package | revision=2.1.0 | package=Linux kernel package | request=name}} STM32MP15-Ecosystem-v2.1.0 Developer Package Sources] to the following directory:<br> '''$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package''' | |||
* Uncompress the tarball file to get the Linux® kernel tarball, the ST patches and the ST configuration fragments | * Uncompress the tarball file to get the Linux® kernel tarball, the ST patches and the ST configuration fragments | ||
{{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem- | {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package | ||
{{PC$}} tar xvf | {{PC$}} tar xvf {{EcosystemRelease/Package | revision=2.1.0 | package=Linux kernel package | request=name}} | ||
<div class="mw-collapsible mw-collapsed"> | <div class="mw-collapsible mw-collapsed"> | ||
======For {{EcosystemRelease | revision= | ======For {{EcosystemRelease | revision=2.0.0}}====== | ||
<div class="mw-collapsible-content"> | <div class="mw-collapsible-content"> | ||
* Download the [{{EcosystemRelease/Package | revision=2.0.0 | package=Linux kernel package | request=url}}/{{EcosystemRelease/Package | revision=2.0.0 | package=Linux kernel package | request=name}} STM32MP15-Ecosystem-v2.0.0 Developer Package Sources] to the following directory:<br> '''$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package''' | |||
* Download the [ | |||
* Uncompress the tarball file to get the Linux® kernel tarball, the ST patches and the ST configuration fragments | * Uncompress the tarball file to get the Linux® kernel tarball, the ST patches and the ST configuration fragments | ||
{{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem- | {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package | ||
{{PC$}} tar xvf | {{PC$}} tar xvf {{EcosystemRelease/Package | revision=2.0.0 | package=Linux kernel package | request=name}} | ||
</div> | |||
==Prepare the Linux® kernel source code== | ==Prepare the Linux® kernel source code== | ||
* Extract the Linux® kernel source | * Extract the Linux® kernel source | ||
For {{EcosystemRelease | revision= | For {{EcosystemRelease | revision=2.1.0}} | ||
{{PC$}} cd | {{PC$}} cd {{EcosystemRelease/Package | revision=2.1.0 | package=Linux kernel package | request=path}} | ||
{{PC$}} tar xvf | {{PC$}} tar xvf {{EcosystemRelease/Package | revision=2.1.0 | package=Linux kernel source | request=name}} | ||
For {{EcosystemRelease | revision=2.0.0}}<span class="mw-collapsible mw-collapsed"> | |||
For {{EcosystemRelease | revision= | {{PC$}} cd {{EcosystemRelease/Package | revision=2.0.0 | package=Linux kernel package | request=path}} | ||
{{PC$}} cd | {{PC$}} tar xvf {{EcosystemRelease/Package | revision=2.0.0 | package=Linux kernel source | request=name}} | ||
{{PC$}} tar xvf | |||
</span> | </span> | ||
* Apply the ST patches | * Apply the ST patches | ||
{{PC$}} cd {{EcosystemRelease/Package | revision=2.1.0 | package=Linux kernel source | request=path}} /* '''For {{EcosystemRelease | revision=2.1.0 }} '''*/ | |||
{{PC$}} cd {{EcosystemRelease/Package | revision=2.0.0 | package=Linux kernel source | request=path}} /* '''For {{EcosystemRelease | revision=2.0.0 }} '''*/ | |||
{{PC$}} for p in `ls -1 ../*.patch`; do patch -p1 < $p; done | {{PC$}} for p in `ls -1 ../*.patch`; do patch -p1 < $p; done | ||
* Apply fragments | * Apply fragments | ||
{{PC$}} make multi_v7_defconfig fragment*.config | {{PC$}} make ARCH=arm multi_v7_defconfig "fragment*.config" | ||
{{PC$}} for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r .config $f; done | {{PC$}} for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r .config $f; done | ||
{{PC$}} yes <nowiki>''</nowiki> | make oldconfig | {{PC$}} yes <nowiki>''</nowiki> | make ARCH=arm oldconfig | ||
==Build the Linux® kernel source code for the first time== | ==Build the Linux® kernel source code for the first time== | ||
{{Info|The first time the kernel is build it could take several minutes.}} | {{Info|The first time the kernel is build it could take several minutes.}} | ||
* Build kernel images (uImage and vmlinux) and device tree (dtbs) | * Build kernel images (uImage and vmlinux) and device tree (dtbs) | ||
{{PC$}} make uImage vmlinux dtbs LOADADDR=0xC2000040 | {{PC$}} make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040 | ||
* Build kernel module | * Build kernel module | ||
{{PC$}} make modules | {{PC$}} make ARCH=arm modules | ||
* Generate output build artifacts | * Generate output build artifacts | ||
{{PC$}} mkdir -p $PWD/install_artifact/ | {{PC$}} mkdir -p $PWD/install_artifact/ | ||
{{PC$}} make INSTALL_MOD_PATH="$PWD/install_artifact" modules_install | {{PC$}} make ARCH=arm INSTALL_MOD_PATH="$PWD/install_artifact" modules_install | ||
==Deploy the Linux® kernel on the board== | ==Deploy the Linux® kernel on the board== | ||
===Push the Linux® kernel into the board=== | ===Push the Linux® kernel into the board=== | ||
{{PC$}} scp arch/arm/boot/uImage root@<board ip address>:/boot | {{PC$}} scp arch/arm/boot/uImage root@<board ip address>:/boot | ||
===Push the devicetree into the board=== | ===Push the devicetree into the board=== | ||
{{PC$}} scp arch/arm/boot/dts/stm32mp157*.dtb root@<board ip address>:/boot | {{PC$}} scp arch/arm/boot/dts/stm32mp157*.dtb root@<board ip address>:/boot | ||
===Push the kernel modules into the board=== | ===Push the kernel modules into the board=== | ||
* Remove the link created inside the '''install_artifact/lib/modules/<kernel version>''' directory | |||
* Remove the link created inside the '''install_artifact/lib/modules/ | For {{EcosystemRelease | revision=2.1.0}}: | ||
{{PC$}} rm install_artifact/lib/modules/4. | {{PC$}} rm install_artifact/lib/modules/5.4.56/build install_artifact/lib/modules/5.4.56/source | ||
For {{EcosystemRelease | revision=2.0.0}}: | |||
{{PC$}} rm install_artifact/lib/modules/5.4.31/build install_artifact/lib/modules/5.4.31/source | |||
{{PC$}} rm install_artifact/lib/modules/4. | |||
* Optionally, strip kernel modules (to reduce the size of each kernel modules) | * Optionally, strip kernel modules (to reduce the size of each kernel modules) | ||
Line 93: | Line 86: | ||
* Go to the Linux® kernel source directory | * Go to the Linux® kernel source directory | ||
For {{EcosystemRelease | revision= | For {{EcosystemRelease | revision=2.1.0}}: | ||
{{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem- | {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package/{{EcosystemRelease/Package | revision=2.1.0 | package=Linux kernel package | request=path}}/{{EcosystemRelease/Package | revision=2.1.0 | package=Linux kernel source | request=path}} | ||
For {{EcosystemRelease | revision= | For {{EcosystemRelease | revision=2.0.0}}:<span class="mw-collapsible mw-collapsed"> | ||
{{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem- | {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package/{{EcosystemRelease/Package | revision=2.0.0 | package=Linux kernel package | request=path}}/{{EcosystemRelease/Package | revision=2.0.0 | package=Linux kernel source | request=path}} | ||
</span> | </span> | ||
* Edit the ''./drivers/gpu/drm/stm/drv.c'' source file | * Edit the ''./drivers/gpu/drm/stm/drv.c'' source file | ||
* Add a log information in the ''stm_drm_platform_probe'' function as follow | * Add a log information in the ''stm_drm_platform_probe'' function as follow | ||
Line 125: | Line 118: | ||
<noinclude> | <noinclude> | ||
{{NoIndex}} | |||
__NOTOC__ | |||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
{{PublicationRequestId | Auto}} | {{PublicationRequestId | Auto}} | ||
</noinclude> | </noinclude> |
Latest revision as of 12:57, 13 November 2020
1. Overview[edit source]
This stage explains how modify, rebuild and reload the Linux® kernel.
You will first be guided to install the Linux® kernel source code in the Developer Package directory. Then step by step you will execute procedures to modify, rebuild and reload the Linux® kernel.
2. Download the the Linux® kernel source code[edit source]
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
For ecosystem release v2.1.0
[edit source]
- Download the STM32MP15-Ecosystem-v2.1.0 Developer Package Sources to the following directory:
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package - Uncompress the tarball file to get the Linux® kernel tarball, the ST patches and the ST configuration fragments
cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package
tar xvf en.SOURCES-kernel-stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12.tar.xz
Expand
For ecosystem release v2.0.0
For ecosystem release v2.0.0
[edit source]
3. Prepare the Linux® kernel source code[edit source]
- Extract the Linux® kernel source
v2.1.0For ecosystem releasecd stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0 tar xvf linux-5.4.56.tar.xz For ecosystem release v2.0.0
Expand
- Apply the ST patches
v2.1.0cd linux-5.4.56 /* For ecosystem release*/ cd linux-5.4.31 /* For ecosystem release v2.0.0
*/ for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
- Apply fragments
make ARCH=arm multi_v7_defconfig "fragment*.config"
for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r .config $f; done
yes '' | make ARCH=arm oldconfig
4. Build the Linux® kernel source code for the first time[edit source]
- Build kernel images (uImage and vmlinux) and device tree (dtbs)
make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040
- Build kernel module
make ARCH=arm modules
- Generate output build artifacts
mkdir -p $PWD/install_artifact/
make ARCH=arm INSTALL_MOD_PATH="$PWD/install_artifact" modules_install
5. Deploy the Linux® kernel on the board[edit source]
5.1. Push the Linux® kernel into the board[edit source]
scp arch/arm/boot/uImage root@<board ip address>:/boot
5.2. Push the devicetree into the board[edit source]
scp arch/arm/boot/dts/stm32mp157*.dtb root@<board ip address>:/boot
5.3. Push the kernel modules into the board[edit source]
- Remove the link created inside the install_artifact/lib/modules/<kernel version> directory
v2.1.0For ecosystem release: rm install_artifact/lib/modules/5.4.56/build install_artifact/lib/modules/5.4.56/source For ecosystem release v2.0.0
: rm install_artifact/lib/modules/5.4.31/build install_artifact/lib/modules/5.4.31/source
- Optionally, strip kernel modules (to reduce the size of each kernel modules)
find install_artifact/ -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
- Copy Kernel modules
scp -r install_artifact/lib/modules/* root@<ip of board>:/lib/modules
- Using the Linux console, re-generate the list of module dependencies (modules.dep) and the list of symbols provided by modules (modules.symbols)
/sbin/depmod -a
- Synchronize data on disk with memory
sync
5.4. Reboot the board[edit source]
reboot
6. Modifying a built-in Linux kernel device driver[edit source]
This simple example adds unconditional log information when the display driver is probed.
- Using the Linux console, check that there is no log information when the display driver is probed
dmesg | grep -i stm_drm_platform_probe
- Go to the Linux® kernel source directory
v2.1.0For ecosystem release: cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package/stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.4.56-r0/linux-5.4.56 For ecosystem release v2.0.0
:Expand
- Edit the ./drivers/gpu/drm/stm/drv.c source file
- Add a log information in the stm_drm_platform_probe function as follow
DRM_INFO("Simple example - %s\n", __func__); return 0; [...] }static int stm_drm_platform_probe(struct platform_device *pdev) { struct device *dev = &pdev->dev; struct drm_device *ddev; int ret; [...]
- Save the file
- Rebuitd the Linux® kernel
make uImage LOADADDR=0xC2000040
- Update the Linux kernel image into board
scp arch/arm/boot/uImage root@<board ip address>:/boot
- Reboot the board
reboot
- Check that there is now log information when the display driver is probed
dmesg | grep -i stm_drm_platform_probe
[ 2.764080] [drm] Simple example - stm_drm_platform_probe