Approved version. Approved on: 16:49, 12 November 2020
- Last edited 2 years ago ago
Install STM32Cube MP1 package
1 Overview[edit]
This stage explains how to install the STM32Cube MP1 Package.
2 Install STM32Cube MP1 package[edit]
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
2.1 For ecosystem release v2.1.0
[edit]
- Download en.STM32Cube_FW_MP1_V1.3.0.zip to the following directory:
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package - Uncompress the archive file to get the STM32CubeMP1 Package
unzip en.STM32Cube_FW_MP1_V1.3.0.zip
2.2 For ecosystem release v2.0.0
[edit]
- Download en.stm32cubemp1_v1-2-0.zip STM32CubeMP1 Package v1.2.0 to the following directory:
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package - Uncompress the archive file to get the STM32CubeMP1 Package
unzip en.stm32cubemp1_v1-2-0.zip
3 STM32Cube MP1 package structure[edit]
3.1 For ecosystem release v2.1.0
[edit]
The STM32Cube MP1 Package is located in your $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package directory and is named STM32Cube_FW_MP1_V1.3.0:
STM32Cube_FW_MP1_V1.3.0 ├── Drivers │ ├── BSP BSP drivers for the supported STM32MP1 boards │ │ └── [...] │ ├── CMSIS │ │ └── [...] │ └── STM32MP1xx_HAL_Driver HAL drivers for the supported STM32MP1 devices │ └── [...] ├── _htmresc │ └── [...] ├── License.md ├── Middlewares │ └── [...] ├── package.xml ├── Projects │ ├── STM32CubeProjectsList.html List of examples and applications for STM32CubeMP1 Package │ ├── STM32MP157C-DK2 Set of examples and applications → STM32MP15 Discovery kits │ │ └── [...] │ └── STM32MP157C-EV1 Set of examples and applications → STM32MP15 Evaluation boards │ └── [...] ├── Readme.md ├── Release_Notes.html Release note for STM32CubeMP1 Package └── Utilities └── [...]
3.2 For ecosystem release v2.0.0
[edit]
The STM32Cube MP1 Package is located in your $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package directory and is named STM32Cube_FW_MP1_V1.2.0:
STM32Cube_FW_MP1_V1.2.0 ├── Drivers │ ├── BSP BSP drivers for the supported STM32MP1 boards │ │ └── [...] │ ├── CMSIS │ │ └── [...] │ └── STM32MP1xx_HAL_Driver HAL drivers for the supported STM32MP1 devices │ └── [...] ├── _htmresc │ └── [...] ├── License.md ├── Middlewares │ └── [...] ├── package.xml ├── Projects │ ├── STM32CubeProjectsList.html List of examples and applications for STM32CubeMP1 Package │ ├── STM32MP157C-DK2 Set of examples and applications → STM32MP15 Discovery kits │ │ └── [...] │ └── STM32MP157C-EV1 Set of examples and applications → STM32MP15 Evaluation boards │ └── [...] ├── Readme.md ├── Release_Notes.html Release note for STM32CubeMP1 Package └── Utilities └── [...]