Board$

Revision as of 10:59, 18 May 2022 by Registered User (Merge articles)

1. Usage

The Board$ template is used to prefix a command that must be executed on a board, with a board-specific prompt.
Thanks to the board-prompt class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.

Usage:  {{Board$}}

2. Basic examples

You type You get
ls test command executed on the board
{{Board$}} ls test<br>
test1.txt test2.txt

ls test
test1.txt test2.txt

3. More examples

You type You get
2 commands executed on the board and preformatted text block (space at the beginning of each line)
 {{Board$}} ls test
 test1.txt test2.txt
 {{Board$}} cat test/test1.txt
 This is a test
 ls test
test1.txt test2.txt
 cat test/test1.txt
This is a test
Command executed on the board and preformatted text block (space at the beginning of each line)
 {{Board$}} ls test
 test1.txt test2.txt
 ls test
test1.txt test2.txt
Long command executed on the board and preformatted text block (space at the beginning of each line)
 {{Board$}} this is a so long command executed on the board that a horizontal scrolling bar is needed
 this is a so long command executed on the board that a horizontal scrolling bar is needed

4. Maintenance

This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.

5. Code

No categories assignedEdit