Last edited 3 years ago

STLightGreen

1. Usage

The STLightGreen template is used to color text in pages, with the STMicroelectronics corporate primary color shade of light green (█).

Usage:  {{STLightGreen|<text to color>|tint=<tint>}}

Where:

  • <text to color> is the text to format in light green. If this template is called with no text, the hexadecimal code of the color is returned.
  • <tint> is the tint of the color expressed in percentage. If tint is not set then the original color is used (tint = 100%). The possible value are:
    • 75: 75% of the original color tint
    • 50: 50% of the original color tint
    • 25: 25% of the original color tint

2. Basic examples

You type You get
Coloring text in light green
This is a {{STLightGreen|STMicroelectronics corporate color: shade of light green: █}}

This is a STMicroelectronics corporate color: shade of light green: █

Coloring text in 75% tint of light green
This is a {{STLightGreen|STMicroelectronics corporate color: 75% tint of light green: █ | tint=75}}

This is a STMicroelectronics corporate color: 75% tint of light green: █

Coloring text in 50% tint of light green
This is a {{STLightGreen|STMicroelectronics corporate color: 50% tint of light green: █ | tint=50}}

This is a STMicroelectronics corporate color: 50% tint of light green: █

Coloring text in 25% tint of light green
This is a {{STLightGreen|STMicroelectronics corporate color: 25% tint of light green: █ | tint=25}}

This is a STMicroelectronics corporate color: 25% tint of light green: █

Getting the hexadecimal code of the color
{{STLightGreen}} is the hexadecimal code of STMicroelectronics light green.

#49B170 is the hexadecimal code of STMicroelectronics light green.

Getting the hexadecimal code of the 75% tint of the color
{{STLightGreen | tint=75}} is the hexadecimal code of STMicroelectronics 75% tint of light green.

#77C594 is the hexadecimal code of STMicroelectronics 75% tint of light green.

Getting the hexadecimal code of the 50% tint of the color
{{STLightGreen | tint=50}} is the hexadecimal code of STMicroelectronics 50% tint of light green.

#A4D8B7 is the hexadecimal code of STMicroelectronics 50% tint of light green.

Getting the hexadecimal code of the 25% tint of the color
{{STLightGreen | tint=25}} is the hexadecimal code of STMicroelectronics 25% tint of light green.

#C7E7D3 is the hexadecimal code of STMicroelectronics 25% tint of light green.

3. More examples

You type You get
light green and bold
This is a {{STLightGreen|'''STMicroelectronics'''}} corporate color: '''{{STLightGreen|shade of light green: █}}'''

This is a STMicroelectronics corporate color: shade of light green: █

light green and italic
This is a {{STLightGreen|''STMicroelectronics''}} corporate color: ''{{STLightGreen|shade of light green: █}}''

This is a STMicroelectronics corporate color: shade of light green: █

4. Maintenance

This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.

5. Code

#49B170

No categories assignedEdit