How to install X-LINUX-AI v2.0.0 on OpenSTLinux v1.2.0

X-LINUX-AI v2.0.0 is officially delivered on top of the OpenSTLinux v2.0.0 but it also supports OpenSTLinux v1.2.0.

This article explains how to use and rebuild X-LINUX-AI v2.0.0 on an OpenSTLinux v1.2.0 distribution. For more detailed information about X-LINUX-AI Expansion Package, refer to X-LINUX-AI OpenSTLinux Expansion Package.

1. Validated hardware[edit source]

As any software expansion package, X-LINUX-AI is supported on all STM32MP1 Series. It has been validated on the following boards:

  • STM32MP157C-DK2[1]
  • STM32MP157C-EV1[2]
  • STM32MP157A-EV1[3]

2. Installing X-LNUX-AI from OpenSTLinux AI package repository[edit source]

Info white.png Information
STMicroelectronics package repository service is provided for evaluation purposes only. Its content can be updated at anytime without notice. It is therefore not approved for use in production.

All the generated X-LINUX-AI packages are available from the OpenSTLinux AI package repository service hosted at the non-browsable URL http://extra.packages.openstlinux.st.com/AI.

This repository contains AI packages that can be simply installed using apt-* utilities. These utilities are the same as the ones used on a Debian system:

  • the main group contains the selection of AI packages whose installation is automatically tested by STMicroelectronics
  • the updates group is reserved for future use like package revision update.

You can install them individually or by group of packages.

2.1. Prerequisites[edit source]

  • The Starter Package must be flashed on your SD card
STM32MP157x-DKx Starter Package procedure
or
STM32MP157x-EV1 Starter Package procedure
  • Your board must have an internet connection either through the network cable or through a WiFi connection.
Info white.png Information

If your internet access depends on a proxy server, define the http_proxy environment variable with the following command before any apt-* commands:

 export http_proxy='http://<proxy url>:<proxy port>/'

2.2. Configuring AI OpenSTLinux package repository[edit source]

Once the board is booted, execute the following command from the console to configure the AI OpenSTLinux package repository:

 wget http://extra.packages.openstlinux.st.com/AI/1.2/pool/config/a/apt-openstlinux-ai/apt-openstlinux-ai_1.0_armhf.deb
 apt-get install ./apt-openstlinux-ai_1.0_armhf.deb
Info white.png Information
This command may issue a warning message similar to the following:
N: Can't drop privileges for downloading as file '/home/root/apt-openstlinux-ai_1.0_armhf.deb'
couldn't be accessed by user '_apt'. - pkgAcquire::Run (13: Permission denied)

You can safely ignore it.


Then synchronize the AI OpenSTLinux package repository.

 apt-get update

2.3. Installing AI packages[edit source]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.

2.3.1. Installing all X-LINUX-AI packages[edit source]

Command Description
apt-get install packagegroup-x-linux-ai
This command installs all the X-LINUX-AI packages (TensorFlow Lite, Edge TPU, armNN, application samples and tools)

2.3.2. Installing AI framework related packages[edit source]

Command Description
apt-get install packagegroup-x-linux-ai-tflite
This command installs X-LINUX-AI packages related to TensorFlow Lite framework (including application samples)
apt-get install packagegroup-x-linux-ai-tflite-edgetpu
This command installs X-LINUX-AI packages related to the Edge TPU framework (including application samples)
apt-get install packagegroup-x-linux-ai-armnn-tflite
This command installs X-LINUX-AI packages related to the armNN framework (including application samples)

2.3.3. Installing individual packages[edit source]

Command Description
apt-get install arm-compute-library
This command installs Arm Compute Library (ACL)
apt-get install arm-compute-library-tools
This command installs Arm Compute Library utilities (graph examples and benchmarks)
apt-get install armnn
This command installs arm Neural Network SDK (armNN)
apt-get install armnn-tensorflow-lite
This command installs armNN TensorFlow Lite parser
apt-get install armnn-tensorflow-lite-examples
This command installs armNN TensorFlow Lite examples
apt-get install armnn-tfl-benchmark
This command installs armNN benchmark application for TensorFlow Lite models
apt-get install armnn-tfl-cv-apps-image-classification-c++
This command installs C++ image classification example using armNN TensorFlow Lite parser
apt-get install armnn-tfl-cv-apps-object-detection-c++
This command installs C++ object detection example using armNN TensorFlow Lite parser
apt-get install armnn-tools
This command installs armNN utilitites such as unitary tests
apt-get install libedgetpu1
This command installs Edge TPU libraries and the USB rules
apt-get install python3-tensorflow-lite
This command installs Python TensorFlow Lite inference engine
apt-get install python3-tensorflow-lite-edgetpu
This command installs Python TensorFlow Lite inference engine for Edge TPU
apt-get install tensorflow-lite-tools
This command installs Tensorflow Lite utilities
apt-get install tflite-cv-apps-edgetpu-image-classification-c++
This command installs C++ image classification example using Coral Edge TPU TensorFlow Lite API
apt-get install tflite-cv-apps-edgetpu-image-classification-python
This command installs Python image classification example using Coral Edge TPU TensorFlow Lite API
apt-get install tflite-cv-apps-edgetpu-object-detection-c++
This command installs C++ object detection example using Coral Edge TPU TensorFlow Lite API
apt-get install tflite-cv-apps-edgetpu-object-detection-python
This command installs Python object detection example using Coral Edge TPU TensorFlow Lite API
apt-get install tflite-cv-apps-image-classification-c++
This command installs C++ image classification using TensorFlow Lite
apt-get install tflite-cv-apps-image-classification-python
This command installs Python image classification example using TensorFlow Lite
apt-get install tflite-cv-apps-object-detection-c++
This command installs C++ object detection example using TensorFlow Lite
apt-get install tflite-cv-apps-object-detection-python
This command installs Python object detection example using TensorFlow Lite
apt-get install tflite-edgetpu-benchmark
This command installs benchmark application for Edge TPU models
apt-get install tflite-models-coco-ssd-mobilenetv1
This command installs TensorFlow Lite COCO SSD Mobilenetv1 model
apt-get install tflite-models-coco-ssd-mobilenetv1-edgetpu
This command installs TensorFlow Lite COCO SSD Mobilenetv1 model for Edge TPU
apt-get install tflite-models-mobilenetv1
This command installs TensorFlow Lite Mobilenetv1 model
apt-get install tflite-models-mobilenetv1-edgetpu
This command installs TensorFlow Lite Mobilenetv1 model for Edge TPU
Info white.png Information
For more information about how to use apt-* utilities, check the Package repository for OpenSTLinux distribution article.

3. Re-generating X-LINUX-AI OpenSTLinux distribution[edit source]

Use the following procedure to re-generate the complete distribution and enable the X-LINUX-AI expansion package.
This procedure is mandatory if you need to update by yourself some frameworks or modify the application samples.
For more details, expand the following sections:

3.1. Downloading the STM32MP1 Distribution Package v1.2.0[edit source]

Install the STM32MP1 Distribution Package v1.2.0, but do not initialize the OpenEmbedded environment (do not source the envsetup.sh).

3.1.1. Cloning the meta-st-stm32mpu-ai git repositories[edit source]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
 cd <Distribution Package installation directory>/layers/meta-st
 git clone https://github.com/STMicroelectronics/meta-st-stm32mpu-ai.git -b v2.0.0_thud

3.2. Setting up the build environment[edit source]

 cd ../..
 DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh

3.3. Adding the new layers to the build system[edit source]

 bitbake-layers add-layer ../layers/meta-st/meta-st-stm32mpu-ai

3.4. Building the image[edit source]

 bitbake st-image-ai
Info white.png Information
Building the image can take a long time since it depends on the host computer performance.

3.5. Flashing the built image[edit source]

Follow this link to know how to flash the built image.

4. References[edit source]