ClonedFrom

Revision as of 12:48, 25 March 2020 by Registered User

1. Usage

The ClonedFrom template is used to indicate that a page was not in the "approved" state, when it was cloned from another wiki (a.k.a. source wiki). Then, it is up to the editor to decide if the original page should be complete first (before modifying the cloned one), or if the modifications in the cloned page are independent of the completion of the original page.

It puts a message box with a "light blue copy" icon in the page.

Only logged-in users who have writing permissions, can see this box. However, do not put any confidential information in the parameters of this template.

Usage:  {{ClonedFrom | <source wiki>}}

Where <source wiki> is the mandatory name of the source wiki.

2. Basic examples

You type You get
ClonedFrom "stm32mpu"
{{ClonedFrom | stm32mpu}}

3. More examples

You type You get
No source wiki supplied
{{ClonedFrom}}

4. Code

Using models.png Before editing, please read carefully
This page was not approved when cloned from the unidentified original wiki:
  • If your modifications apply both to this wiki and the original wiki, it is highly recommended to work in the original wiki.
  • If your modifications are relevant only for this wiki, it is however recommended to complete first the page in the original wiki, in order to limit the merge effort.

Template:2


No categories assignedEdit