This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion
This article provides the following information:
- How to download and install the latest U-Boot for the STM32 microprocessor Series used
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP15-Ecosystem-v1.0.0 release[edit source]
- The STM32MP1 U-Boot is delivered through a tarball file named
- SOURCES-u-boot-openstlinux-4.19-thud-mp1-19-02-20.tar.xz for STM32MP157C-EV1 and STM32MP157X-DKX boards
- Download and install the STM32MP1 U-Boot
- By downloading this software package, you agree to be bound to the terms of the Limited License Agreement. The detailed content licenses can be found here
STM32MP1 Developer Package U-Boot - STM32MP15-Ecosystem-v1.0.0 release | |
---|---|
Download | |
Installation |
$ cd <working directory path>/Developer-Package
$ tar xvf SOURCES-u-boot-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20.tar.xz $ cd stm32mp1-boards-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-2018.11-r0/ $ tar xvf v2018.11.tar.gz |
Release note |
Details of the content of the U-Boot are available in the associated STM32MP15 ecosystem release note. If you are interested in previous releases, please refer to the archives of the ecosystem release note. |
- The U-Boot installation directory is in the <Developer Package installation directory>/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi directory, and is named u-boot-stm32mp-<U-Boot version>:
u-boot-stm32mp-2018.11-r0 U-Boot installation directory ├── [*].patch ST patches to apply during the U-Boot preparation (see next chapter) ├── u-boot-2018.11 U-Boot source code directory ├── Makefile.sdk Makefile for the U-Boot compilation ├── README.HOW_TO.txt Helper file for U-Boot management: reference for U-Boot build ├── series List of all ST patches to apply └── v2018.11.tar.gz Tarball file of the U-Boot source code