STDarkBlue

Revision as of 09:39, 14 October 2021 by Registered User (Merge articles)
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

1. Usage

The STDarkBlue template is used to color text in pages, with the STMicroelectronics corporate primary color shade of dark blue (█).

Where:

Usage:  {{STDarkBlue|<text to color>|tint=<tint>}}
  • <text to color> is the text to format in dark blue. If this template is called with no text, the hexadecimal code of the color is returned.
  • <tint> is the tint of the color expressed in percentage. If tint is not set then the original color is used (tint = 100%). The possible value are:
    • 75: 75% of the original color tint
    • 50: 50% of the original color tint
    • 25: 25% of the original color tint

2. Basic examples

You type You get
Coloring text in dark blue
This is a {{STDarkBlue|STMicroelectronics corporate color: shade of dark blue: █}}

This is a STMicroelectronics corporate color: shade of dark blue: █

Coloring text in 75% tint of dark blue
This is a {{STDarkBlue|STMicroelectronics corporate color: 75% tint of dark blue: █ | tint=75}}

This is a STMicroelectronics corporate color: 75% tint of dark blue: █

Coloring text in 50% tint of dark blue
This is a {{STDarkBlue|STMicroelectronics corporate color: 50% tint of dark blue: █ | tint=50}}

This is a STMicroelectronics corporate color: 50% tint of dark blue: █

Coloring text in 25% tint of dark blue
This is a {{STDarkBlue|STMicroelectronics corporate color: 25% tint of dark blue: █ | tint=25}}

This is a STMicroelectronics corporate color: 25% tint of dark blue: █

Getting the hexadecimal code of the color
{{STDarkBlue}} is the hexadecimal code of STMicroelectronics dark blue.

#03234B is the hexadecimal code of STMicroelectronics dark blue.

Getting the hexadecimal code of the 75% tint of the color
{{STDarkBlue | tint=75}} is the hexadecimal code of STMicroelectronics 75% tint of dark blue.

#425A78 is the hexadecimal code of STMicroelectronics 75% tint of dark blue.

Getting the hexadecimal code of the 50% tint of the color
{{STDarkBlue | tint=50}} is the hexadecimal code of STMicroelectronics 50% tint of dark blue.

#8191A5 is the hexadecimal code of STMicroelectronics 50% tint of dark blue.

Getting the hexadecimal code of the 25% tint of the color
{{STDarkBlue | tint=25}} is the hexadecimal code of STMicroelectronics 25% tint of dark blue.

#BDC5D0 is the hexadecimal code of STMicroelectronics 25% tint of dark blue.

3. More examples

You type You get
Dark blue and bold
This is a {{STDarkBlue|'''STMicroelectronics'''}} corporate color: '''{{STDarkBlue|shade of dark blue: █}}'''

This is a STMicroelectronics corporate color: shade of dark blue: █

Dark blue and italic
This is a {{STDarkBlue|''STMicroelectronics''}} corporate color: ''{{STDarkBlue|shade of dark blue: █}}''

This is a STMicroelectronics corporate color: shade of dark blue: █

4. Maintenance

This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.

5. Code

#03234B

No categories assignedEdit