This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage
Historically, the Grey template was used to color text in pages, with the "classic MediaWiki grey" color. It is now mapped on the STDarkGrey template that is a STMicroelectronics corporate color.
Usage: {{Grey|<text to color>}}
Where <text to color> is the text to format in grey. If this template is called with no text, the hexadecimal code of the color is returned.
Do not use this template anymore: use the STDarkGrey template instead. |
2. Basic examples
You type | You get |
---|---|
Coloring text in "classic MediaWiki" grey: it is now mapped on the STDarkGrey template
This was a {{Grey|"classic MediaWiki" color: grey: █}}: it is now mapped on the ST dark grey. |
This was a "classic MediaWiki" color: grey: █: it is now mapped on the ST dark grey. |
Getting the hexadecimal code of the color
{{Grey}} is the hexadecimal code of STMicroelectronics dark grey. |
#4F5251 is the hexadecimal code of STMicroelectronics dark grey. |
3. More examples
You type | You get |
---|---|
Grey and bold
This was a {{Grey|'''"classic MediaWiki"'''}} color: '''{{Grey|grey: █}}''': it is now mapped on the ST dark grey. |
This was a "classic MediaWiki" color: grey: █: it is now mapped on the ST dark grey. |
Grey and italic
This was a {{Grey|''"classic MediaWiki"''}} color: ''{{Grey|grey: █}}'': it is now mapped on the ST dark grey. |
This was a "classic MediaWiki" color: grey: █: it is now mapped on the ST dark grey. |
4. Code
#4F5251