This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. rootfs partition
Recipe Name | Package Name | Version | License | Description |
---|---|---|---|---|
arm-compute-library | arm-compute-library | 20.05 |
MIT |
arm compute library |
armnn | armnn | 20.05 |
MIT |
armNN inference engine |
armnn | armnn-tensorflow-lite | 20.05 |
MIT |
armNN TensorFlow Lite parser |
flatbuffer | flatbuffer | 1.12.0 |
Apache-2.0 |
Flatbuffer framework |
gstreamer1.0 | gstreamer1.0 | 1.16.2 |
LGPLv2+ |
GStreamer 1.0 multimedia framework |
gstreamer1.0-plugins-bad | gstreamer1.0-plugins-bad-debugutilsbad | 1.16.2 |
GPLv2+ |
GStreamer plugin for debugutilsbad |
gstreamer1.0-plugins-bad | gstreamer1.0-plugins-bad-waylandsink | 1.16.2 |
GPLv2+ |
GStreamer plugin for waylandsink |
gstreamer1.0-plugins-base | gstreamer1.0-plugins-base-app | 1.16.2 |
GPLv2+ |
GStreamer plugin for app |
gstreamer1.0-plugins-base | gstreamer1.0-plugins-base-videoconvert | 1.16.2 |
GPLv2+ |
GStreamer plugin for videoconvert |
gstreamer1.0-plugins-base | gstreamer1.0-plugins-base-videorate | 1.16.2 |
GPLv2+ |
GStreamer plugin for videorate |
gstreamer1.0-plugins-good | gstreamer1.0-plugins-good-video4linux2 | 1.16.2 |
GPLv2+ |
GStreamer plugin for video4linux2 |
gstreamer1.0-plugins-base | gstreamer1.0-plugins-base-videoscale | 1.16.2 |
GPLv2+ |
GStreamer plugin for videoscale |
gtk+3 | gtk+3-locale-en | 3.24.14 |
LGPLv2 |
Multi-platform toolkit for creating GUIs - en translations |
opencv | libopencv-core | 4.1.0 |
BSD-3-Clause |
Open source computer vision core framework |
python3 | libpython3.5m1.0 | 3.5.6 |
PSFv2 |
The Python Programming Language |
python3 | python3-ctypes | 3.8.2 |
PSFv2 |
Python C types support |
python3 | python3-multiprocessing | 3.8.2 |
PSFv2 |
Python multiprocessing support |
python3-numpy | python3-numpy | 1.17.4 |
BSD-3-Clause |
A sophisticated numeric processing package for Python |
opencv | python3-opencv | 4.1.0 |
BSD-3-Clause |
Python open source computer vision framework |
python3 | python3-threading | 3.8.2 |
PSFv2 |
Python threading & synchronization support |
python3-pillow | python3-pillow | 6.2.1 |
MIT |
Python Imaging Library |
python3-pygobject | python3-pygobject | 3.34.0 |
LGPLv2.1 |
Python GObject bindings |
tensorflow-lite | python3-tensorflow-lite | 2.2.0 |
Apache-2.0 |
Python TensorFlow Lite inference engine |
2. userfs partition
Recipe Name | Package Name | Version | License | Description |
---|---|---|---|---|
armnn | armnn-tensorflow-lite-examples | 20.05 |
MIT |
armNN TensorFlow Lite examples |
armnn-tfl-benchmark | armnn-tfl-benchmark | 1.0 |
GPLv2 |
armNN benchmark for TensorFlow Lite models |
armnn-tfl-cv-apps-image-classification-c++ | armnn-tfl-cv-apps-image-classification-c++ | 1.0 |
GPLv2 |
armNN TensorFlow Lite C++ image classification example |
armnn-tfl-cv-apps-object-detection-c++ | armnn-tfl-cv-apps-object-detection-c++ | 1.0 |
GPLv2 |
armNN TensorFlow Lite C++ object detection example |
armnn | armnn-tools | 20.05 |
MIT |
armNN tools |
tensorflow-lite | tensorflow-lite-tools | 2.2.0 |
Apache-2.0 |
Tensorflow Lite utilities |
tflite-cv-apps-image-classification-c++ | tflite-cv-apps-image-classification-c++ | 1.0 |
GPLv2 |
TensorFlow Lite C++ image classification example |
tflite-cv-apps-image-classification-python | tflite-cv-apps-image-classification-python | 1.0 |
GPLv2 |
TensorFlow Lite Python image classification example |
tflite-cv-apps-object-detection-c++ | tflite-cv-apps-object-detection-c++ | 1.0 |
BSD-3-Clause |
TensorFlow Lite C++ object detection example |
tflite-cv-apps-object-detection-python | tflite-cv-apps-object-detection-python | 1.0 |
BSD-3-Clause |
TensorFlow Lite Python object detection example |
tflite-models-coco-ssd-mobilenetv1 | tflite-models-coco-ssd-mobilenetv1 | 1.0 |
Apache-2.0 |
TensorFlow Lite COCO SSD Mobilenetv1 model |
tflite-models-mobilenetv1 | tflite-models-mobilenetv1 | 1.0 |
Apache-2.0 |
TensorFlow Lite Mobilenetv1 model |