Install the SDK

Revision as of 16:02, 9 October 2019 by Registered User (→‎Starting up the SDK)


1. Overview[edit source]

This stage explains how to install the SDK.
The SDK for OpenSTLinux distribution provides a stand-alone cross-development toolchain and libraries tailored to the contents of the specific image flashed in the board.

2. Host computer configuration[edit source]

2.1. Install extra package[edit source]

In order to do basic development tasks or basic cross-compilation, some extra Ubuntu packages should be installed:

 sudo apt-get update
 sudo apt-get install sed wget curl cvs subversion git-core coreutils unzip texi2html texinfo docbook-utils gawk python-pysqlite2 diffstat help2man make gcc build-essential g++ desktop-file-utils chrpath libxml2-utils xmlto docbook bsdmainutils iputils-ping cpio python-wand python-pycryptopp python-crypto
 sudo apt-get install libsdl1.2-dev xterm corkscrew nfs-common nfs-kernel-server device-tree-compiler mercurial u-boot-tools libarchive-zip-perl
 sudo apt-get install ncurses-dev bc linux-headers-generic gcc-multilib libncurses5-dev libncursesw5-dev lrzsz dos2unix lib32ncurses5 repo libssl-dev
 sudo apt-get install default-jre

2.2. Additionnal configurations[edit source]

  • Allow up to 16 partitions per mmc

By default, on Linux system, a maximum of 8 partitions are allowed on mmc. All Packages (Starter Package, ...) need more than 10 partitons for the storage device. In order to extend the number of partitions per device to 16, the following options must be added to modprobe:

 echo 'options mmc_block perdev_minors=16' > /tmp/mmc_block.conf
 sudo mv /tmp/mmc_block.conf /etc/modprobe.d/mmc_block.conf

3. Download the SDK[edit source]

3.1. For ecosystem release v1.1.0[edit source]
 cd $HOME/STM32MPU_workspace/tmp
 tar xvf en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-19-10-09.tar.xz
3.2. For ecosystem release v1.0.0[edit source]
 cd $HOME/STM32MPU_workspace/tmp
 tar xvf en.SDK-x86_64-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20.tar.xz

4. Run the SDK installation script[edit source]

4.1. For ecosystem release v1.1.0[edit source]
  • Create your STM32MP15 Developer Package SDK directory on your host computer
 mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Developer-Package
 mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Developer-Package/SDK
  • Change the permissions of the SDK installation script so that it is executable
 chmod +x $HOME/STM32MPU_workspace/tmp/stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-10-09.sh
  • Execute the SDK installation script
 $HOME/STM32MPU_workspace/tmp/stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-10-09.sh -d $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Developer-Package/SDK
  • A successful installation outputs the following log:
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 2.6-openstlinux-4.19-thud-mp1-19-10-09
=====================================================================================================================
You are about to install the SDK to "/local/home/frq08927/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Developer-Package/SDK". Proceed[Y/n]? Y
Extracting SDK..................................................................................................................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
 $ . /<working directory absolute path>/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi
4.2. For ecosystem release v1.0.0[edit source]
  • Create your STM32MP15 Developer Package SDK directory on your host computer
 mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package
 mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/SDK
  • Change the permissions of the SDK installation script so that it is executable
 chmod +x $HOME/STM32MPU_workspace/tmp/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-02-20.sh
  • Execute the SDK installation script
 $HOME/STM32MPU_workspace/tmp/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-openstlinux-4.19-thud-mp1-19-02-20.sh -d $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/SDK
  • A successful installation outputs the following log:
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 2.6-openstlinux-4.19-thud-mp1-19-02-20
=====================================================================================================================
You are about to install the SDK to "/local/home/frq08927/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/SDK". Proceed[Y/n]? Y
Extracting SDK..................................................................................................................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
 $ . /<working directory absolute path>/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi

5. Starting up the SDK[edit source]

Info white.png Information
The SDK environment setup script must be run once in each new working terminal in which you cross-compile

For ecosystem release v1.1.0

 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Developer-Package 
 source SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi

For ecosystem release v1.0.0

  cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package 
 source SDK/environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi



The following checkings allow to ensure that the environment is correctly setup:

  • Check the target architecture
 echo $ARCH
arm
  • Check the toolchain binary prefix for the target tools
 echo $CROSS_COMPILE
arm-openstlinux_weston-linux-gnueabi-
  • Check the C compiler version
 $CC --version
arm-openstlinux_weston-linux-gnueabi-gcc (GCC) 8.2.0
Copyright (C) 2018 Free Software Foundation, Inc.
This is free software; see the source for copying conditions.  There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
  • Check that the SDK version is the expected one
 echo $OECORE_SDK_VERSION
  
2.6-openstlinux-4.19-thud-mp1-19-10-09 /* For ecosystem release  v1.1.0  */

2.6-openstlinux-4.19-thud-mp1-19-02-20 /* For ecosystem release  v1.0.0  */


If any of these commands fails or does not return the expected result, please try to reinstall the SDK.