This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage[edit source]
The EcosystemRelease/Component template returns the version of a software component delivered by an ecosystem release revision.
Usage: {{EcosystemRelease/Component | revision=<revision> | component=<component>}}
Where:
- <revision> is the mandatory revision of the ecosystem release, for which the version of the software component is requested.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
- <component> is the mandatory software component delivered by the ecosystem release revision, for which the version of the component is requested. The possible values are:
- Linux kernel
- U-Boot
- TF-A
- OP-TEE
- STM32CubeMPU
- OpenEmbedded
- Android
The returned value is:
- a string that contains the version of the software component delivered by the ecosystem release revision.
- an empty string, if the software component is not delivered by the ecosystem release revision.
- "unknown revision", if <<revision> is not supported.
- "unknown component", if <<component> is not supported.
2. Basic examples[edit source]
You type | You get |
---|---|
Linux kernel version for v1.0.0 revision requested
{{EcosystemRelease/Component | revision=1.0.0 | component=Linux kernel}}
|
Linux kernel LTS v4.19.9 |
U-Boot version for v1.0.0 revision requested
{{EcosystemRelease/Component | revision=1.0.0 | component=U-Boot}}
|
U-Boot v2018.11 |
TF-A version for v1.0.0 revision requested
{{EcosystemRelease/Component | revision=1.0.0 | component=TF-A}}
|
TF-A v2.0 |
OP-TEE version for v1.0.0 revision requested
{{EcosystemRelease/Component | revision=1.0.0 | component=OP-TEE}}
|
OP-TEE v3.3.0 |
STM32CubeMPU version for v1.0.0 revision requested
{{EcosystemRelease/Component | revision=1.0.0 | component=STM32CubeMPU }} |
STM32CubeMP1 Package v1.0.0 |
OpenEmbedded version for v1.0.0 revision requested
{{EcosystemRelease/Component | revision=1.0.0 | component=OpenEmbedded}} |
OpenEmbedded v2.6 (Thud) |
Android version for v1.1.0 revision requested
{{EcosystemRelease/Component | revision=1.1.0 | component=Android}} |
Android v9.0.0_r46 |
3. More examples[edit source]
You type | You get |
---|---|
Linux kernel version for v1.1.0 revision requested
{{EcosystemRelease/Component | revision=1.1.0 | component=Linux kernel}}
|
Linux kernel LTS v4.19.9 |
Android version for the v1.1.0 revision requested
{{EcosystemRelease/Component | revision=1.1.0 | component=Android}} |
Android v9.0.0_r46 |
Android version for the v1.0.0 revision requested: Android is not supported by this ecosystem release revision
{{EcosystemRelease/Component | revision=1.0.0 | component=Android}} |
|
U-Boot version for an unspecified revision requested
{{EcosystemRelease/Component | component=U-Boot}}
|
unknown revision |
TF-A version for an unknown revision requested
{{EcosystemRelease/Component | revision=0.0.1 | component=TF-A}}
|
unknown revision |
Unspecified component
{{EcosystemRelease/Component | revision=1.0.0}} |
unknown component |
Unknown component
{{EcosystemRelease/Component | revision=1.0.0 | component=not supported}} |
unknown component |
4. Code[edit source]
unknown component