This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage
The InternalInfo template is used to store, in a page, information that are restricted to STMicroelectronics employees (and therefore useless for any other reader): configurations specific to the STMicroelectronics network, links to internal resources (e.g. video files) etc.
It puts a message box with a "dark blue be.ST" icon in the page.
Only signed-up users who have writing permissions, can see this box. However, do not put any confidential information in the parameters of this template.
Usage: {{InternalInfo | <message>}}
Where <message> is the mandatory internal info message.
2. Basic examples
You type | You get |
---|---|
Internal info
{{InternalInfo | When connecting to the STMicroelectronics network, you have to execute these additional commands: ...}} |
|
3. More examples
You type | You get |
---|---|
No message supplied
{{InternalInfo}} |
|
Message supplied with a long sentence
{{InternalInfo | The message is a long sentence. Lorem ipsum: isdem diebus Apollinaris Domitiani gener, paulo ante agens palatii Caesaris curam, ad Mesopotamiam missus a socero per militares numeros immodice scrutabatur, an quaedam altiora meditantis iam Galli.}} |
|