This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.![]() | ||||||
Develop on Arm® Cortex®-A7 | Develop on Arm® Cortex®-M4 | |||||
![]() |
Install the SDK | ![]() |
Create a simple hello-world application | ![]() |
Modify, rebuild and reload the Linux® kernel | ![]() |
1. Overview[edit source]
This stage explains how to create, build and execute a simple C code application using the freshly installed SDK.
2. Code[edit source]
- Create a directory that will host your source codes
For ecosystem release v2.1.0: mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package/stm32mp1-openstlinux-20-11-12 mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package/stm32mp1-openstlinux-20-11-12/sources For ecosystem release v2.0.0
: mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package/stm32mp1-openstlinux-20-06-24 mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package/stm32mp1-openstlinux-20-06-24/sources
- Create a directory for your user space example
For ecosystem release v2.1.0: mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package/stm32mp1-openstlinux-20-11-12/sources/gtk_hello_world_example cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Developer-Package/stm32mp1-openstlinux-20-11-12/sources/gtk_hello_world_example For ecosystem release v2.0.0
: mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package/stm32mp1-openstlinux-20-06-24/sources/gtk_hello_world_example cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.0.0/Developer-Package/stm32mp1-openstlinux-20-06-24/sources/gtk_hello_world_example
- Create the source code file for your user space example: gtk_hello_world.c
#include <gtk/gtk.h> static void print_hello (GtkWidget *widget, gpointer data) { g_print ("Hello World\n"); } static void activate (GtkApplication *app, gpointer user_data) { GtkWidget *window; GtkWidget *button; GtkWidget *button_box; window = gtk_application_window_new (app); gtk_window_set_title (GTK_WINDOW (window), "Window"); gtk_window_set_default_size (GTK_WINDOW (window), 200, 200); button_box = gtk_button_box_new (GTK_ORIENTATION_HORIZONTAL); gtk_container_add (GTK_CONTAINER (window), button_box); button = gtk_button_new_with_label ("Hello World"); g_signal_connect (button, "clicked", G_CALLBACK (print_hello), NULL); g_signal_connect_swapped (button, "clicked", G_CALLBACK (gtk_widget_destroy), window); gtk_container_add (GTK_CONTAINER (button_box), button); gtk_widget_show_all (window); } int main (int argc, char **argv) { GtkApplication *app; int status; app = gtk_application_new ("org.gtk.example", G_APPLICATION_FLAGS_NONE); g_signal_connect (app, "activate", G_CALLBACK (activate), NULL); status = g_application_run (G_APPLICATION (app), argc, argv); g_object_unref (app); return status; }
3. Build[edit source]
- Create the makefile for your user space example: Makefile
PROG = gtk_hello_world SRCS = gtk_hello_world.c CLEANFILES = $(PROG) # Add / change option in CFLAGS and LDFLAGS CFLAGS += -Wall $(shell pkg-config --cflags gtk+-3.0) LDFLAGS += $(shell pkg-config --libs gtk+-3.0) all: $(PROG) $(PROG): $(SRCS) $(CC) -o $@ $^ $(CFLAGS) $(LDFLAGS) clean: rm -f $(CLEANFILES) $(patsubst %.c,%.o, $(SRCS))
- Cross-compile the project
make
4. Deploy and execute[edit source]
- Push this binary into the board (Ethernet connection needed)
scp gtk_hello_world root@<board ip address>:/usr/local
- Execute your user space example
cd /usr/local/ ./gtk_hello_world (gtk_hello_world:6370): dbind-WARNING **: 18:17:49.914: Error retrieving accessibility bus address: org.a11y.Bus.Error: Failed to execute chi)
- A GTK windows is displayed
- Click on the "Hello world" button to close the window. Hello world is displayed in the console:
Hello world
![]() |
![]() |
![]() |